Test Instrumentation
  • Challenges & Projects
  • Project14
  • Test Instrumentation
  • More
  • Cancel
Test Instrumentation
Blog "No lies" IR Thermometer - part II
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Test Instrumentation to participate - click to join for free!
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: koudelad
  • Date Created: 23 Sep 2018 8:26 PM Date Created
  • Views 3179 views
  • Likes 11 likes
  • Comments 8 comments
  • target 3001
  • ir_thermometer
  • psoc 4
  • diytestinstruch
Related
Recommended

"No lies" IR Thermometer - part II

koudelad
koudelad
23 Sep 2018
image

Test Instrumentation

Enter Your Electronics & Design Project for a chance to win a Grand Prize for Originality, a Tool Set, and a $100 Shopping Cart!

Back to The Project14 homepage image

Project14 Home
Monthly Themes
Monthly Theme Poll

 

Blog posts:

"No lies" IR Thermometer - part I

This is part 2

"No lies" IR Thermometer - part III

"No lies" IR Thermometer - part IV

 

IR thermometer v1 – the hardware

In my previous blog post I described my motivation to build my own body IR thermometer, included a few sentences about the principles and showed 2 prototypes using a ready-made development kit and a breadboard with PSoC 5LP and PSoC 4 devices. I also mentioned, that I wanted to create my first professionally made PCB.

 

As written before, my approach is to do incremental development, one step at a time. You will definitely see images of electronics made by an amateur. However, my goal is to learn at least a small bit of something new every time I am doing something, so feel free to comment what can I make better next time.

 

The design software

The first step to create a PCB is usually creating schematics. Why usually? I have a friend that has a good memory and a sense of routing signals, so he usually draws PCBs with up to ca. 300 components (yes, three hundred) in his design software straight away.

 

I am a fan of more planning (drawing schematics) and only after that, placing the components and drawing tracks. About 10 years ago, almost every amateur I met (physically or on the internet) used EAGLE. I never really got used to the controls, so I tried about 10 design programs and then found Target 3001! The fun part is, I tried EAGLE, KiCAD and some software packages offered by component distributors and ended up with Target 3001! again. I don’t want to make any advertisement and I have no interest in doing so, but I like the software for two things. First, it gets the job done quickly, the controls are quite intuitive for me. Second, it is being developed almost three decades by a family company. If you write them an email and ask for support, it is not unusual you get an answer from the founder or his son. Pretty rare these days.

 

The schematics

It won’t be surprising how I started drawing. I found the schematics of the PSoCRegistered 4 CY8CKIT-049 4200 Prototyping Kit, removed what wasn’t necessary and added all the components from the breadboard.

 

Just a few notes about the design:

 

J1 is a power connector and the idea is to power the device directly by 2 AA or AAA alkaline batteries.

 

J5 is a connector intended for UART. I might find it useful in the future, but it is not implemented at the moment.

 

There are two push buttons and one LED. The LED has no function and only one of the buttons starts the measurement. The other button has no function. Both buttons have unpopulated pin header in parallel with them. My idea was to embed the device into a box, but leave the possibility to control the thermometer without the box, too.

 

Here comes the full schematics. I know, it is kind of chaotic.

image

 

PCB

And the PCB I drew based on the schematics. My first PCB sent to a PCB manufacturer ever image

image

 

I ordered the PCB at a smaller Czech company to show some support to local companies. My friend helped me to prepare the data (especially for the pool service, which makes the PCB cheaper). I thought exporting should be easy, but it is worth asking the manufacturer about formats etc. to avoid additional costs of manual adjustments at the manufacturing facility.

 

One week passed and this is what I got:

image

image

 

I also knew that I wouldn’t be able to solder the chip with my current soldering iron. So, this was a perfect excuse to buy a new one, with a finer handle and a tip. Plus, better solder and flux. I have seen many videos on YouTube and they have one thing in common. Professionals looking for a professional outcome use a good quality soldering iron, solder and flux.

 

By the way, have you seen this series of soldering in avionics industry? Must see for everyone looking for a professional soldering result. https://www.youtube.com/watch?v=0SnOW2VdCTI . I don’t say all should do it this way, but it is worth knowing all the steps.

 

Here is my soldering. On the left is the thermometer PCB, on the right is a simple practice board bought for a few Euros. I highly recommend practicing after longer periods of not soldering.

 

image

image

As you can see, there is a jumper wire between the power connector and ground of the remaining board. I made an error concatenating signals, which was discovered after assembly image

 

And last, finalized assembly of version 1.

image

image

 

Did it work on the first power up? No – it took me a week to figure out I rotated the chip by 180 degrees. The chip has two circular markings at the edges and when I soldered the chip, I haven’t noticed it. The smaller one is the correct (and mentioned in the datasheet). Fun fact: according to the datasheet is the chip label irrelevant to the chip orientation.

Fortunately, I was able to remove the chip using a common hot air gun (not for soldering) and solder it again.

image

 

Did it work on the second power up? No – it took me another week to find a missing ground connection.

 

My takeaways

  • If the design software features a design rule check, use it. If I had used it properly, I wouldn’t have soldered the jumper wire between two different ground signals.
  • Use one size of components if possible. I mixed 1206 and 0805 resistors and capacitors. The less sizes, the better to maintain stock supplies.
  • Do not play with mirroring the components on the PCB. I mirrored two connectors (serial port and programming header) and then had to solder them from the other side to keep the layout as printed on solder mask. I was fortunate with this 2,54 mm header, but other connector types would mean a useless PCB.
  • Have a proper lightning and make sure all components are placed on the right places.

 

TO BE CONTINUED

 

David

  • Sign in to reply

Top Comments

  • fmilburn
    fmilburn over 8 years ago +5
    Hi David, that is fairly advanced for your first PCB and is looking quite nice. Frank
  • koudelad
    koudelad over 8 years ago +5
    Thanks to all of you for the kind words. Well, it is a first professionally manufactured PCB and the first made PCB after 15 years. I used the same program before to draw one or two PCBs when I was about…
  • shabaz
    shabaz over 8 years ago +4
    Hi David, That's really impressive. I can't recall my first PCB but I'm sure it must have been really bad. Also it is interesting to see the Melexis device being used - they make nice sensors, but they…
Parents
  • Marvian
    Marvian over 2 years ago

    Hi David, I am new to PSOC5 and I love this project and try to build it but I could not to read the IR, project files the google drive link does not work and I appreciate for sharing  the files.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • Marvian
    Marvian over 2 years ago

    Hi David, I am new to PSOC5 and I love this project and try to build it but I could not to read the IR, project files the google drive link does not work and I appreciate for sharing  the files.