Test Instrumentation
  • Challenges & Projects
  • Project14
  • Test Instrumentation
  • More
  • Cancel
Test Instrumentation
Blog Project PITS update
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Test Instrumentation to participate - click to join for free!
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: three-phase
  • Date Created: 2 Dec 2018 10:12 PM Date Created
  • Views 2757 views
  • Likes 8 likes
  • Comments 10 comments
  • mcgg relay
  • photodiode
  • current pickup
  • comparator
  • scits
  • diytestinstruch
Related
Recommended

Project PITS update

three-phase
three-phase
2 Dec 2018
image

Test Instrumentation

Enter Your Electronics & Design Project for a chance to win a Grand Prize for Originality, a Tool Set, and a $100 Shopping Cart!

Back to The Project14 homepage image

Project14 Home
Monthly Themes
Monthly Theme Poll

 

Project PITS has moved forward since the initial prototype was seen to work.

 

Since deciding that the best place for the on / off switch was between the charger and the boost circuit, the pre-manufactured board could not be utilised. The circuit has therefore been expanded utilising a MCP73831 charger integrated circuit from Microchip and a MC34063 for On Semiconductors to build up the boost circuit to convert the 3.7V from the 18650 cell to the required 5V.

 

image

 

image

This has created a much larger parts list as seen above, now giving a total parts cost of just over £75.00. The only major part missing from the cost now will be the cost of the PCB. Given the increase in components, the PCB has substantially changed but I have still managed to keep it within the case size.

 

Front Copper Layout

image

Rear Copper Layout

image

At the front, the board has been shortened to give room for the push button and 4 way socket that will be used to make connections to both the photodiode and the injection test set.

 

I am wondering If I should have a complete cutout of the copper around the whole of the battery positive clip as appose to just around the solder pads.

 

The battery clips themselves  have been positioned on the PCB utilising measurements from a manufactured battery holder, to get the correct tension on the spring clips. A couple of concerns are surrounding the connections to the USB socket and whether or not a copper track should be run up to the negative battery clip from this. I am also wondering if I should look at fusing  from the positive battery clip to the outgoing circuit and incoming from the charger. I am just wary of the power capability within the lithium ion cells and looking to prevent potential issues in the event of faults occurring.

 

image

 

Practically, not much has moved on. The 4 way connector and on / off switch have been mounted into the front of the case. I will need to drill holes for the LEDs and cut out for the USB connector, but this will not be done until I have a PCB to confirm the positioning.

 

imageimage

The next thing to do will be to order the required parts in and select someone to manufacture the PCB and ensure that I can generate the correct information that they require.

  • Sign in to reply

Top Comments

  • three-phase
    three-phase over 7 years ago +4
    I have now added a single 1A poly fuse to the battery positive connection. This pretty much completes the initial circuit. Over the weekend, I hope to set up the soft latch circuit and try it with the…
  • three-phase
    three-phase over 7 years ago in reply to three-phase +3
    Found the problem for the keep out area, The 'no copper pour' option is deselected by default, so selecting that removed the copper from the area.
  • genebren
    genebren over 7 years ago +3
    Donald, The updates to your project look great. The MCP73831 is a great choice for the Li Ion charging circuit. On the boost side, you could greatly simplify your circuit by using a boost convertor with…
Parents
  • genebren
    genebren over 7 years ago

    Donald,

     

    The updates to your project look great.  The MCP73831 is a great choice for the Li Ion charging circuit.  On the boost side, you could greatly simplify your circuit by using a boost convertor with an enable input.  I have used the PAM2401 part in some similar designs.  By using the enable pin, the circuit uses < 1uA of current when shut down.  Your switch could control the enable line and you would then not need the inline MOSFET (and associated circuitry) to turn off power to the boost.

     

    Gene

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • three-phase
    three-phase over 7 years ago in reply to genebren

    Many thanks for the information genebren, that looks like quite a useful device. Looks like it would need to come from Mouser or Digikey and not my regular suppliers in the UK.

     

    It would need some experimentation to see if it would work with the soft latching circuit I have, as I believe it works better with a bit of load and using it on the enable pin would reduce the load to it and it may oscillate. Would certainly reduce the number of components.

     

    I will perhaps look to redesign the circuit over the next couple of weeks and incorporate the latch device identified by shabaz in the previous blog.

     

    Kind regards.

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • genebren
    genebren over 7 years ago in reply to three-phase

    Donald,

     

    I had not fully understood  (and still don't) your soft latching circuit, but I suspect that you are correct in assuming that it might not work directly with the boost regulator.  What I have done in the past, is to use a pushbutton switch to wake up a microcontroller, which in turn can latch on the boost circuit.  I like this type of control, as I can sample the battery voltage and make a determination about if it is safe to continue operation, or if I should shutdown the boost circuit.  (see by write up on this topic Walky the Biped Robot - Power pack )  Once on, the pushbutton can be sampled to also shut down the circuit (microcontroller releases the enable signal).

     

    The PAM2401 is one of the few boost circuits that I have seen that have a true enable (I am sure that there are more, but it is difficult to search for these) that shuts down the boost circuit and isolates the output (no pass-through, i.e. input, through inductor/diode to output).

     

    If you decide to try this approach, I can send you a sample of the PAM2401 so you can try it out.

     

    Best of luck,

    Gene

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • genebren
    genebren over 7 years ago in reply to three-phase

    Donald,

     

    I had not fully understood  (and still don't) your soft latching circuit, but I suspect that you are correct in assuming that it might not work directly with the boost regulator.  What I have done in the past, is to use a pushbutton switch to wake up a microcontroller, which in turn can latch on the boost circuit.  I like this type of control, as I can sample the battery voltage and make a determination about if it is safe to continue operation, or if I should shutdown the boost circuit.  (see by write up on this topic Walky the Biped Robot - Power pack )  Once on, the pushbutton can be sampled to also shut down the circuit (microcontroller releases the enable signal).

     

    The PAM2401 is one of the few boost circuits that I have seen that have a true enable (I am sure that there are more, but it is difficult to search for these) that shuts down the boost circuit and isolates the output (no pass-through, i.e. input, through inductor/diode to output).

     

    If you decide to try this approach, I can send you a sample of the PAM2401 so you can try it out.

     

    Best of luck,

    Gene