Vision Thing
  • Challenges & Projects
  • Project14
  • Vision Thing
  • More
  • Cancel
Vision Thing
Forum Beaglebone Ai Heating Issues
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Vision Thing to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 124 replies
  • Subscribers 18 subscribers
  • Views 21490 views
  • Users 0 members are here
  • beagleboneai
  • beaglebone ai
  • BeagleBone
  • ai
  • beagleboard
Related

Beaglebone Ai Heating Issues

ipv1
ipv1 over 7 years ago

While experimenting with the device, I found that the board would shutdown without warning. The reasons is...

 

image

 

Now I tried a number of combos like us the USB tether, connect with display(yes I have the cursed microHDMI cable) and use standalone but every time, it just overheats if I do anything.

 

Idle temps are high too. Was wondering if I got a bad board or is it everyone?

  • Sign in to reply
  • Cancel

Top Replies

  • mudz
    mudz over 7 years ago +7
    After seeing all of you in so much trouble I decided - Why you should have all the fun so iI bought this kit too, to get into the same trouble pool.. After all, we all are community members. Cheers to…
  • tariq.ahmad
    tariq.ahmad over 7 years ago +6
    Hi ipv1 , I looked into this and this is a known issue: BeagleBone AI - Frequently Asked Questions (FAQ) They recommend adding a larger heat sink and cooling via fan.
  • 14rhb
    14rhb over 7 years ago in reply to 14rhb +6
    Hi shabaz - I've made a first prototype which seems to fit quite well. Packing out the top spacing by one extra washer was enough to get it to grip the existing heatsink fins. I'll make a bracket over…
  • clem57
    clem57 over 7 years ago in reply to 14rhb

    Wow! 14rhb that is industrial strength. I would call it a "heavy duty, harder than a Bone" Do you know what it weighs with that on it?

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Cancel
  • 14rhb
    14rhb over 7 years ago in reply to clem57

    Thank you image

     

    It's only aluminium and probably won't register on the kitchen scales but I'll have a go at weighing it.

     

    The downside will be not being able to use capes on this board.

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Cancel
  • cstanton
    cstanton over 7 years ago in reply to gdstew

    > And again, so far this is not even close to running it under full load

     

    Apparently the GUI environment runs by default on the BeagleBone AI, and disabling this helps the temperatures to subside somewhat.

     

     

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Cancel
  • cstanton
    cstanton over 7 years ago in reply to jomoenginer

    > The trick is to find that Cape Fan.  I have not been able to locate it.

     

    The official one is a couple of months away, so I'm told.

     

    Until then, mayermakes has been designing an add-on board image

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Cancel
  • cstanton
    cstanton over 7 years ago in reply to gdstew

    > luckily it will be a very small banshee.

     

    Seems appropriate for Halloween - Projects and Videos

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Cancel
  • mudz
    mudz over 7 years ago in reply to cstanton

    I was thinking of making one, when board arrives >>>

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • cstanton
    cstanton over 7 years ago in reply to shabaz

    > without the active cooling, it would throttle more, especially if it detects no cooling is attached

     

    I wish I could get my head around cpufreq a bit more to get a system service package to handle this, I would've perhaps hoped that one existed in debian to manage this for us already but I'm not certain/conviced, I think laptop-utils would/used to do something like this but perhaps not for ARM based controllers?

     

    This seems to be something which other boards manage to do, but I'm not sure of the intricacies of how. If anyone knows I think it'd be pretty useful for this board to work on it at least - or point me in the right direction, dabbling with linux is fun.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • shabaz
    shabaz over 7 years ago in reply to 14rhb

    Hi Rod,

     

    That should do it : ) Very cool look! Also, it looks like the end may be about 20mm square, so in theory you could even mount a fan sideways, to leave the slots visible and not covered by a fan.

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Cancel
  • mudz
    mudz over 7 years ago in reply to cstanton

    I'm convinced that this is a powerful processor with DSP cores similar to pc processor but smaller version (Didn't got hands on board yet). Surely it will heat up and demands similar active cooling like in pc's/laptops. You can try copper pipes and fan to transfer heat, setup will be bulky but you will be able to use Caps.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • 14rhb
    14rhb over 7 years ago in reply to shabaz

    Thank you. That is a very good idea - blowing the air through (towards the ethernet) will have a clearer flow than downwards. The end measures 15mm so it is still possible. I could also add two more fins on the outside of the stack.

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • Cancel
<>