• Products and Partners
    Products and Partners
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
Vision Thing
  • Challenges & Projects
  • Project14
  • Vision Thing
  • More
  • Cancel
Vision Thing
Documents Project14 | Vision Thing: Beaglebone AI Your Vision Thing Project!
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Vision Thing to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Engagement
  • Author Author: tariq.ahmad
  • Date Created: 9 Sep 2019 7:08 PM Date Created
  • Last Updated Last Updated: 5 Nov 2019 10:25 PM
  • Views 7430 views
  • Likes 12 likes
  • Comments 57 comments
Related
Recommended

Project14 | Vision Thing: Beaglebone AI Your Vision Thing Project!

image

Vision Thing

Enter Your Project for a chance to win an Oscilloscope Grand Prize Package for the Most Creative Vision Thing Project!

Back to The Project14 homepage image

Project14 Home
Monthly Themes
Monthly Theme Poll

 

 

In the Comments Below: Tell Us How You Would Use the BeagleBone AI for Your Vision Thing Project!

 

We'll Send Out Boards for Project Proposals that Use Them! 

 

 

image

 

You don't have permission to edit metadata of this video.
Edit media
x
image
Upload Preview
image

 

We are offering up to 20 FREE Beaglebone AI Boards in exchange for Vision Thing projects that use them!

 

Beaglebone AI Cooling Cape Addon Available from mayermakes:  BB AI cooling Addon board available

image
Buy NowBuy Now
We are offering up to 20 FREE Beaglebone AI Boards in exchange for Vision Thing projects that use them!

 

What is a Vision Thing project and how do you use the BeagleBone AI to do one?

 

There's a lot of variety with how you choose to implement your project.  It's a great opportunity to do something creative that stretches the imagination of what hardware can do.  Your project can be either a vision based project involving anything that is related to Computer Vision and Machine Learning , Camera Vision and AI based projects, Deep Learning, using hardware.  Or, it can be a graphics project involving something graphical such as adding a graphical display to a microcontroller, image processing on a microcontroller, image recognition interface a camera to a microcontroller,  or FPGA - camera interfacing/image processing/graphical display.

 

What makes the Beaglebone AI suitable for Vision Thing  Projects?

 

BeagleBone AI is a high-end board for developers building artificial-intelligence and computer-vision applications. Its main AI features include a Texas Instruments (TI) AM5729 system on chip (SoC), TI C66x digital-signal-processor (DSP) cores and embedded-vision-engine (EVE) cores. The board has the same form-factor as the popular and cheap BeagleBone Black but with much higher specifications.

 

  • It features a completely open source design: https://github.com/beagleboard/beaglebone-ai

 

The AI-ready board comes with 1GB RAM and 16GB on-board eMMC flash with a high-speed interface, a USB Type-C port for power and a dual-role controller, and a USB Type-A host. There's also Gigabit Ethernet and Wi-Fi. With preinstalled software, the BeagleBone AI also saves buyers from having to download equipment to get the device up and running.

image
The Most Creative Vision Thing Wins a Keysight DSOXO11G Oscilloscope!

Learn more by visiting:

  • BeagleBoneRegistered AI - Technical Specifications
  • BeagleBoneRegistered AI - Frequently Asked Questions (FAQ)
  • BeagleBoneRegistered Black, Blue, Wireless, Industrial, Green, AI Comparison Chart
  • BeagleBoneRegistered AI - Getting Started

So: what do you have to do to be in the running for one of the brand new Beagleboard AI? Just follow the instructions below!

 

1. Register and/or log-in to the element14 Community

2. Leave a comment on this post or on Project14 | Vision Thing: Build Things Using Graphics, AI, Computer Vision, & Beyond!  telling us what you'd like to build for your Vision Thing project with the new Beagleboard AI!

3.  Once you receive a new board submit your finished Vision Thing  project for a chance to win a Keysight DSOXO11G Oscilloscope!

 

 

The Most Promising Vision Thing Project Proposals Win a Free Beaglebone AI to Use In Your Vision Thing Project!

 

Submit Your Completed Project in Vision Thing  for a Chance to Win a Keysight DSOXO11G Oscilloscope!

  • image processing
  • competition
  • digital-signal processor
  • visionthingch
  • dsoxo11g oscillocope
  • keysight
  • soc
  • usb type-c
  • system on a chip
  • beaglebone ai
  • graphical display
  • emcc flash
  • image recognition
  • beaglebone ai vision thing
  • microcontroller
  • embedded-vision-engine
  • camera interfacing
  • Share
  • History
  • More
  • Cancel
  • Sign in to reply

Top Comments

  • dubbie
    dubbie over 7 years ago +5
    Having more-or-less decided on something for the Vision Thing based on Arduino and possibly Processing as well, I have just seen this opportunity to use the BeagleBone AI. Being mostly used to using Arduino…
  • Fred27
    Fred27 over 7 years ago +5
    A friend is heavily involved in canoe racing. Apparently the timing is a haphazard affair with people pressing stopwatches, writing down the number on the canoe, entering it into Excel, etc. It's fraught…
  • kk99
    kk99 over 7 years ago +3
    Few years ago I saw attempt to use neural networks for image classification for computer aided diagnosis (CAD) e.g. initial check for the presence of *** cancer on images.
Parents
  • mdombro
    mdombro over 7 years ago

    I have an idea of building an autonomous camera panning and zooming system. You would point the camera at an object you wish to track and then the system would try to always keep that object in the center of the frame. As the object moves the tracking algorithm would indicate how the camera needs to pan (up/down, left or right, how fast, etc) and then control signals for a gimbal could be generated. Additionally, the tracking algorithm could estimate the apparent size of the object, and direct an additional motor to control the zoom level of a camera to keep the object roughly the same size in the frame regardless of object range (within the limits of the lens zoom capability).

     

    The potential use cases could be keeping a camera on someone filming a video solo (like youtube vloggers), tracking race cars around a track, tracking radio control aircraft through its flight, or any situation where someone wants to film within a larger area but does not have a person who can man a camera.

     

    An additional goal of this system would be to allow various cameras to be used with it, rather than having a single camera built as part of the system. That way the user could select the camera body and lens type they desired depending on the conditions, but still have autonomous tracking capabilities. In other words, the user could place their own video camera onto the system, calibrate a few parameters, and now have an autonomous tracking system.

     

    The Beaglebone AI would be a perfect platform for this system with its coupling of computer vision capabilities and real-time programmable control. The Beaglebone AI would have the computational power to process video data and run a machine vision tracking algorithm, while also being able to generate the signals to control servos and brushless motors for the gimbaling system, all on a single board to reduce size, weight, and overall circuit complexity.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • clem57
    clem57 over 7 years ago in reply to mdombro

    This sounds familiar... Oh yes I saw this:
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
  • clem57
    clem57 over 7 years ago in reply to mdombro

    This sounds familiar... Oh yes I saw this: