• Products and Partners
    Products and Partners
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
Vision Thing
  • Challenges & Projects
  • Project14
  • Vision Thing
  • More
  • Cancel
Vision Thing
Documents Project14 | Vision Thing: Beaglebone AI Your Vision Thing Project!
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Vision Thing to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Engagement
  • Author Author: tariq.ahmad
  • Date Created: 9 Sep 2019 7:08 PM Date Created
  • Last Updated Last Updated: 5 Nov 2019 10:25 PM
  • Views 7425 views
  • Likes 12 likes
  • Comments 57 comments
Related
Recommended

Project14 | Vision Thing: Beaglebone AI Your Vision Thing Project!

image

Vision Thing

Enter Your Project for a chance to win an Oscilloscope Grand Prize Package for the Most Creative Vision Thing Project!

Back to The Project14 homepage image

Project14 Home
Monthly Themes
Monthly Theme Poll

 

 

In the Comments Below: Tell Us How You Would Use the BeagleBone AI for Your Vision Thing Project!

 

We'll Send Out Boards for Project Proposals that Use Them! 

 

 

image

 

You don't have permission to edit metadata of this video.
Edit media
x
image
Upload Preview
image

 

We are offering up to 20 FREE Beaglebone AI Boards in exchange for Vision Thing projects that use them!

 

Beaglebone AI Cooling Cape Addon Available from mayermakes:  BB AI cooling Addon board available

image
Buy NowBuy Now
We are offering up to 20 FREE Beaglebone AI Boards in exchange for Vision Thing projects that use them!

 

What is a Vision Thing project and how do you use the BeagleBone AI to do one?

 

There's a lot of variety with how you choose to implement your project.  It's a great opportunity to do something creative that stretches the imagination of what hardware can do.  Your project can be either a vision based project involving anything that is related to Computer Vision and Machine Learning , Camera Vision and AI based projects, Deep Learning, using hardware.  Or, it can be a graphics project involving something graphical such as adding a graphical display to a microcontroller, image processing on a microcontroller, image recognition interface a camera to a microcontroller,  or FPGA - camera interfacing/image processing/graphical display.

 

What makes the Beaglebone AI suitable for Vision Thing  Projects?

 

BeagleBone AI is a high-end board for developers building artificial-intelligence and computer-vision applications. Its main AI features include a Texas Instruments (TI) AM5729 system on chip (SoC), TI C66x digital-signal-processor (DSP) cores and embedded-vision-engine (EVE) cores. The board has the same form-factor as the popular and cheap BeagleBone Black but with much higher specifications.

 

  • It features a completely open source design: https://github.com/beagleboard/beaglebone-ai

 

The AI-ready board comes with 1GB RAM and 16GB on-board eMMC flash with a high-speed interface, a USB Type-C port for power and a dual-role controller, and a USB Type-A host. There's also Gigabit Ethernet and Wi-Fi. With preinstalled software, the BeagleBone AI also saves buyers from having to download equipment to get the device up and running.

image
The Most Creative Vision Thing Wins a Keysight DSOXO11G Oscilloscope!

Learn more by visiting:

  • BeagleBoneRegistered AI - Technical Specifications
  • BeagleBoneRegistered AI - Frequently Asked Questions (FAQ)
  • BeagleBoneRegistered Black, Blue, Wireless, Industrial, Green, AI Comparison Chart
  • BeagleBoneRegistered AI - Getting Started

So: what do you have to do to be in the running for one of the brand new Beagleboard AI? Just follow the instructions below!

 

1. Register and/or log-in to the element14 Community

2. Leave a comment on this post or on Project14 | Vision Thing: Build Things Using Graphics, AI, Computer Vision, & Beyond!  telling us what you'd like to build for your Vision Thing project with the new Beagleboard AI!

3.  Once you receive a new board submit your finished Vision Thing  project for a chance to win a Keysight DSOXO11G Oscilloscope!

 

 

The Most Promising Vision Thing Project Proposals Win a Free Beaglebone AI to Use In Your Vision Thing Project!

 

Submit Your Completed Project in Vision Thing  for a Chance to Win a Keysight DSOXO11G Oscilloscope!

  • image processing
  • competition
  • digital-signal processor
  • visionthingch
  • dsoxo11g oscillocope
  • keysight
  • soc
  • usb type-c
  • system on a chip
  • beaglebone ai
  • graphical display
  • emcc flash
  • image recognition
  • beaglebone ai vision thing
  • microcontroller
  • embedded-vision-engine
  • camera interfacing
  • Share
  • History
  • More
  • Cancel
  • Sign in to reply

Top Comments

  • dubbie
    dubbie over 7 years ago +5
    Having more-or-less decided on something for the Vision Thing based on Arduino and possibly Processing as well, I have just seen this opportunity to use the BeagleBone AI. Being mostly used to using Arduino…
  • Fred27
    Fred27 over 7 years ago +5
    A friend is heavily involved in canoe racing. Apparently the timing is a haphazard affair with people pressing stopwatches, writing down the number on the canoe, entering it into Excel, etc. It's fraught…
  • kk99
    kk99 over 7 years ago +3
    Few years ago I saw attempt to use neural networks for image classification for computer aided diagnosis (CAD) e.g. initial check for the presence of *** cancer on images.
Parents
  • bt_jac
    bt_jac over 7 years ago

    The BeagleBone AI board fits perfecly into a project I've been working on for a while - smart parking assistant. The goal of this project is to create a device which helps drivers to park their cars in a safe and convenient way. There are several ways to achieve this goal - the easiest and the cheapest ones are the ultrasonic sensors. More complicated and more expensive are parking cameras. Both solutions have their advantages - but they don't fulfill all my expectations towards such systems. The main disadvantage is that they are not able to detect incoming pedestrians and cyclist who are not in their detection area - and such persons can appear from nowhere in just a second. Another weak point is unability to detect curbs - especially those lower ones - and small obstacles that lay on a path of a car.

    The solution here seems to be AI - especially taking into account the latest achievments in this area. The device I'm trying to build will have the following configuration:

    - two webcameras located behind the rear window of a car (it allows measuring range to obstacles) - they should have wide detection area - to find incoming threats like pedestrians mentioned above

    - main computer responsible for analysing images taken by both cameras (in this role - BeagleBone AI)

    - driver's smartphone which receives data from the main computer via WiFi

    - accelerometer - to detect direction of a car - as I'm not going to change anything in car's instalation - inlcuding connecting devices to rear lights

    - IR lamp + light sensor - to illuminate an area in the night

    Such configuration should allow the device to:

    - detect pedestrians and cyclists closing to a car - and give an information about a potential collision (based on a distance, speed, direction and type of an incoming object)

    - detect and classify small obstacles in the back of the car and warn driver in case when they can be a potentail threat (bottles, sharp rocks etc.)

    - measure whether there is enough place to park a car there

    - check, whether a car is parked in line with any markings on a road

    To implement all those features I plan to use TF library (classification and detection of objects) together with OpenCV (measuring range, detection of edges). Additionaly - but rather as a second step - I was thinking about adding handling a voice/sound messages - to inform/warn a user not only with a message/image displayed on a screen of a smartphone - but also through speakers connected to the main computer.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • bt_jac
    bt_jac over 7 years ago

    The BeagleBone AI board fits perfecly into a project I've been working on for a while - smart parking assistant. The goal of this project is to create a device which helps drivers to park their cars in a safe and convenient way. There are several ways to achieve this goal - the easiest and the cheapest ones are the ultrasonic sensors. More complicated and more expensive are parking cameras. Both solutions have their advantages - but they don't fulfill all my expectations towards such systems. The main disadvantage is that they are not able to detect incoming pedestrians and cyclist who are not in their detection area - and such persons can appear from nowhere in just a second. Another weak point is unability to detect curbs - especially those lower ones - and small obstacles that lay on a path of a car.

    The solution here seems to be AI - especially taking into account the latest achievments in this area. The device I'm trying to build will have the following configuration:

    - two webcameras located behind the rear window of a car (it allows measuring range to obstacles) - they should have wide detection area - to find incoming threats like pedestrians mentioned above

    - main computer responsible for analysing images taken by both cameras (in this role - BeagleBone AI)

    - driver's smartphone which receives data from the main computer via WiFi

    - accelerometer - to detect direction of a car - as I'm not going to change anything in car's instalation - inlcuding connecting devices to rear lights

    - IR lamp + light sensor - to illuminate an area in the night

    Such configuration should allow the device to:

    - detect pedestrians and cyclists closing to a car - and give an information about a potential collision (based on a distance, speed, direction and type of an incoming object)

    - detect and classify small obstacles in the back of the car and warn driver in case when they can be a potentail threat (bottles, sharp rocks etc.)

    - measure whether there is enough place to park a car there

    - check, whether a car is parked in line with any markings on a road

    To implement all those features I plan to use TF library (classification and detection of objects) together with OpenCV (measuring range, detection of edges). Additionaly - but rather as a second step - I was thinking about adding handling a voice/sound messages - to inform/warn a user not only with a message/image displayed on a screen of a smartphone - but also through speakers connected to the main computer.