microbit
  • Learn
  • Learning Center
  • STEM Academy
  • microbit
  • More
  • Cancel
microbit
micro:bit Blog 10 BBC micro:bit Projects in 10 Days: Day Four - Camera Time
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join microbit to participate - click to join for free!
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: jlucas
  • Date Created: 3 Jun 2016 11:38 AM Date Created
  • Views 5921 views
  • Likes 20 likes
  • Comments 5 comments
  • micro:bit
  • bbc micro:bit
  • microbit
  • beginner micro:bit projects
  • bbc microbit
  • ten bbc micro:bit projects
  • beginner_microbit_projects
  • bbc_micro:bit
  • 10projects10days
Related
Recommended

10 BBC micro:bit Projects in 10 Days: Day Four - Camera Time

jlucas
jlucas
3 Jun 2016

About this project

 

This project introduces the BBC micro:bit's camera functionality, allowing users to take a timed photo using the device.

 

What you'll need

 

1 x BBC micro:bit

1 x Micro USB

1 x Computer or tablet

2 x AAA Batteries & Battery Holder

 

Project walkthrough

 

  • Go to the BBC micro:bit website, click 'create code' and begin a new Microsoft Block Editor project.

 

  • Under the left-hand commands menu, click 'Input' and find the 'On button [A] pressed do...' tile.

 

  • We want to tell the device to take a photograph when the 'A' button is pressed. However, we also want to add in a five second delay to allow us to set up the shot. To enable the camera, select 'Devices' from the left-hand menu, and drag in the tile 'Tell camera to [take photo]. Attach to your 'On button [A] pressed do...' tile, and change [take photo] to [launch photo mode].

 

image

  • To set up a countdown timer, drag in a 'set [item] to tile, and rename [item] to [counter].

 

  • Attach a number tile from the 'Maths' menu, and set it to [5].

 

image

  • Now we need to tell the timer to start counting down when the A button is pressed. This is a slightly different process to the last time we created a countdown timer (see Project Two). First you'll need to bring in a tile entitled 'for [i] from 0 to [4] do...' and attach it to your code. This tile can be found in the loops menu.

 

  • In this tile, the [i] simply represents the variable being referenced in the code - in this case, the countdown timer. Feel free to change the name to something that makes more sense to you, but don't use 'counter' as we've already used this as a variable in this code. I've used 'Countdown' in this demo. Also, change the [4] to a [5] to bring it in line with your five second countdown timer.

 

image

  • Under 'do', drag in a 'show number' tile from the 'Basic' menu, and drag a 'counter' tile from the Variables menu into the input box.

 

  • Now drag in a 'change [item] by [1]' tile, also from the Variables menu, change [item] to [counter] and change [1] to [-1], to instruct the timer to count backwards from 5.

 

  • Finally, drag in another 'Tell camera to [take photo]' tile from the devices menu, and attach this at the bottom, as indicated here:

 

image

  • Now hit 'Run' to test out your script on the emulator. When you push the 'A' button the counter should begin counting down from 5 to 0. At zero, the device should take a photo. Compile your script and transfer it to your BBC micro:bit device to test it out for real. You can access your photos from the BBC micro:bit drive when you attach the device to your computer.

 

Once students have mastered this project, what else can they do with the BBC micro:bit camera functionality? Encourage them to play around with different commands and techniques, and let us know how they get on in the comments section below...

  • Sign in to reply

Top Comments

  • zenandy
    zenandy over 10 years ago +6
    It would help to specify the requirements for a smartphone here. The Micro:bit doesn't have an onboard camera.
  • shabaz
    shabaz over 10 years ago +3
    It looks like this uses the Bluetooth and BLE capabilities of the micro:bit. I'm no expert, but there are dozens/hundreds? of profiles for doing different things, and one of them is for camera control…
  • volly
    volly over 10 years ago +2
    Like Andy says. Please clarify the fact that the micro:bit does not come with any onboard peripherals like speakers, cameras, etc. It would also be a good thing to add instructions on how exactly to attach…
Parents
  • volly
    volly over 10 years ago

    Like Andy says. Please clarify the fact that the micro:bit does not come with any onboard peripherals like speakers, cameras, etc. It would also be a good thing to add instructions on how exactly to attach these specific devices....

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • volly
    volly over 10 years ago

    Like Andy says. Please clarify the fact that the micro:bit does not come with any onboard peripherals like speakers, cameras, etc. It would also be a good thing to add instructions on how exactly to attach these specific devices....