microbit
  • Learn
  • Learning Center
  • STEM Academy
  • microbit
  • More
  • Cancel
microbit
micro:bit Blog 10 BBC micro:bit Projects in 10 Days: Day Seven - Roll the Dice
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join microbit to participate - click to join for free!
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: jlucas
  • Date Created: 3 Jun 2016 11:44 AM Date Created
  • Views 5430 views
  • Likes 20 likes
  • Comments 9 comments
  • micro:bit
  • bbc micro:bit
  • microbit
  • beginner micro:bit projects
  • bbc microbit
  • ten bbc micro:bit projects
  • beginner_microbit_projects
  • bbc_micro:bit
  • 10projects10days
Related
Recommended

10 BBC micro:bit Projects in 10 Days: Day Seven - Roll the Dice

jlucas
jlucas
3 Jun 2016

About this project

 

This project turns the BBC micro:bit into an electronic dice, programming the device to display a random number from 1-6 on the LED array when shaken.

 

What you'll need

 

1 x BBC micro:bit

1 x Micro USB

1 x Computer or tablet

2 x AAA Batteries & Battery Holder

 

Project walkthrough

 

  • Go to the BBC micro:bit website, click 'create code' and begin a new Microsoft Block Editor project.

 

  • From the Input commands menu, drag in an 'if [shake] do' tile.

 

  • When the device is shaken, we want it to display a random number from 1-6. To do this, first we need to create a new variable.

 

  • Attach a 'set [item]' tile, and rename the variable to 'roll'.

 

  • Now go to the Math command menu and attach a 'pick random [0] to [4]' tile. Change the figure in the dialog box to 5, like so:

 

image

  • Because the roll has a range of 0-5 rather than 1-6, we have to tell the device to show the number one when it rolls a zero, the number two when it rolls a one, and so on.

 

  • Drag in an 'if/do' tile and, for 'if', attach a '[0] = [0]' tile from the logic menu. Drag a 'roll' variable into the left dialogue box.

 

  • For 'do', attach a 'show leds' tile and set it to display the 'one' side of a standard dice by lighting up a single bulb at the co-ordinate 2/2.

 

image

 

  • Click on the blue cog symbol in your 'if/do' tile and add an 'else if/do' option.

 

  • Use this to program your BBC micro:bit to display the 'two' side of the dice when the device rolls a one.

 

image

 

  • Using more 'else/if' and 'else' tiles, repeat the steps above so that when the roll is 2, 3, 4 5, the device shows a 3, 4, 5 and 6 dice side respectively.

image

image

  • You're done! Run your program to test it in the right-hand emulator, then click compile to download the script and transfer it to your BBC micro:bit.

 

When your students have mastered this project, what else can they do with the random command? Challenge them to develop different projects using the LED array, such as a dice that displays images rather than numbers, or a 'trick dice' that only rolls even numbers. Let us know what they come up with in the comments section below...

  • Sign in to reply

Top Comments

  • volly
    volly over 9 years ago in reply to vandia +3
    vandia https://www.youtube.com/watch?v=WK8jhupl7r0
  • volly
    volly over 9 years ago in reply to vandia +3
    vandia Shake Dice in Action: https://www.youtube.com/watch?v=1-Rdz9tb2bg
  • balearicdynamics
    balearicdynamics over 10 years ago +2
    Something that seems not yet noted ... The value added of this example is just Dice ... It sounds to me as random that is not a so obvious but useful feature in micro-controller small devices Enrico
Parents
  • vandia
    vandia over 9 years ago

    Would love to see a photo of the actual outcome on a working unit!

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • vandia
    vandia over 9 years ago

    Would love to see a photo of the actual outcome on a working unit!

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
Children
  • volly
    volly over 9 years ago in reply to vandia

    vandia

     

    https://www.youtube.com/watch?v=WK8jhupl7r0

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • vandia
    vandia over 9 years ago in reply to volly

    Thanks.... good to see an actual unit working lol.
    My computer lagged during the video, but it didn't show the dice thing, did it? I was curious about a die-rolling animation on it lol.

     

    Also, what do you call a platform like that, with LEDs in a square, if I wanted to connect and control it with another device? I need one a good few inches wide, lol. Any ideas?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • volly
    volly over 9 years ago in reply to vandia

    vandia

     

    Shake Dice in Action:

     

    https://www.youtube.com/watch?v=1-Rdz9tb2bg

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • vandia
    vandia over 9 years ago in reply to volly

    Thanks! ...if I get one, I may want to do a shaking animation on the screen when you're shaking it!
    Or, anyone else is free to give it a try! lol