microbit
  • Learn
  • Learning Center
  • STEM Academy
  • microbit
  • More
  • Cancel
microbit
micro:bit Blog [PROJECT] BBC Micro:bit – LED Panel Effects Controller – version 1 by Cabe
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join microbit to participate - click to join for free!
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: Catwell
  • Date Created: 31 Oct 2019 7:31 PM Date Created
  • Views 3812 views
  • Likes 8 likes
  • Comments 1 comment
  • project
  • microbit
  • diy
  • addressable leds
  • cabeatwell
  • led controller
Related
Recommended

[PROJECT] BBC Micro:bit – LED Panel Effects Controller – version 1 by Cabe

Catwell
Catwell
31 Oct 2019

image

I activated one effect in this section of the LED panel. (via ME)

 

I will admit, I could not expand the memory much with the Micro:bit for the last project. So, before I explore memory expansion, I thought I would see what else I could do with the 8x8 LED grid panel.

Although the LED panel is simply a reconfiguration of an addressable LED strip, but I wanted it to act like a screen. So, when the keypad is pressed, I wanted effects to correlate with the buttons. So, in this version I wanted to do splash effects at those points.

 

The software works as follows:

- Power it up.

- Immediately press buttons to light up the LED panel in relation to the keypad.

    

First, let’s gather all the necessary components you’ll need to build this project.

1x BBC Micro:bit

1x Kitronik Inventor’s Kit

1x Addressable LED panel

1x 16 button matrix keypad

 

Video demonstration of the project:

You don't have permission to edit metadata of this video.
Edit media
x
image
Upload Preview
image

 

STEP 1

Load the code onto the Micro:bit.

I am providing the hex file you need to drag and drop onto the Micro:bit, and the python code as two separate files. For the below process, just use the hex file.

Plug the MicroUSB cable into the Micro:bit, and plug the other end of the cable to a PC or MAC.

At this point, you are going to copy over the code to the Micro:bit. I am providing the program (code) in this post that needs to be copied over. When the Micro:bit plugs into a computer, it shows up as a USB flash drive. All you have to do is copy the file over to the Micro:bit, like it’s a USB Flash Drive, and the Micro:bit will reset, and the program is active.

You can remove the Micro:bit from the computer at this point. The program will start running, and without the rest of the circuit, it will not function.

●

A little bit about the code:

 

STEP 2

The schematic is fairly straight forward. It’s also the same as the last project. Wire it up like the drawing.

image

STEP 3

Setup

The software works as follows:

- Power it up.

- Immediately press buttons to light up the LED panel in relation to the keypad.

 

Conclusion:

Speed of the Micro:bit is a huge drawback to this project. It can display the effects, but it’s very choppy. I will have to explore how to make this happen a bit faster. Easiest thing I could do is offload the LED control to an Arduino. Then I could swap in Micro:bit boards like cartridges for different effects. Maybe…

Attachments:
Microbit 2019 10 30 LED Panel Effects Controller.zip
  • Sign in to reply

Top Comments

  • dubbie
    dubbie over 6 years ago +2
    Some interesting effects. I might try something similar with the 8x8 LED display I have. It updates much faster. Dubbie
Parents
  • dubbie
    dubbie over 6 years ago

    Some interesting effects. I might try something similar with the 8x8 LED display I have. It updates much faster.

     

    Dubbie

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • dubbie
    dubbie over 6 years ago

    Some interesting effects. I might try something similar with the 8x8 LED display I have. It updates much faster.

     

    Dubbie