Member and Staff Blogs Frequency-To-Voltage Converter With An Analog Discovery 3
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Leaderboard
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Community Hub to participate - click to join for free!
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: dougw
  • Date Created: 28 Jan 2024 1:00 AM Date Created
  • Views 3563 views
  • Likes 12 likes
  • Comments 1 comment
  • dougw
  • LM2907
  • Digilent Analog Discovery 3
  • frequency to voltage converter
Related
Recommended

Frequency-To-Voltage Converter With An Analog Discovery 3

dougw
dougw
28 Jan 2024

Intro

As part of the Analog Discovery 3 road test, I want to show examples of using both its waveform generator and its oscilloscope at the same time with a real circuit.

This example uses an TI LM2907 (developed by National Instruments before they were acquired by TI) frequency-to-voltage converter chip. I used the Digilent AD3 to generate various frequencies for the circuit to convert to voltages, actually I used the sweep function of the AD3 to continuously sweep the frequency from 5 Hz to 1 KHz.

I also wanted to see what the frequency response of the circuit is. To do this I created a step change in frequency to see how long the circuit takes to respond. Then I increased the modulation frequency until the circuit's response decreased to 50% of its maximum amplitude. This gave a measure of the circuits bandwidth to measure frequency changes.

F to V Circuit Demo

You don't have permission to edit metadata of this video.
Edit media
x
image
Upload Preview
image

Schematic

image

VO = VCC × fIN × C2 × R1 × K

This formula indicates the output voltage is proportional to both capacitance and frequency, so if C2 is constant the output is proportional to the input frequency and if the frequency is constant, the output is proportional to C2.

Discussion

The Analog Discovery 3 Is very useful in experimenting with circuits like this where the circuit may need a variable frequency input and you want to see the waveforms at various places in the circuit.

The user interface is different from other instruments and there are many features to understand, but adjusting settings with a mouse and keyboard is quick and easy. Finding the bandwidth of an analog frequency to voltage converter like this could be quite an exercise with traditional instrumentation, but with the AD3 it can all be done with one instrument.

Links:

AD3 Unboxing

Pretty Cool Raster Text Display on an AD3

AD3 Enclosure

AD# - Frequency-to-Voltage Converter

AD3 - Capacitance-to-Voltage Converter

Digilent Analog Discovery 3 Road Test

Digilent Analog Discovery 3 Specifications

LM2907 Datasheet

  • Sign in to reply
  • DAB
    DAB over 2 years ago

    Very interesting demo.

    The Discovery Kit has some very useful features.