Member and Staff Blogs Simple Passive Component V-I Curve Tracer
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Leaderboard
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Community Hub to participate - click to join for free!
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: fmilburn
  • Date Created: 1 May 2022 3:43 AM Date Created
  • Views 15857 views
  • Likes 12 likes
  • Comments 12 comments
  • capacitor
  • curve tracer
  • V-I Curve
  • diode
  • waveform generator
  • oscilloscope
  • led
  • function generator
  • resistor
Related
Recommended

Simple Passive Component V-I Curve Tracer

fmilburn
fmilburn
1 May 2022

If you are like me you don't use the XY plot function on your oscilloscope often but it can be handy at times.  I was reviewing videos by W2AEW on YouTube and saw this one where he describes a simple method for viewing components using only a waveform generator and an oscilloscope.  The short (less than 3 minutes) video below demonstrates how it works.

You don't have permission to edit metadata of this video.
Edit media
x
image
Upload Preview
image

The setup is quite simple.

Simple V-I Curve Tracer

The function generator produces a triangular waveform across the DUT which is in series with a shunt resistor used to measure current.  The oscilloscope in XY mode has the X-axis set to measure the voltage across the DUT while the current is displayed on the Y-axis.  There is a problem with this setup, however.  The X-axis probe is measuring the voltage across both the DUT and the shunt resistor.  This can be acceptable if the voltage drop across the shunt resistor is small.  Some oscilloscopes allow the math function to be used in XY mode so that the voltage across the shunt resistor can be subtracted from the DUT reading.  Mine does not.  Other approaches would be to use a differential probe for the DUT or a current sensing probe for the current.

My oscilloscope is a Keysight DSO-X 1102G which has a built-in waveform generator.  The waveform generator was set to 50-ohm output with a 3V p-p symmetric triangle wave.  To get a clean trace the acquire mode on the oscilloscope has been set to high resolution.

The screenshot below shows a red LED under test.

Red LED Under Test

Thanks for reading and comments are always welcome!

  • Sign in to reply

Top Comments

  • Andrew J
    Andrew J over 4 years ago +1
    I thought the quality was good. In fact, I actually thought the embedded video was from W2AEW and I spent some minutes scratching my head working out why your comment made no sense!! Great post.
  • fmilburn
    fmilburn over 4 years ago in reply to beacon_dave +1
    Thanks, I've corrected the typo. That is a good point about 50Ω output mode. I may remake the video when I get my new microphone - don't want to add any more confusion to the internet than is already out…
Parents
  • fmilburn
    fmilburn over 4 years ago

    The real reason for this post is that I've decided my videos aren't that good so I've downloaded ShotCut, an open-source video editing program, and I am learning to use it.  This is my first attempt.  There are pops at the start of the inserted audio - I think I need to let it run a bit before starting to talk and then edit that out.  I'm pretty sure the problem is the software.  If not that, then it must be the camera and I need to buy a new one.  It can't be me :-)

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • Jan Cumps
    Jan Cumps over 4 years ago in reply to fmilburn

    I think the video quality is very good. The audio quality could use a bit of love. Not the voice, but the sound. There's echo in the room and some sort of distortion (do you use a software noise reduction? If yes, I can hear the artifacts of it)

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • Jan Cumps
    Jan Cumps over 4 years ago in reply to fmilburn

    I think the video quality is very good. The audio quality could use a bit of love. Not the voice, but the sound. There's echo in the room and some sort of distortion (do you use a software noise reduction? If yes, I can hear the artifacts of it)

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
Children
  • fmilburn
    fmilburn over 4 years ago in reply to Jan Cumps

    After listening to it again this morning I agree with your comment on audio quality.  The room I'm in is large and reflective.  I'm using the microphone on my laptop computer without noise reduction.  The computer is located behind and to the side of a monitor and turning my head blocks sound and changes the volume.  The spaces between the sound clips that were edited into the video are also evident.  I'm going to buy an external microphone and see how that works.