Browse By Tags

  • Winners Announcement - Holidays Competition 2024

    It’s time! As we saw in last week’s wrap-up , we have had so many fantastic holiday-themed submissions, but there can only be one winner…and a second place winner and five runner-ups Just as a quick reminder, let’s look back at the competition theme.…
  • Holidays Competition Announcement ☃︎

    The Holidays competition is over for now - but tune back in during winter 2025 for another festive challenge! Check out 2024's winners for inspiration in the official announcement here . It is the most wonderful time of the year! Season's greetings…
  • Welcome Analog Discovery 3! another pocket but powerful digital oscilloscope

     Analog Discovery 3:  14-bit 125 MS/s USB Oscilloscope,

    Function Generator, Logic Analyzer, Pattern Generator,

    and Variable Power Supply

                              

    Invitation

    At the very beginning I would like to THANK very much to Element14 and Digilent for the trust and...

  • Multicomp Pro MP750511 Arbitrary Waveform Generator

    We need two Electronic Engineers to create a short video on how to use an arbitrary waveform generator in return we'll let you keep the test equipment for FREE.

    About the Mulitcomp Pro RoadTest Fundamentals Series

    This RoadTest is a part of our Fundamentals...

  • Terms and Conditions for Multicomp Pro - Applications of Waveform Generators

    Multicomp Pro - Applications of Waveform Generators Terms and Conditions These are the terms and conditions which govern the Multicomp Pro MP750511 Waveform Generator RoadTest. This Contest requires participants to submit an application indicating…
  • Simple Passive Component V-I Curve Tracer

    If you are like me you don't use the XY plot function on your oscilloscope often but it can be handy at times. I was reviewing videos by W2AEW on YouTube and saw this one where he describes a simple method for viewing components using only a waveform…
  • Review: EDU33212A 2-channel Arbitrary Waveform Generator

    EDU33212A Waveform Generator Review - John Porter The Keysight EDU33212A Waveform Generator adds advanced signal generation to the Keysight Smart Bench Essentials series. The EDU33212A is easy for students to use and get started, however has many…
  • Keysight Smart Bench Essentials Review

    Keysight Smart Bench Essentials Review - John Porter

    Are you looking for a set of modern, feature-packed, coordinated instruments for your bench? Keysight’s Smart Bench Essentials (SBE) provides a complete solution of four essential devices, each...

  • Digilent ADP3450 In-Depth – Ch7: Using the ADP3450 in Various Applications

    In this blog post, I put the Digilent Analog Discovery Pro ADP3450 into various applications. Lissajous Waveform Generation Having access to two waveform generator channels and two oscilloscope channels naturally leads to the temptation to generate…
  • Digilent ADP3450 In-Depth – Ch4: Tour of Digilent WaveForms

    In this chapter, I will look more into detail of each of the modules within the Digilent WaveForms application, while also providing some insight into the user experience of using the ADP3450 in these modes. Digilent WaveForms Tour & User Experience…
  • Digilent ADP3450 In-Depth – Ch8: Instrument Performance Tests

    This chapter will cover a number of instrument performance tests that I conducted to ascertain the capability of the instrument and verify its specifications compared to its datasheet. This is perhaps the most exciting part of the review, not least because…
  • Digilent ADP3450 In-Depth – Ch1: Market Survey & Feature Introduction

    In this blog, I will be looking at the Digilent Analog Discovery Pro ADP3450 and how it compares with other products on the market. I will also be looking at what is unique about the ADP3450 and who it might appeal to. Feature Introduction The Digilent…
  • Digilent ADP3450 In-Depth – Ch3: Setup of Waveforms & Documentation

    This blog posting will consider the initial set-up procedure for the hardware and software, while also evaluating the support and documentation provided. Obtaining Software To actually run the ADP3450, you will need to download the WaveForms software…
  • Digilent ADP3450 In-Depth – Ch2: Unboxing

    This blog post is dedicated to the unboxing of the Digilent Analog Discovery Pro ADP3450 Mixed Signal Oscilloscope, featuring images of the unit and included probes for the RoadTest. Unboxing The ADP3450 arrived in a surprisingly large box – about…
  • Digilent ADP3450 In-Depth – Ch5: Linux Mode, LAN & Wi-Fi Connectivity

    One of the most interesting features of the Digilent Analog Discovery Pro ADP3450 is the Linux Mode for embedded development. This represents a bit of a paradigm shift in USB test instruments – no longer are they just following the commands of a remotely…
  • Streaming data from a portable mixed-signal oscilloscope

    This project will show you how to stream data and control the Digilent Analog Discovery Pro Digilent Analog Discovery Pro (ADP3450/ADP3250) remotely. There are 2 ways to establish the connection, using Standard Mode and Linux Mode, to communicate with…
  • The Origins of Delayed Timings on Oscilloscopes - Workbench Wednesdays 43

    You don't have permission to edit metadata of this video. Edit media Dimensions x Small Medium Large Custom Subject (required) Brief Description…
  • "Keysight Wave" is Back!

    to Coordinated Universal Time
    Keysight Technologies
    It's finally here! Wave 2019 is happening now. Wondering what it's all about? This online event for engineers features massive giveaways and tips & tricks designed to make you an engineering legend. Tune in to the Keysight Labs YouTube Channel and the...
  • Build and Measure Signals and Systems on Electronics Explorer

    The Digilent Electronics Explorer Electronics Explorer includes all of the test and measurement equipment needed to design, build, and test analog and digital circuits of all types. Built around a large solderless breadboard, the Electronics Explorer…
  • Use Analog Discovery 2 to create harmonics and look at its spectrum

    This post shows how to create harmonics in a specific signal with the Analog Discovery 2 Analog Discovery 2 and look at the spectrum through FFT mode . We will use the Oscilloscope and Waveform / Signal Generator instruments in Analog Discovery 2. Basic…