Member and Staff Blogs Simple Passive Component V-I Curve Tracer
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Leaderboard
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Community Hub to participate - click to join for free!
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: fmilburn
  • Date Created: 1 May 2022 3:43 AM Date Created
  • Views 15837 views
  • Likes 12 likes
  • Comments 12 comments
  • capacitor
  • curve tracer
  • V-I Curve
  • diode
  • waveform generator
  • oscilloscope
  • led
  • function generator
  • resistor
Related
Recommended

Simple Passive Component V-I Curve Tracer

fmilburn
fmilburn
1 May 2022

If you are like me you don't use the XY plot function on your oscilloscope often but it can be handy at times.  I was reviewing videos by W2AEW on YouTube and saw this one where he describes a simple method for viewing components using only a waveform generator and an oscilloscope.  The short (less than 3 minutes) video below demonstrates how it works.

You don't have permission to edit metadata of this video.
Edit media
x
image
Upload Preview
image

The setup is quite simple.

Simple V-I Curve Tracer

The function generator produces a triangular waveform across the DUT which is in series with a shunt resistor used to measure current.  The oscilloscope in XY mode has the X-axis set to measure the voltage across the DUT while the current is displayed on the Y-axis.  There is a problem with this setup, however.  The X-axis probe is measuring the voltage across both the DUT and the shunt resistor.  This can be acceptable if the voltage drop across the shunt resistor is small.  Some oscilloscopes allow the math function to be used in XY mode so that the voltage across the shunt resistor can be subtracted from the DUT reading.  Mine does not.  Other approaches would be to use a differential probe for the DUT or a current sensing probe for the current.

My oscilloscope is a Keysight DSO-X 1102G which has a built-in waveform generator.  The waveform generator was set to 50-ohm output with a 3V p-p symmetric triangle wave.  To get a clean trace the acquire mode on the oscilloscope has been set to high resolution.

The screenshot below shows a red LED under test.

Red LED Under Test

Thanks for reading and comments are always welcome!

  • Sign in to reply

Top Comments

  • Andrew J
    Andrew J over 4 years ago +1
    I thought the quality was good. In fact, I actually thought the embedded video was from W2AEW and I spent some minutes scratching my head working out why your comment made no sense!! Great post.
  • fmilburn
    fmilburn over 4 years ago in reply to beacon_dave +1
    Thanks, I've corrected the typo. That is a good point about 50Ω output mode. I may remake the video when I get my new microphone - don't want to add any more confusion to the internet than is already out…
  • fmilburn
    fmilburn over 4 years ago in reply to Andrew J

    Being confused with W2AEW is a nice compliment. I think the main difference is he actually knows what he is talking about :-)

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • fmilburn
    fmilburn over 4 years ago in reply to shabaz

    Hi Shabaz,

    Thanks!  I made the video in front of a large bay window with indirect light that softens shadows.  As long as the natural light is not mixed with indoor lighting it works well.

    The transformer method is interesting.  I've never used them in my projects but should get one to experiment with.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • fmilburn
    fmilburn over 4 years ago in reply to Jan Cumps

    After listening to it again this morning I agree with your comment on audio quality.  The room I'm in is large and reflective.  I'm using the microphone on my laptop computer without noise reduction.  The computer is located behind and to the side of a monitor and turning my head blocks sound and changes the volume.  The spaces between the sound clips that were edited into the video are also evident.  I'm going to buy an external microphone and see how that works.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • shabaz
    shabaz over 4 years ago

    Hi Frank,

    Nice video and explanation! 

    Also, nice lighting, shadows were at a minimum, I struggle with that. 

    The same circuit and equipment can also be used as an impedance meter. One option to solve the voltage on X point that you mention,  is to find a transformer and use that to isolate the function generator. Then, the ground of the 'scope probes can be put in the middle junction of the DUT and resistor, i.e. Y connected to the bottom of the circuit instead. The transformer method has its own limitations however, since then you can only test within a certain frequency range.

    Great experiment it provides so much insight into a range of components and networks.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • Andrew J
    Andrew J over 4 years ago

    I thought the quality was good.  In fact, I actually thought the embedded video was from W2AEW and I spent some minutes scratching my head working out why your comment made no sense!!  Great post.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
<>