Member and Staff Blogs Year of the Monkey Badge: Hao Xie Nian!
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Leaderboard
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Community Hub to participate - click to join for free!
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: spannerspencer
  • Date Created: 29 Jan 2016 10:35 AM Date Created
  • Views 7383 views
  • Likes 8 likes
  • Comments 64 comments
  • helpful_hints
  • tips_and_tricks
  • chinese_new_year
  • year_of_the_monkey
Related
Recommended

Year of the Monkey Badge: Hao Xie Nian!

spannerspencer
spannerspencer
29 Jan 2016

Year of the MonkeyCelebrate Chinese New Year with element14!

 

Day Eight: Happy New Year!

 

Hao xie nian! The holidays are upon us, which is wonderful news, albeit the end of our element14 celebrations. And here we are, welcoming in the Year of the Monkey, and a brand new badge to usher it in.

 

Now that it's the Year of the Monkey, all you need to do to win our time-limited badge is stop by to read and comment on each of our New Year blogs. The badge will only be available to earn until February 23, after which you'll have to wait 12 years before it comes up again (given the cycle of the Chinese zodiac).

 

Monkey Business

The monkey signifies a year of creativity, innovation, and also of mischief. Which seems quite fitting for the element14 Community!image

 

So in honour of the cheeky monkey that'll be looking over our celestial shoulders this year, we want you to give all your top tips, cheats, hints and tricks that you regularly employ while working on your electronics projects.

 

Thanks for joining in with our Chinese New Year celebrations, and may you have a splendid year swinging from the trees and causing all manner of mischief!

  • Sign in to reply

Top Comments

  • ipv1
    ipv1 over 10 years ago +9
    Here's a tip for some the newbies..
  • clem57
    clem57 over 10 years ago +4
    When soldering headers, do one end pin first and do other end next. Check alignment carefully before finishing row. Clem
  • spannerspencer
    spannerspencer over 10 years ago +4
    My top tip: When you get up to the 30th floor and realise you've forgotten to bring a fuse with you to get a PSU working again, you can always rob the one out of your multimeter Guess how I figured that…
  • grahamwebberjhb
    grahamwebberjhb over 10 years ago +4
    When building a prototype PCB use 0 ohm resistors on the supply to major circuit blocks this allows you to easily remove parts of the circuit to find the culprit, if things do not work first time.
  • bwelsby
    bwelsby over 10 years ago +4
    When working on a new project document everything. Divide large complicated projects into smaller easy to manage chunks. Work out a testing strategy Read datasheets at least twice. When you have a problem…
  • dougw
    dougw over 10 years ago +3
    If it looks like your soldering is getting dangerously messy, or has unwanted solder bridges, clean the tip of your iron and use more flux. Probably the most useful diagnostic instrument is your eyes …
  • Robert Peter Oakes
    Robert Peter Oakes over 10 years ago +3
    A really great tip you will thank me for at some point (I learned this the hard way) Try to train yourself to NOT grab your soldering iron if you drop it or if it falls I did this in my late teens, it…
  • Robert Peter Oakes
    Robert Peter Oakes over 10 years ago in reply to Robert Peter Oakes +3
    Oh and in the spirit of the year of the Monkey Put enough monkeys in a room with enough equipment and time and they will create Ultron and take over the world, or atleast create some awsome AI Gung He…
  • Robert Peter Oakes
    Robert Peter Oakes over 10 years ago +3
    Well a few of us are there
  • COMPACT
    COMPACT over 10 years ago in reply to shabaz +3
    Hi Shabaz, Most persons thought the universe was earth centric or flat and that's the case with soldering temperatures as well. The drop in temperature of the energy source when soldering is the reason…
Parents
  • COMPACT
    COMPACT over 10 years ago

    Another just important piece of advice - "Don't use too high a temperature soldering iron"

    All a high temperature does is turn flux into soot - so don't!

     

    The important thing is to energy to the intended solder joint and using a hot iron only damages PCBs and components.

    I use temperatures as low as 260 deg C for SnPb joints and slightly higher for Pb free. (And never more than 300 deg C).

    Doing this attenuates the risk of damaging stuff and it allows you to apply heat for longer without any undue ramifications.

     

    A soldering iron with a very fast recovery time or using a Tip with a large thermal mass helps a lot!

    Avoid using really narrow soldering tips (e.g. 1.0mm or less) unless you can't avoid it because of

     

    A preheater definitely helps - preheat the workpiece to say 100 deg C first and the touch the solder joints with the iron to initiate the solder reflow.

     

    One you have defined a proven process document it and use it repeatedly.

     

    Gung He Fut Choy!

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • shabaz
    shabaz over 10 years ago in reply to COMPACT

    Hi COMPACT!

     

    I don't know that applies to everyone, my normal tip temperature setting (leaded solder with 180 deg or so melting point) is typically 330 or 340 deg C or higher. The temperature will drop as heat is transferred into the join, and then the iron will be compensating by pumping more power into the tip to bring the temperature up again.

     

    Ask a dozen people and they give a dozen best practices with soldering : ) I guess whatever works best comes with experience and the tools we use, and will be different for us all.

     

    Since there is a desire to make the join and get out of there fast! my ideal setting is 330 deg C. (or sometimes higher - e.g. if soldering connectors despite swapping to a bigger tip - the behaviour won't be exactly the same so the best temperature from experience per tip and type of target, in my case the temp is increased to 340 or 350 with these larger joins).

     

    Regarding tip size, since most work is surface mount, my all-rounder tip size is 1mm ellipse-shaped conical slice, personally I find it difficult to use the tinier tips with points, but others may excel with them, would be interesting to know.

    Although I should swap out, at 1mm if I'm lazy on a particular day : ( I keep using it with stripboard too.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • COMPACT
    COMPACT over 10 years ago in reply to shabaz

    Hi Shabaz,

     

    Most persons thought the universe was earth centric or flat and that's the case with soldering temperatures as well.

     

    The drop in temperature of the energy source when soldering is the reason why one should use a large mass tip or an iron that can deliver energy on demand.

    Another way to address this via thermal relief pads on PCBs. The thermal reliefs are stop the energy escaping into unwanted areas such as power planes (and dropping the joint temperature).

     

    When using lower temperatures there's actually no rush to remove the iron from the joint and its further assisted with flux paste.

    The lower temperatures also extend tip life.  (Another way to extend tip life is to get an auto powering down soldering iron).

     

    Here's another hint, Don't use conical tips unless there is a good reason!  Chisel and double chisel tips are the way to go and for SMD work you may want to use a single chisel well tip.

    Chisel tips provide a large contact surface area to the solder joint.

     

    Many soldering equipment manufacturers supply their soldering stations with conical tips to force the consumer to by additional tips (chisel tips).

    Conical tips make good dart heads.

     

    Here's a thought experiment for you - what would you expect to happen if you wave soldered a PCB with the molten solder fountain at 350 deg C or higher ?

    Some manufacturers recommend a solder pot temperature of 271 deg C which is in the same ballpark as the temperatures I use (i.e. < 300 deg C) so why have it +80 deg C hotter?

     

    And remember "Controlled Surface Tension is your friend"

     

    Have a look at this video. Notice that there are no burnt bits of flux formed, use of FLUX PASTE and chisel tip and the slow pace of soldering.

    Since it is Pb free soldering the joints never look glossy like SnPb.

    You don't have permission to edit metadata of this video.
    Edit media
    x
    image
    Upload Preview
    image

     

     

    Cheers

     

    Compact

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • shabaz
    shabaz over 10 years ago in reply to COMPACT

    Hi!

     

    I don't see any of the symptoms you mention though. So it really does vary from iron to iron, user to user.

    I don't use conical tips like you mention, it is a flat, ellipse shaped slice off a conical shape.

    Chisel and double chisel may work out well for some.

     

    I use the ellipse-shaped conical slice even for 0.4mm pitch, still works.

    I guess use whatever works best for your conditions. Some are happier with the larger tips and drag soldering.

    My point is just that it's not possible to state that the temp should be lower than 300 degrees C - the default varies for different irons and

    the way people use it (bit shape, bit size, target area) and for me the preferred temp is definitely nowhere near your preferred temp.

     

    Thermal relief isn't possible when soldering wires to connectors, so I use the beefiest tip suitable for the job but my temperature is still set to 330-340 degrees.

    I don't see burnt flux on any join, just clear transparent flux residue, which can be soaked up immediately if desired with a dry or IPA wipe (clean the board later if needed).

    The thought experiment you mention is dissimilar to normal soldering methods, because although pot and solder temperature in the thought experiment

    may be a specific value, for iron-based soldering I'm not heating the solder to 330 degrees. The iron is at that temperature. When applied to the

    joint in question, the joint temperature rises and as it rises the solder is applied.

    Lower temps may keep the tip life healthier but I'm more concerned with the join. There are solutions for tip life anyway like auto-cooling down irons as you mention.

     

    EDIT: Just noticed this diagram in some PACE brochure here (PDF), which might say it better than my poor description/anecdotal results above.

    image

     

    The brochure doesn't mention the initial tip  temperature either, the actual value can chosen can vary for different situations such as tip size and iron power.

    However you can see tip temperature drop as the joint is made, and simultaneously the joint temperature rise as the joint is made, and they unite at an intermediate point.

    Of course, even though they say this is 'ideal iron performance' the brochure is 9 years old, and technology changes. So I guess such old information could be taken

    with a pinch of salt or just of historical relevance, all I can say is that it appears to work for me at some 330-340 degrees C tip temperature. You may have more modern

    gear.  The irons mentioned in the PACE brochure (TD-100) are still current models on their website and available from Farnell, so such a graph might still apply to these

    particular irons but this is a guess. I'm not knowledgeable enough in soldering process technology to know what improvements have been made in recent years.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • shabaz
    shabaz over 10 years ago in reply to shabaz

    For anyone interested in purchasing an iron, just noticed the PACE ST-50 station looks quite reasonably priced, it comes with a TD-100 iron.

    I noticed from someone's online photos that the ST-50 insides look quite nicely built.

    I haven't tried it, it would be interesting to hear from anyone who has used it.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • COMPACT
    COMPACT over 10 years ago in reply to shabaz

    The use of overly high temperatures is to compensate for product flaws and poor technique.

    The PERFOMance graph even shows it and says that the tip temperature is "Too Hot".

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • shabaz
    shabaz over 10 years ago in reply to COMPACT

    Overly high is of course bad, but what is overly high?

     

    Not sure they're saying a flawed product would exhibit the behaviour in the graph.. because the pink line shows the solder joint temperature correctly

    going up to reach solder joint temperature, and it never goes into the 'too hot' zone. It goes into the green 'Ideal' zone per solder join.

     

    I was under the impression PACE tools were quite high-end, and it is a currently shipping product.

    Also there is a JBC brochure that shows a similar thing, and they explicitly mention 350 degrees C to be recommended in their text.

    The graph on the right clearly shows how their iron bounced back to 350 degrees C after each solder join, whereas the

    gray line (competitor iron) couldn't recover so quickly. The JBC graphs do not show the solder joint temperature, but it too would have

    started at cold and then would have risen as the heat was applied until it was in some ideal green zone.

    image

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • shabaz
    shabaz over 10 years ago in reply to COMPACT

    Overly high is of course bad, but what is overly high?

     

    Not sure they're saying a flawed product would exhibit the behaviour in the graph.. because the pink line shows the solder joint temperature correctly

    going up to reach solder joint temperature, and it never goes into the 'too hot' zone. It goes into the green 'Ideal' zone per solder join.

     

    I was under the impression PACE tools were quite high-end, and it is a currently shipping product.

    Also there is a JBC brochure that shows a similar thing, and they explicitly mention 350 degrees C to be recommended in their text.

    The graph on the right clearly shows how their iron bounced back to 350 degrees C after each solder join, whereas the

    gray line (competitor iron) couldn't recover so quickly. The JBC graphs do not show the solder joint temperature, but it too would have

    started at cold and then would have risen as the heat was applied until it was in some ideal green zone.

    image

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
Children
  • COMPACT
    COMPACT over 10 years ago in reply to shabaz

    Using lower soldering temperatures is as hard a sell as using proper ESD and moisture control precautions!

    (it only takes 20 volts of induced static to cause damage - That's just a wave of the hand!)

     

    People use the excuse "Because we've always done it that way!" to perpetually tout 350 deg C soldering temperatures.

    Another important thing is not to get the PCB substrate reaching its glass transition temperature and ruining it.

     

    Here's another way to look at it.

    If you have a warm shower at an acceptable temperature of less than 40 deg C, you'll have a good shower and your body temperature can get warmer because you've allowed the heat to sink in.

    You don't shower or bathe at 100 degrees C because you'll scold yourself and your body temperature still remain normal.

     

    I use a range of soldering equipment including Haako, JBC, ERSA, Weller and PDR.

    I've also got some no name stuff but that is used very carefully because the risk of damaging something is much greater.

     

    All I can say is try it and see.

     

    It is actually much better to blow off as much solder off a PCB as possible but that's another story!!

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • shabaz
    shabaz over 10 years ago in reply to COMPACT

    I'm not using an excuse to perpetually tout any specific temperature though - I can't speak for others who might : (

    All I can say is that experimentally/anecdotally  330-340 degrees  was arrived at as optimal for the chosen bit size and target joints, and it does appear to confirm soldering iron vendor's results as shown above.

     

    The physics seems reasonable. I don't shower with a single 1mm jet of water close to 100 degrees C, but if  for the experiment there was a heat conductive piece of metal on top of the skin (my skin is not as heat conductive), it probably wouldn't scold for a period, because the temperature will still be rising. Of course for the analogy the jet of water would have to be adjusted to drop in temperature over time like the soldering iron bit does.

     

    I've not experienced burnt flux on PCBs nor PCBs entering glass transition nor (to the best of my knowledge, because there is always the possibility of some latent i.e. hidden defect that has occurred) of any component damage either.

     

    I have never experienced the issues mentioned and flux leaves clear residue, no component or board damage of course, and I happily see a join within a second or two max. After inspecting the smaller joins under a magnifier, any rework if there was a solder bridge is successful too, no component or board damage, so it is repeatable in the same area. Holes with thermal relief are of course fine but so are non-thermal relief holes (which are sometimes essential to the board design), no board damage in either case.

     

    I understand the lower temperatures work for you though. It is just that I'm very happy with the combination I've arrived at (length of soldering time, bit size, bit shape and so on), which requires me to have a far higher soldering iron temperature which does corroborate with the PACE and JBC docs, and can confirm I do not see the issues mentioned earlier. But if people do, it totally would be wise to reduce temperature as you suggest.