Member's Forum Triac not shutting off (24v AC sprinkler valve control)
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Leaderboard
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Community Hub to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Replies 34 replies
  • Answers 16 answers
  • Subscribers 597 subscribers
  • Views 6168 views
  • Users 0 members are here
  • valve
  • ac
  • triac
  • sprinkler
  • 24v
  • opensprinkler
Related

Triac not shutting off (24v AC sprinkler valve control)

ntewinkel
ntewinkel over 9 years ago

Hi All,

 

I'm working on replacing my aging and broken sprinkler controller, and found some open source software (OpenSprinkler) to run on a Raspberry Pi that handles the scheduling very nicely (plus it has an app for my phone).

With that software I'm able to control a couple of shift registers to turn LEDs on and off, simulating the sprinkling zones.

 

I'm not very familiar with TRIACs (read: not at all familiar, never used them before image), but recently I learned that the sprinkler valves use 24v AC and that TRIACs would be a good way to switch them, with relays generally being rather big once you get 16 of them lined up, and regular power transistors only being good for DC.

 

I bought some BRT12H "non-zero crossing" opto-isolating TRIACs (datasheet: http://www.vishay.com/docs/83689/83689.pdf), because they seemed to meet the desirements of opto-isolating and AC for 250mA.

 

I hooked them up (with 220ohm resistors from shift registers to TRIACs), and it all looked promising when I turned the first zone on (sprinklers worked, yay!), but then it wouldn't shut off (sprinklers still working, not yay!). It only shuts off if I remove the 24v power momentarily.

 

I've done some Googling around but have not yet found any solution, and to be honest it's not making a whole lot of sense to me (yet... hopefully yet).

 

I did find out that TRIACs (in general?) need to cross zero (volts?) to turn off. I'm not sure what this "non-zero crossing" bit means but I have a nagging suspicion that it's a key part of the issue.

Should I have bought "zero crossing" TRIACs instead?

 

Can anyone help shed some light?  ...and hopefully also shed a solution image

 

ps, I did see that I can buy a pre-built board for not too expensive (about $80 after shipping and taxes), but it's a cool DIY project and it would be far more satisfying (and educational) to build it myself.

 

edit: While doing more searching for answers I noticed that SSRs (solid state relays) do exist that are tiny chips, like this one, DIP-8: http://www.sharpsma.com/webfm_send/335  - very cool.

 

Thanks!

-Nico

  • Sign in to reply
  • Cancel

Top Replies

  • jw0752
    jw0752 over 9 years ago in reply to ntewinkel +3 suggested
    Hi Nico, AC solenoids will convert to DC solenoids quite easily if you are willing to reduce the voltage. What will remain constant for proper operation is the wattage of the solenoid. For example your…
  • D_Hersey
    D_Hersey over 9 years ago in reply to jw0752 +2 suggested
    You are using LV, so it probably won't matter as much, but for line potentials, only certain types of Cs are a good choice in this rough service, metallized polyester being one.
  • jc2048
    jc2048 over 9 years ago in reply to ntewinkel +2 suggested
    "And what is the best way to figure out the values?" Iteration. Increase the capacitor value and decrease the resistor value a bit and try again. But when you get down to a resistor value of 100 ohms and…
  • mcb1
    0 mcb1 over 9 years ago in reply to ntewinkel

    DC makes sense to me

    This was interesting reading, but on my browser the diagrams didn't show up.

    AC vs. DC | Flow Control Network

     

    With winter here, it looks like you have ample time to resolve the problems

     

     

    Mark

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • ntewinkel
    0 ntewinkel over 9 years ago in reply to mcb1

    I don't think it's your browser - I don't see the pictures either image

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • ntewinkel
    0 ntewinkel over 9 years ago in reply to mcb1

    I finally had the time (and parts) to get back to this again, and your circuit works perfectly, thanks Mark! mcb1

     

    I'm using moc3021 for the optoisolator, and mac97A for the triac.

     

    I was wondering what the purpose is of the two 1n4148 diodes?

    From another circuit diagram, I noticed they just used a bigger resistor - and the circuit works if I replace the (150r and diodes) with a single 1k resistor.

     

    And OpenSprinkler doesn't do any of that - and looks like kind of a bad design now image

     

    Thanks,

    -Nico

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • mcb1
    0 mcb1 over 9 years ago in reply to ntewinkel

    I was wondering what the purpose is of the two 1n4148 diodes?

    You aren't alone in that.

     

    It would stop voltage less than 0.6v from passing, and since it is AC it requires back to back, but other than that I'm not sure.

    Since it worked in a piece of commercial equipment, we simply copied it and I've used it ever since.

     

    Mark

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
<