Member's Forum I think this is a buck converter, but I'm not entirely sure.
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Leaderboard
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Community Hub to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Replies 18 replies
  • Answers 3 answers
  • Subscribers 597 subscribers
  • Views 2252 views
  • Users 0 members are here
Related

I think this is a buck converter, but I'm not entirely sure.

capacitance_incarnate
capacitance_incarnate over 9 years ago

So I have this little chip here from a cigarette lighter psu, but there isn't a voltage regulator any where in it. If this is indeed a buck converter, that would explain the lack of a regulator, but I'm new to this kind of stuff, (I first got into it  while creating a project for school last year) so I would appreciate any help I can get.

imageimageimage

  • Sign in to reply
  • Cancel

Top Replies

  • rachaelp
    rachaelp over 9 years ago in reply to capacitance_incarnate +2 suggested
    Take a look at the datasheet for the controller here (assuming it is the one Shabaz is referring to): http://www.farnell.com/datasheets/1723944.pdf?_ga=1.226316314.1698039299.1446112257 If you look at…
  • shabaz
    shabaz over 9 years ago +1 verified
    Hi Jake, That is a voltage regulator, also known as a DC-DC converter or a Buck converter when it uses an inductor and switching and steps down the voltage. You could confirm by examining the part code…
  • rachaelp
    rachaelp over 9 years ago in reply to capacitance_incarnate +1
    Jake Linville wrote: ok so the big resistor up top is a 0.39 Ω ± 2%. I'm assuming thats the one that I need to replace, because there is no way I could replace the little ones on the bottom. Unfortunately…
  • rachaelp
    0 rachaelp over 9 years ago in reply to capacitance_incarnate

    Jake Linville wrote:

     

    ...although I now know that I'm going to have to find someone to replace the surface mount resistors for me.

    Or use it as an excuse to invest in a decent soldering station! You don't have to spend huge amounts to get something adequate for starting out and it'll prove to be exceedingly useful time and time again if you continue to pursue electronics further image

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • shabaz
    0 shabaz over 9 years ago in reply to capacitance_incarnate

    Hi Jake,

     

    You didn't specify the reason for 4.7V, but if you're happy with "about 4.7V" then you could put a diode in series with the output. The output won't be accurate any more, but will be lower than 5V slightly (could vary to 4V or lower). For any accuracy you need to take the approach Rachael mentions with the resistors,but needs the steps mentioned (soldering capability, resistors purchased). If you're interested in this as a hobby, see this URL for lots of information: I Want to Do Electronics!  Where do I start?

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • capacitance_incarnate
    0 capacitance_incarnate over 9 years ago in reply to shabaz

    well, the reason is I'm actually trying to make an adapter for my 3ds. There was an old gameboy advance charger that hooked into both the wall or a cigarette lighter. I plan on making one of these that is fine tuned for the 3ds, as it is VERY cheaply made and will break at a little over 5 volts (it normally wants 4.6)

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • capacitance_incarnate
    0 capacitance_incarnate over 9 years ago in reply to rachaelp

    I actually do have a soldering station. I picked it up for that project I mentioned, and have been making small circuits for fun, but because I'm a broke 15 year old, the only parts I have come from broken radios and computers. although I do have plenty of resistors.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • rachaelp
    0 rachaelp over 9 years ago in reply to shabaz

    shabaz wrote:

     

    You didn't specify the reason for 4.7V, but if you're happy with "about 4.7V" then you could put a diode in series with the output.

    Yes if you only need approximately 4.7V then this is a good idea. If you use a schottky diode then the Vf of the diode should be low enough that you'll be around the 4.5-4.7V range depending on the exact device chosen and the current being drawn.

     

    shabaz wrote:

     

    If you're interested in this as a hobby, see this URL for lots of information: I Want to Do Electronics! Where do I start?

    I'll second this, and its author (jw0752 has done a lot of other great blogs which are worth reading if you're interested.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • capacitance_incarnate
    0 capacitance_incarnate over 9 years ago in reply to rachaelp

    ok so I've located r1. its 1.2Ω. Im still working on r2. once i find that, ill plug it into that equation that Texas instruments has, and I'll replace r1. and issues in doing that?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • rachaelp
    0 rachaelp over 9 years ago in reply to capacitance_incarnate

    I hope it's not 1.2 ohm. Do you mean Kohm? You can do as you said to calculate the two resistor values. You might need to replace both to get the output you need as you will be restricted to standard values which can be easily obtained.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • capacitance_incarnate
    0 capacitance_incarnate over 9 years ago in reply to rachaelp

    whoops. yea i meant  kohms. I found what I belive to be r1, its a .43 kohm and a 3.3 kohm in series, so if at all possible i want to try to only mess with r1.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
<