Member's Forum Question regarding thermal resistance of a UA7805 regulator
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Leaderboard
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Community Hub to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Replies 16 replies
  • Answers 4 answers
  • Subscribers 629 subscribers
  • Views 2816 views
  • Users 0 members are here
Related

Question regarding thermal resistance of a UA7805 regulator

Andrew J
Andrew J over 7 years ago

From the datasheet, the TO-220 package has the following thermal characteristics:

 

Rja = 19C/W

Rjc(top) = 17C/W

Rjp(top) = 3C/W  (jp in this case means Junction-to-exposed pad)

 

Am I right in thinking that for a TO-220, the Rjp value is a reference to the tab when used with a heatsink?  Typically, Rjc would be used, but if this was the case, then adding a heatsink of any thermal resistance > 2C/W would make it worse!  An older version of this datasheet just referred to:

Rja = 19C/W

Rjc = 3C/W

 

This would tie in with my interpretation.

 

Thanks,

 

Andrew

  • Sign in to reply
  • Cancel
Parents
  • dougw
    0 dougw over 7 years ago

    It sounds like you are thinking the R between case and air is 2 C/W.

    I would have expected Rca can be greater than Rjc.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • Andrew J
    0 Andrew J over 7 years ago in reply to dougw

    Not sure I understand Doug.  When I've been doing a thermal calculation it is along the lines of:

     

    Pdiss = V*I

    Tj = (Pdiss * Rja) + ambient  (no heatsink)

    Tj = (Pdiss * (Rjc+Rha)) + ambient (heatsink with thermal resistance of Rha)

     

    Typically, Rjc is a lot less for an IC than Rja because it's a value to use with a heatsink:  Junction-to-Case-to-heatsink-to-air (ignoring thermal paste or thermal pad).  In the datasheet, Rjc is only 2C/W less than Rja so adding a heatsink would make it worse.

    Example

    Ambient: 25C

    Pdiss: 2W

    Tj = 2w*19c/w + 25C = 63C

    Tj = (2W * (17c/w+10c/w)) + 25 = 79C (with heatsink Rha of 10c/w)

     

    If the Rjp value was used:

    Tj = (2W * (3c/w + 10c/w)) + 25 = 51C

     

    Hence my question.  In the slightly older version of the datasheet, TI only gave a Rja = 19c/w and Rjc = 3c/w.

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • dougw
    0 dougw over 7 years ago in reply to Andrew J

    I think we are saying the same thing. The case-to-air resistance should be the main component in the junction-to-air resistance number (Rja = Rjc + Rca).

    Heatsinks increase the surface area which reduces the metal-to-air resistance which decreases the case-to-air resistance because case-to-heatsink resistance (metal-to-metal) resistance is small.

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • Andrew J
    0 Andrew J over 7 years ago in reply to shabaz

    Measuring current for reading three thermistors and displaying text values on the LCD is drawing approximately 0.235mA - although it does vary between that and 0.224mA.  I could get away with a 15C/W heatsink which can be quite small (and I think I might squeeze in just) but I much prefer your idea especially as it's a pin equivalent, fits and a lot more efficient.  I also don't know if it will work a lot harder once I get the graphics going and the voltage/current monitoring.  Got one on order so I will be able to test it out tomorrow hopefully.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • shabaz
    0 shabaz over 7 years ago in reply to Andrew J

    Hi Andrew,

     

    You might find the Arduino takes much less power on average (but I'm not sure.. also depends on which Arduino) in which case the 7805 may be fine with a smaller heatsink, but in any case that DC-DC converter should be ok without a heatsink.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • Andrew J
    0 Andrew J over 7 years ago in reply to shabaz

    Doug / Shabaz,

     

    that's brilliant thanks.  I didn't realise such things existed. 

     

    The Arduino takes 5v input, 5.5V max, 320mA (average use of features) and inverting charge pump (LTC1683) 3.5V to 5.5V max, 14mA so a 5V 1A converter should be sufficient - possibly 500mA, although the datasheet for the Arduino mentions the provision of a 5V 1A supply.  Is there anything in the datasheet I need to be picking up on?

     

    The Traco Power component, for example, gives 50mV pk-pk; 0.4% regulation load variation.  It doesn't state any thermal characteristics except "Allows full load operation upto +70C ambient without heatsink"

     

    Can't thank you enough!

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • shabaz
    0 shabaz over 7 years ago in reply to dougw

    There's several that are designed to replace a 7805 almost directly (taking up almost the same amount of space), e.g.:

    https://uk.farnell.com/c/power-line-protection/power-supplies/dc-dc-converters/dc-dc-linear-regulator-converters?output-…

    • Cancel
    • Vote Up +4 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • dougw
    0 dougw over 7 years ago in reply to Andrew J

    Could you add an external DC-DC converter module to get the voltage down where you want it?

    • Cancel
    • Vote Up +4 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • Andrew J
    0 Andrew J over 7 years ago in reply to shabaz

    No, that was an example.  I need to get rid of 6w.  In my original calcs, without Arduino, current draw is in small mA so power dissipation was tiny.  If I’d have realised in time, I would have gone with a different approach: the issue is the voltage drop from a rectified 24V input to 5V output which I initially was going to do something about just because of inefficiency but didn’t because, well, I had an LM7805 to hand and it was going to work.

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • shabaz
    0 shabaz over 7 years ago in reply to Andrew J

    Hi Andrew,

     

    How much power needs to be dissipated? I saw a value of 2W in an earlier comment, is that an example, or the actual value?

    If it's 2W, then it shouldn't need a large heatsink, e.g.:

    image

     

    A 15 degC/W heatsink will be quite small, so might fit if there's a bit of space around the TO220.

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • Andrew J
    0 Andrew J over 7 years ago in reply to shabaz

    Working at it! 

     

    Just realised a big rookie mistake: forgetting to take into account the current requirements of an Arduino which is going to cause big thermal problems for my LM7805.  I've gone from negligible power dissipation to extremely significant with PCBs due for delivery on Thursday and no room for a heatsink - minimum of 8C/W so quite large.  Thinking of pros and cons of either:

    1. redesigning and re-ordering a PCB with room for a heatsink
    2. off-boarding the LM7805 and connecting with short wires and the LM7805 on a heatsink
    3. redesigning and re-ordering 2 PCBs, providing a 5V@0.5A PSU and dropping the LM7805 altogether.

    Option 2 is the easiest and cheapest but option 3 is the best but most expensive.  Once I start soldering though, option 3 becomes VERY expensive!

     

    What I think I'll do is option 2.  At the moment, I can envisage other problems surfacing that will require reworking so it would make sense to wait until that happens.  I just need to watch the impact of doing it.  Also V2 of my project would be a lot cheaper to create as I'll have the vast majority of the parts already.  I'm prototyping that part of the circuit now to verify the impact.

     

    Hey ho.  I can commend myself for spotting it before I fry everything whilst kicking myself for missing it when I spent so long on the design and thermal calcs in the first place!!

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • Andrew J
    0 Andrew J over 7 years ago in reply to shabaz

    Working at it! 

     

    Just realised a big rookie mistake: forgetting to take into account the current requirements of an Arduino which is going to cause big thermal problems for my LM7805.  I've gone from negligible power dissipation to extremely significant with PCBs due for delivery on Thursday and no room for a heatsink - minimum of 8C/W so quite large.  Thinking of pros and cons of either:

    1. redesigning and re-ordering a PCB with room for a heatsink
    2. off-boarding the LM7805 and connecting with short wires and the LM7805 on a heatsink
    3. redesigning and re-ordering 2 PCBs, providing a 5V@0.5A PSU and dropping the LM7805 altogether.

    Option 2 is the easiest and cheapest but option 3 is the best but most expensive.  Once I start soldering though, option 3 becomes VERY expensive!

     

    What I think I'll do is option 2.  At the moment, I can envisage other problems surfacing that will require reworking so it would make sense to wait until that happens.  I just need to watch the impact of doing it.  Also V2 of my project would be a lot cheaper to create as I'll have the vast majority of the parts already.  I'm prototyping that part of the circuit now to verify the impact.

     

    Hey ho.  I can commend myself for spotting it before I fry everything whilst kicking myself for missing it when I spent so long on the design and thermal calcs in the first place!!

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Children
  • Andrew J
    0 Andrew J over 7 years ago in reply to shabaz

    Measuring current for reading three thermistors and displaying text values on the LCD is drawing approximately 0.235mA - although it does vary between that and 0.224mA.  I could get away with a 15C/W heatsink which can be quite small (and I think I might squeeze in just) but I much prefer your idea especially as it's a pin equivalent, fits and a lot more efficient.  I also don't know if it will work a lot harder once I get the graphics going and the voltage/current monitoring.  Got one on order so I will be able to test it out tomorrow hopefully.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • shabaz
    0 shabaz over 7 years ago in reply to Andrew J

    Hi Andrew,

     

    You might find the Arduino takes much less power on average (but I'm not sure.. also depends on which Arduino) in which case the 7805 may be fine with a smaller heatsink, but in any case that DC-DC converter should be ok without a heatsink.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • Andrew J
    0 Andrew J over 7 years ago in reply to shabaz

    Doug / Shabaz,

     

    that's brilliant thanks.  I didn't realise such things existed. 

     

    The Arduino takes 5v input, 5.5V max, 320mA (average use of features) and inverting charge pump (LTC1683) 3.5V to 5.5V max, 14mA so a 5V 1A converter should be sufficient - possibly 500mA, although the datasheet for the Arduino mentions the provision of a 5V 1A supply.  Is there anything in the datasheet I need to be picking up on?

     

    The Traco Power component, for example, gives 50mV pk-pk; 0.4% regulation load variation.  It doesn't state any thermal characteristics except "Allows full load operation upto +70C ambient without heatsink"

     

    Can't thank you enough!

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • shabaz
    0 shabaz over 7 years ago in reply to dougw

    There's several that are designed to replace a 7805 almost directly (taking up almost the same amount of space), e.g.:

    https://uk.farnell.com/c/power-line-protection/power-supplies/dc-dc-converters/dc-dc-linear-regulator-converters?output-…

    • Cancel
    • Vote Up +4 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • dougw
    0 dougw over 7 years ago in reply to Andrew J

    Could you add an external DC-DC converter module to get the voltage down where you want it?

    • Cancel
    • Vote Up +4 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • Andrew J
    0 Andrew J over 7 years ago in reply to shabaz

    No, that was an example.  I need to get rid of 6w.  In my original calcs, without Arduino, current draw is in small mA so power dissipation was tiny.  If I’d have realised in time, I would have gone with a different approach: the issue is the voltage drop from a rectified 24V input to 5V output which I initially was going to do something about just because of inefficiency but didn’t because, well, I had an LM7805 to hand and it was going to work.

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • shabaz
    0 shabaz over 7 years ago in reply to Andrew J

    Hi Andrew,

     

    How much power needs to be dissipated? I saw a value of 2W in an earlier comment, is that an example, or the actual value?

    If it's 2W, then it shouldn't need a large heatsink, e.g.:

    image

     

    A 15 degC/W heatsink will be quite small, so might fit if there's a bit of space around the TO220.

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer