Member's Forum Question regarding thermal resistance of a UA7805 regulator
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Leaderboard
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Community Hub to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Replies 16 replies
  • Answers 4 answers
  • Subscribers 629 subscribers
  • Views 2827 views
  • Users 0 members are here
Related

Question regarding thermal resistance of a UA7805 regulator

Andrew J
Andrew J over 7 years ago

From the datasheet, the TO-220 package has the following thermal characteristics:

 

Rja = 19C/W

Rjc(top) = 17C/W

Rjp(top) = 3C/W  (jp in this case means Junction-to-exposed pad)

 

Am I right in thinking that for a TO-220, the Rjp value is a reference to the tab when used with a heatsink?  Typically, Rjc would be used, but if this was the case, then adding a heatsink of any thermal resistance > 2C/W would make it worse!  An older version of this datasheet just referred to:

Rja = 19C/W

Rjc = 3C/W

 

This would tie in with my interpretation.

 

Thanks,

 

Andrew

  • Sign in to reply
  • Cancel
Parents
  • dougw
    0 dougw over 7 years ago

    It sounds like you are thinking the R between case and air is 2 C/W.

    I would have expected Rca can be greater than Rjc.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • Andrew J
    0 Andrew J over 7 years ago in reply to dougw

    Not sure I understand Doug.  When I've been doing a thermal calculation it is along the lines of:

     

    Pdiss = V*I

    Tj = (Pdiss * Rja) + ambient  (no heatsink)

    Tj = (Pdiss * (Rjc+Rha)) + ambient (heatsink with thermal resistance of Rha)

     

    Typically, Rjc is a lot less for an IC than Rja because it's a value to use with a heatsink:  Junction-to-Case-to-heatsink-to-air (ignoring thermal paste or thermal pad).  In the datasheet, Rjc is only 2C/W less than Rja so adding a heatsink would make it worse.

    Example

    Ambient: 25C

    Pdiss: 2W

    Tj = 2w*19c/w + 25C = 63C

    Tj = (2W * (17c/w+10c/w)) + 25 = 79C (with heatsink Rha of 10c/w)

     

    If the Rjp value was used:

    Tj = (2W * (3c/w + 10c/w)) + 25 = 51C

     

    Hence my question.  In the slightly older version of the datasheet, TI only gave a Rja = 19c/w and Rjc = 3c/w.

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • dougw
    0 dougw over 7 years ago in reply to Andrew J

    I think we are saying the same thing. The case-to-air resistance should be the main component in the junction-to-air resistance number (Rja = Rjc + Rca).

    Heatsinks increase the surface area which reduces the metal-to-air resistance which decreases the case-to-air resistance because case-to-heatsink resistance (metal-to-metal) resistance is small.

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • Andrew J
    0 Andrew J over 7 years ago in reply to shabaz

    Measuring current for reading three thermistors and displaying text values on the LCD is drawing approximately 0.235mA - although it does vary between that and 0.224mA.  I could get away with a 15C/W heatsink which can be quite small (and I think I might squeeze in just) but I much prefer your idea especially as it's a pin equivalent, fits and a lot more efficient.  I also don't know if it will work a lot harder once I get the graphics going and the voltage/current monitoring.  Got one on order so I will be able to test it out tomorrow hopefully.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • shabaz
    0 shabaz over 7 years ago in reply to Andrew J

    Hi Andrew,

     

    You might find the Arduino takes much less power on average (but I'm not sure.. also depends on which Arduino) in which case the 7805 may be fine with a smaller heatsink, but in any case that DC-DC converter should be ok without a heatsink.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • Andrew J
    0 Andrew J over 7 years ago in reply to shabaz

    Doug / Shabaz,

     

    that's brilliant thanks.  I didn't realise such things existed. 

     

    The Arduino takes 5v input, 5.5V max, 320mA (average use of features) and inverting charge pump (LTC1683) 3.5V to 5.5V max, 14mA so a 5V 1A converter should be sufficient - possibly 500mA, although the datasheet for the Arduino mentions the provision of a 5V 1A supply.  Is there anything in the datasheet I need to be picking up on?

     

    The Traco Power component, for example, gives 50mV pk-pk; 0.4% regulation load variation.  It doesn't state any thermal characteristics except "Allows full load operation upto +70C ambient without heatsink"

     

    Can't thank you enough!

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • shabaz
    0 shabaz over 7 years ago in reply to dougw

    There's several that are designed to replace a 7805 almost directly (taking up almost the same amount of space), e.g.:

    https://uk.farnell.com/c/power-line-protection/power-supplies/dc-dc-converters/dc-dc-linear-regulator-converters?output-…

    • Cancel
    • Vote Up +4 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • dougw
    0 dougw over 7 years ago in reply to Andrew J

    Could you add an external DC-DC converter module to get the voltage down where you want it?

    • Cancel
    • Vote Up +4 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • Andrew J
    0 Andrew J over 7 years ago in reply to shabaz

    No, that was an example.  I need to get rid of 6w.  In my original calcs, without Arduino, current draw is in small mA so power dissipation was tiny.  If I’d have realised in time, I would have gone with a different approach: the issue is the voltage drop from a rectified 24V input to 5V output which I initially was going to do something about just because of inefficiency but didn’t because, well, I had an LM7805 to hand and it was going to work.

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • Andrew J
    0 Andrew J over 7 years ago in reply to shabaz

    No, that was an example.  I need to get rid of 6w.  In my original calcs, without Arduino, current draw is in small mA so power dissipation was tiny.  If I’d have realised in time, I would have gone with a different approach: the issue is the voltage drop from a rectified 24V input to 5V output which I initially was going to do something about just because of inefficiency but didn’t because, well, I had an LM7805 to hand and it was going to work.