• Products and Partners
    Products and Partners
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
Member's Forum Testing a Mosfet and Schottky in-circuit; Bit more advice
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Leaderboard
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Community Hub to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Replies 31 replies
  • Answers 27 answers
  • Subscribers 630 subscribers
  • Views 8925 views
  • Users 0 members are here
Related

Testing a Mosfet and Schottky in-circuit; Bit more advice

Andrew J
Andrew J over 7 years ago

I presume this is possible with power off, looking for resistance between drain and source?

 

I'm pretty sure I've killed it - resistance is 0.33Ohms between these two pins image  Out of circuit, on a good one, it is > 13MOhms.  Looking at my circuit, I've solder the Schottky Rectifier the wrong way around - cathode to ground imageimageimage  Pretty sure that won't have done the Mosfet any good, it was too hot to touch.  Can't believe I've been so stupid - by good luck, rather than management, the other Schottky I have in the circuit (not shown below) is the right way around.

 

Is there a way of testing the Schottky rectifier in-circuit - I've tried it and the DMM 'beeps' as it detects a normal junction; measures 0.159v and 0.579V depending upon orientation of test leads?  Just to clarify - in the schematic below you can see how the Schottky rectifier should be - however, as I say, it's actually reversed and I don't know if that might affect readings. So, with the COM lead to the cathode and test (red) lead to anode it reads 0.159v; with the COM lead to the anode and test (red) lead to cathode it reads 0.579V.  I can test one out of circuit and I get 0.157V and OL respectively.  I think that indicates it is ok but in circuit it isn't reading as OL: I have to remove it to swap it around in any case so would the advice be to chuck it and use a new one? 

 

I'm really hoping I can get it off with wick and an iron and without damaging the board; ditto the Mosfet. I really don't want to lump out for a rework station.

 

Is there likely to be damage to other components down stream?  Any tips for testing components without removing them from the circuit?

 

This is only part of the circuit but shows the relationship between the Mosfet and Schottky rectifier:

 

image

 

[silently screaming inside]

  • Sign in to reply
  • Cancel
Parents
  • jc2048
    0 jc2048 over 7 years ago

    Resistance reading in-circuit is difficult because of paths round through the power and through the ICs [via the protection circuits]. You'll tend to see initially low readings that move because you're charging decoupling capacitors. I don't like doing it because of the possibility of damage to chips [a handheld meter is probably worse than a good bench meter in that respect], but then I tend to be very over-cautious.

     

    Commercially, you'd chuck the components and use new ones (the parts cost is much, much lower than the cost to you of a person messing around with parts that are suspect). Actually, you might well label the board carefully, put it to one side, and move to the next, unused prototype, unless there were good reasons for sticking with the same one.

     

    For a personal project it's different and you may want to experiment a bit. The MOSFET and Schottky are fairly robust. Just because you can't bear to touch it doesn't mean it is dead. The controller is working current mode, monitoring the current through the MOSFET with R2. With the back-to-front Schottky clamping the output, the controller would keep increasing the current through the MOSFET to try and get the voltage up but there would be some limit to that, so the part's dissipation wouldn't necessarily have been enough to destroy it.

     

    So you might try just reworking the Schottky [if the Schottky SMD package is the type with fold-under legs, they're easy to get off even with a standard soldering iron as you can lift one end at a time]. Are you able to substitute a bench supply for the power rail? If so, one approach might be to apply a very low voltage that was under the controllers's lock-out voltage and was safe for the following circuit and see if the MOSFET feeds that to the coil without there being any gate drive.

     

    The feedback arrangement is a bit odd [and, possibly, a bit dangerous]. If you lost the connection to R6 you'd lose the feedback and the converter would ramp up the voltage to try and compensate, so you want to be careful with that depending on where it comes from and what it's supposed to be doing.

    • Cancel
    • Vote Up +7 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • Andrew J
    0 Andrew J over 7 years ago in reply to jc2048

    I wasn't sure how possible it was to test in-circuit and how skewed the result would be. 

     

    However, having taken both pieces of the board, the Schottky rectifier is reading 0.159Ohms and OL; a known good one is reading 0.157Ohms and OL.  I think that's ok and I put it back on the board in the correct orientation.

     

    The Mosfet is reading 0.33Ohms between drain and source (out of circuit).  A known good one is reading >34MOhms.  So I think the one I removed is dead.  In goes a new one and back to testing.

    • Cancel
    • Vote Up +5 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • Andrew J
    0 Andrew J over 7 years ago in reply to Andrew J

    Well, on the plus side, I haven't refried the Mosfet!  On the other hand, something isn't working the way it should as it's not turning on - gate voltage is only 0.5V.  U1 is definitely turned on - the ith/run voltage is >1.9V; it's getting power to Vin and Sense.  Back to the datasheet to try and get a better understanding of what that is doing!

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • Andrew J
    0 Andrew J over 7 years ago in reply to shabaz

    Jon / Shabaz,

     

    I've added a comment covering Mosfet and feedback on to Part 11 to move the discussion over there.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • shabaz
    0 shabaz over 7 years ago in reply to Andrew J

    Hi Andrew,

     

    Sorry, I'm just seeing this now (and not had a chance to read through all the work) I've had poor connectivity due to travel (short break to the south-west of England, to catch some sun.. until it rained!).

    Regarding the boost voltage, your output is designed for beyond 15V I think? (I can't recall). If so, then the design needs a zener diode perhaps, across the gate-source of the MOSFET, because most devices don't tolerate more than 20V or 30V for the gate voltage. You'll also need a series resistor for the gate (i.e. disconnect pin 6 [TG] pin of the IC, and put the resistor in series there), maybe 10 ohm. The zener could be a 10V one, which would still switch on the device very well, and leave safety margin. Unless I've misunderstood, it seems misleading that the datasheet does not mention this, since the IC is designed for up to 30V output.

     

    Also, it's hard to know if the control system you've got to adjust voltage, is having an effect or not. I was wondering, do you have a spare extra chip? If so, it could be worth just prototyping on some scrap board (or on another of the same PCB if you've got some spare) just that IC and parts in a conventional layout (i.e. using a potential divider pair of resistors to set a voltage), get that working confirmed at (say) a high voltage that you expect the design to be able to handle, and then try to add the control circuitry.

    Also, the part is from a distributor, right? (ebay parts are often fakes, that may or may not partially work. I've been burned by that in the past).

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • Andrew J
    0 Andrew J over 7 years ago in reply to jc2048

    That would be useful - I have cross-linked to this thread (your original post) from Part 11.  I do have something to add about the feedback circuit so I can do it there. 

     

    When I say Vgs I actually mean the voltage on the output pin to the Mosfet gate, sorry.  But actually, I now understand this a bit better.  Voltage on the source is 17.4v, so it's ok for Gate voltage to be around 30.  I think you finally got it drummed in me image

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • jc2048
    0 jc2048 over 7 years ago in reply to Andrew J

    Vgs is the difference between the gate and the source. That's the difference between the blue trace and the yellow trace in the second picture. If you adjusted the traces so the gounds were together, you'd see where the MOSFET was off the two traces would be on top of each other (ie zero Vgs) and where it was on it was around 5V apart (5V Vgs). If you experiment with the maths functions, you could probably get the scope to display that nicely for you.

     

    The switch node ringing looks horrible, but isn't seen by the gate. At that stage the Vgs looks like it's still zero. The ringing comes to an end when the top MOSFET turns on again.

     

    I'm not too sure what it's doing, though. When I spoke previously of ringing, I was refering to the other edge where the top MOSFET turns off and the inductor takes the switch node voltage down quickly until the Schottky turns on. Here it looks like the energy in the coil is used up early. That might be the inductor value being too low or the coil saturating or maybe the business with the feedback voltage. Why isn't it up around whatever the internal reference voltage is?

     

    I've just had a look at part 11, which I originally missed. Do you want me to shuffle over to that one rather than have two on the go with different people contributing to each?

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • Andrew J
    0 Andrew J over 7 years ago in reply to jc2048

    I understand it isn't easy, and to be honest I wouldn't expect you to debug it but I do appreciate your input/insights.  I changed the Mosfet this morning but it's made little difference.  For information, I've captured three images:

     

    Switching noise at the terminals (equivalent to the above image) - frequency has changed drastically:

    image

    I've also captured the waveforms at Gate (channel 3, cyan) and SW (channel 1, yellow).  Gate is being driven 5v above SW but it still looks like the switching frequency is 100kHz, there's a fair bit of ringing.  But mostly, 32V pk-pk is way above the allowable gate voltage for the Mosfet, even RMS is too high.  I find the behaviour of the part a bit strange/confusing: gate is driven to SW + 5.6V; SW is driven from 0V to Vin as dictated by the Schottky Rectifier which swings 0v to Vin.  This part accepts Vin upto 36V but I'm providing 24.5V.  So the values follow that 24.5v but I only found one Mosfet with a gate voltage at 30v (actually, only one above 20v) that could drive >3A so it would seem 20v is very standard.

    image

    Interestingly, this is what LT Spice has to say:

    image

    (sorry, not a great picture)  Gate is blue; Sw is white.  Gate is showing pk-pk of 28.744V and RMS 22.302; SW is showing pk-pk of 24.10v and RMS 19.104.

     

    Here's an image of voltage at the feedback pin.  I can't get the volts/div any lower and at a smaller timebase it 'looks' sinusoidal but that is disguising what it really looks like:

    image

     

    I have tried a simpler schematic in LT Spice that works (more in line with the data sheet, without the transistor in the feedback); changing some of the capacitor values removes a lot of current ripple from the inductor - gate, sw and feedback are a lot cleaner.  I'd have to gear myself up to repurchase parts and re-do PCBs to change it.  Or lump out for a re-work station of course.  Ultimately, I'm struggling to see, now, how this chip can provide an output voltage of 15V when that would require a Vin of circa 18V but which would then drive the Gate voltage up to > 20V (albeit in 3.4us pulses - actually that's at 24.5v Vin but you get the idea.)  The datasheet does have state it can drive upto 30V output in step-down configuration and I'm only asking for half that!

     

    I really have appreciated your input and I acknowledge it isn't easy given what you see.  I'd be happy for anyone to chip in thoughts - shabaz?

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • jc2048
    0 jc2048 over 7 years ago in reply to Andrew J

    Sorry Andrew. This kind of remote debugging, gleaning small clues and trying to piece together what might be happening from very partial evidence (even less than you'd have if you were probing a circuit yourself), isn't very easy to do.

     

    When you work as a design engineer, where time is money and there's never enough of it [either time or money], then you accept the hand-holding of the datasheet and work carefully through the design procedure they lay out for you. There's a reason why it's so extensive and detailed for converters and controllers and that's because if you don't have a lot of experience with this kind of design (ie it's not your main speciality) it's easy to get it wrong.

     

    So (unfortunately) I don't have a vast amount of experience in trying to wrangle something like this. It's always been an auxilliary thing to my main development effort and generally there's little problem with POL converters. Plonk them on the board and they do their stuff.

     

    Having thought about it a bit further, the trace you show has a lower frequency variation. If the load is static, that suggests that the voltage feedback isn't very happy with things. The voltage servo loop has a bandwidth that's lower than the switching frequency. Can you slow the timebase and get an idea of the frequency and shape (is it sine like?). You might have a problem with your odd feedback arrangement through the transistor compromising the stability. What that would do on a cycle-by-cycle basis, I'm not sure. This converter also has a current servo loop, which operates over a shorter timescale to give a faster response to current changes in the load, so maybe you've contrived a situation where the two are interacting badly (possibly not helped by the drive to the MOSFET). One experiment you could try would be to remove the transistor and link the pads in such a way as so you had a simple resistive divider and see what effect it had on that lower frequency variation (and the switching frequency).

     

    The ripple comes from the current ripple through the coil and how good the capacitor is in averaging it out. You should be able to model it with a simulator (though the datasheet usually has a section - the part on chosing the inductor - with equations that would help you calculate it). If you can't find models for the inductor and the capacitor(s), a first approximation might be to add a perfect component and add resistors for the ESR in each case. A very simple way to simulate the ripple would be to ignore the controller and just control the top MOSFET with a 5V PWM waveform of the appropriate duty cycle applied between the gate and the source. [Keep in mind that that won't show you if you have any problems with the inductor saturating, though.]

     

    Don't worry about the gate charge thing. Everything considered, I'm surprisingly ignorant about MOSFETs and happy to take lessons from anyone (if no-one else does it, eventually I'll do some MOSFET blogs - I'd like to actually try generating the gate charge curve for real from a selection of parts). You might try looking at the gate charge graph and asking yourself what the straight line up to the area above the threshold voltage, where the voltage plateaus, represents in terms of an equivalent component if you were building a mental model of how the gate behaves. It's a very partial model, the behaviour then becomes more awkward as the channel opens and the charge flowing counters that simple process, but it's the simplest first approximation, if a bit rough and ready.

    • Cancel
    • Vote Up +4 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • Andrew J
    0 Andrew J over 7 years ago in reply to jc2048

    I'm swapping the IRF3205 for an IRLB8721 as it seems a better fit based on parameters I think are important (but I'm not sure!)  Here's a comparison:

     

    image

     

    You can see the IRL is very close to the Si (which is obsolete, not possible to get as old stock and surface mount only.)  The input capacitance is way down and the gate charge is much faster.  I've included the rise/fall/delay times for comparison but my understanding is they are based on a very specific circuit so unlikely to be more relevant than the gate charge.  It was difficult to find anything really as the parametric searching is limited on Farnell and CPC - a lot better on Digikey and RS.  I didn't mean to imply anything by mentioning the gate charge above, hope you didn't take offence - I was just doing a fair bit of reading based on your earlier helpful comments.

     

    Once I have a better fit Mosfet installed, I'll test and take measurements.  I suppose my first question about the switching ripple was whether that was the type of thing you were talking about originally in respect to the Mosfet choice: I've got no past experience to judge!

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
Reply
  • Andrew J
    0 Andrew J over 7 years ago in reply to jc2048

    I'm swapping the IRF3205 for an IRLB8721 as it seems a better fit based on parameters I think are important (but I'm not sure!)  Here's a comparison:

     

    image

     

    You can see the IRL is very close to the Si (which is obsolete, not possible to get as old stock and surface mount only.)  The input capacitance is way down and the gate charge is much faster.  I've included the rise/fall/delay times for comparison but my understanding is they are based on a very specific circuit so unlikely to be more relevant than the gate charge.  It was difficult to find anything really as the parametric searching is limited on Farnell and CPC - a lot better on Digikey and RS.  I didn't mean to imply anything by mentioning the gate charge above, hope you didn't take offence - I was just doing a fair bit of reading based on your earlier helpful comments.

     

    Once I have a better fit Mosfet installed, I'll test and take measurements.  I suppose my first question about the switching ripple was whether that was the type of thing you were talking about originally in respect to the Mosfet choice: I've got no past experience to judge!

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
Children
  • Andrew J
    0 Andrew J over 7 years ago in reply to shabaz

    Jon / Shabaz,

     

    I've added a comment covering Mosfet and feedback on to Part 11 to move the discussion over there.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • shabaz
    0 shabaz over 7 years ago in reply to Andrew J

    Hi Andrew,

     

    Sorry, I'm just seeing this now (and not had a chance to read through all the work) I've had poor connectivity due to travel (short break to the south-west of England, to catch some sun.. until it rained!).

    Regarding the boost voltage, your output is designed for beyond 15V I think? (I can't recall). If so, then the design needs a zener diode perhaps, across the gate-source of the MOSFET, because most devices don't tolerate more than 20V or 30V for the gate voltage. You'll also need a series resistor for the gate (i.e. disconnect pin 6 [TG] pin of the IC, and put the resistor in series there), maybe 10 ohm. The zener could be a 10V one, which would still switch on the device very well, and leave safety margin. Unless I've misunderstood, it seems misleading that the datasheet does not mention this, since the IC is designed for up to 30V output.

     

    Also, it's hard to know if the control system you've got to adjust voltage, is having an effect or not. I was wondering, do you have a spare extra chip? If so, it could be worth just prototyping on some scrap board (or on another of the same PCB if you've got some spare) just that IC and parts in a conventional layout (i.e. using a potential divider pair of resistors to set a voltage), get that working confirmed at (say) a high voltage that you expect the design to be able to handle, and then try to add the control circuitry.

    Also, the part is from a distributor, right? (ebay parts are often fakes, that may or may not partially work. I've been burned by that in the past).

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • Andrew J
    0 Andrew J over 7 years ago in reply to jc2048

    That would be useful - I have cross-linked to this thread (your original post) from Part 11.  I do have something to add about the feedback circuit so I can do it there. 

     

    When I say Vgs I actually mean the voltage on the output pin to the Mosfet gate, sorry.  But actually, I now understand this a bit better.  Voltage on the source is 17.4v, so it's ok for Gate voltage to be around 30.  I think you finally got it drummed in me image

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • jc2048
    0 jc2048 over 7 years ago in reply to Andrew J

    Vgs is the difference between the gate and the source. That's the difference between the blue trace and the yellow trace in the second picture. If you adjusted the traces so the gounds were together, you'd see where the MOSFET was off the two traces would be on top of each other (ie zero Vgs) and where it was on it was around 5V apart (5V Vgs). If you experiment with the maths functions, you could probably get the scope to display that nicely for you.

     

    The switch node ringing looks horrible, but isn't seen by the gate. At that stage the Vgs looks like it's still zero. The ringing comes to an end when the top MOSFET turns on again.

     

    I'm not too sure what it's doing, though. When I spoke previously of ringing, I was refering to the other edge where the top MOSFET turns off and the inductor takes the switch node voltage down quickly until the Schottky turns on. Here it looks like the energy in the coil is used up early. That might be the inductor value being too low or the coil saturating or maybe the business with the feedback voltage. Why isn't it up around whatever the internal reference voltage is?

     

    I've just had a look at part 11, which I originally missed. Do you want me to shuffle over to that one rather than have two on the go with different people contributing to each?

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • Andrew J
    0 Andrew J over 7 years ago in reply to jc2048

    I understand it isn't easy, and to be honest I wouldn't expect you to debug it but I do appreciate your input/insights.  I changed the Mosfet this morning but it's made little difference.  For information, I've captured three images:

     

    Switching noise at the terminals (equivalent to the above image) - frequency has changed drastically:

    image

    I've also captured the waveforms at Gate (channel 3, cyan) and SW (channel 1, yellow).  Gate is being driven 5v above SW but it still looks like the switching frequency is 100kHz, there's a fair bit of ringing.  But mostly, 32V pk-pk is way above the allowable gate voltage for the Mosfet, even RMS is too high.  I find the behaviour of the part a bit strange/confusing: gate is driven to SW + 5.6V; SW is driven from 0V to Vin as dictated by the Schottky Rectifier which swings 0v to Vin.  This part accepts Vin upto 36V but I'm providing 24.5V.  So the values follow that 24.5v but I only found one Mosfet with a gate voltage at 30v (actually, only one above 20v) that could drive >3A so it would seem 20v is very standard.

    image

    Interestingly, this is what LT Spice has to say:

    image

    (sorry, not a great picture)  Gate is blue; Sw is white.  Gate is showing pk-pk of 28.744V and RMS 22.302; SW is showing pk-pk of 24.10v and RMS 19.104.

     

    Here's an image of voltage at the feedback pin.  I can't get the volts/div any lower and at a smaller timebase it 'looks' sinusoidal but that is disguising what it really looks like:

    image

     

    I have tried a simpler schematic in LT Spice that works (more in line with the data sheet, without the transistor in the feedback); changing some of the capacitor values removes a lot of current ripple from the inductor - gate, sw and feedback are a lot cleaner.  I'd have to gear myself up to repurchase parts and re-do PCBs to change it.  Or lump out for a re-work station of course.  Ultimately, I'm struggling to see, now, how this chip can provide an output voltage of 15V when that would require a Vin of circa 18V but which would then drive the Gate voltage up to > 20V (albeit in 3.4us pulses - actually that's at 24.5v Vin but you get the idea.)  The datasheet does have state it can drive upto 30V output in step-down configuration and I'm only asking for half that!

     

    I really have appreciated your input and I acknowledge it isn't easy given what you see.  I'd be happy for anyone to chip in thoughts - shabaz?

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • jc2048
    0 jc2048 over 7 years ago in reply to Andrew J

    Sorry Andrew. This kind of remote debugging, gleaning small clues and trying to piece together what might be happening from very partial evidence (even less than you'd have if you were probing a circuit yourself), isn't very easy to do.

     

    When you work as a design engineer, where time is money and there's never enough of it [either time or money], then you accept the hand-holding of the datasheet and work carefully through the design procedure they lay out for you. There's a reason why it's so extensive and detailed for converters and controllers and that's because if you don't have a lot of experience with this kind of design (ie it's not your main speciality) it's easy to get it wrong.

     

    So (unfortunately) I don't have a vast amount of experience in trying to wrangle something like this. It's always been an auxilliary thing to my main development effort and generally there's little problem with POL converters. Plonk them on the board and they do their stuff.

     

    Having thought about it a bit further, the trace you show has a lower frequency variation. If the load is static, that suggests that the voltage feedback isn't very happy with things. The voltage servo loop has a bandwidth that's lower than the switching frequency. Can you slow the timebase and get an idea of the frequency and shape (is it sine like?). You might have a problem with your odd feedback arrangement through the transistor compromising the stability. What that would do on a cycle-by-cycle basis, I'm not sure. This converter also has a current servo loop, which operates over a shorter timescale to give a faster response to current changes in the load, so maybe you've contrived a situation where the two are interacting badly (possibly not helped by the drive to the MOSFET). One experiment you could try would be to remove the transistor and link the pads in such a way as so you had a simple resistive divider and see what effect it had on that lower frequency variation (and the switching frequency).

     

    The ripple comes from the current ripple through the coil and how good the capacitor is in averaging it out. You should be able to model it with a simulator (though the datasheet usually has a section - the part on chosing the inductor - with equations that would help you calculate it). If you can't find models for the inductor and the capacitor(s), a first approximation might be to add a perfect component and add resistors for the ESR in each case. A very simple way to simulate the ripple would be to ignore the controller and just control the top MOSFET with a 5V PWM waveform of the appropriate duty cycle applied between the gate and the source. [Keep in mind that that won't show you if you have any problems with the inductor saturating, though.]

     

    Don't worry about the gate charge thing. Everything considered, I'm surprisingly ignorant about MOSFETs and happy to take lessons from anyone (if no-one else does it, eventually I'll do some MOSFET blogs - I'd like to actually try generating the gate charge curve for real from a selection of parts). You might try looking at the gate charge graph and asking yourself what the straight line up to the area above the threshold voltage, where the voltage plateaus, represents in terms of an equivalent component if you were building a mental model of how the gate behaves. It's a very partial model, the behaviour then becomes more awkward as the channel opens and the charge flowing counters that simple process, but it's the simplest first approximation, if a bit rough and ready.

    • Cancel
    • Vote Up +4 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer