Member's Forum A Soldering Iron for Christmas
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Leaderboard
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Community Hub to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 21 replies
  • Subscribers 548 subscribers
  • Views 4074 views
  • Users 0 members are here
Related

A Soldering Iron for Christmas

scottiebabe
scottiebabe over 2 years ago

With a few words of encouragement from shabaz and baldengineer I snuck this bad girl into the Christmas tree!

 image

A USB-c powered portable soldering iron!

 image image

image

image

image

image

image

Fully assembled it has a similar form factor to my weller wxmp

image

With the temperature set at 300 degC it struggled a little to melt leaded solder on a copper clad board.

 

When I adjusted the temp to 330 degC the same temp I use on my weller wxmp, Id say its thermal performance felt similar (no scientific evidence).

 

The only obvious criticism I have thus far is the included silicone USB cable is a little on the short side. If the cable was 30 cm longer, I think it would be long enough. I am hopping to find a powerbank that will power this iron, at which point the USB cable length would not be an issue.

 

It also didn’t include a travel or storage pouch…

 image

But that is also okay, I think I am going to try and put together an electronics first aid kit (I have the soldering iron covered).

  • Sign in to reply
  • Cancel

Top Replies

  • Jan Cumps
    Jan Cumps over 2 years ago +5
    what a time to be alive https://youtu.be/qCC941xKuBs
  • scottiebabe
    scottiebabe over 2 years ago in reply to colporteur +3
    I purchased mine through amazon and had it not been for the eggnog in the moosemug I probably would have noticed the $15 off coupon, o well. https://www.amazon.ca/gp/product/B089ZSG7XG/ The complete…
  • scottiebabe
    scottiebabe over 2 years ago +3
    If one was proficient in the mechanical side of things, you could DIY your own USB soldering iron (others have). I just tried heating up one of my weller tips which like the TS80P use a 3.5 mm TRS jack…
  • shabaz
    shabaz over 2 years ago in reply to scottiebabe

    Interesting! Its 144 MHz RISC-V chip should hopefully be able to handle the soldering element heater algorithm : ) Awesome that there is so much choice, USB-C adoption for portable soldering is really high it seems.

    I went for these two, although I probably would have considered the PINECIL had I known about it:

    This one, Sequre S60, accepts JBC C210 series tips, which cover a range of surface-mount and through-hole prototyping, but are no good for large connectors:

    image

    I also ordered this "Smart Electric Soldering Iron" which looks very basic, it is pretty cheap. I don't expect it to be amazing at this price, but I was still curious if it could function as a basic soldering iron. This one is compatible with C245 series tips, which are fine for large connectors, as well as surface-mount. 

    image

    A benefit for these two models though, is that because I already have C210 and C245 tips and know what they solder like, it could be interesting to compare.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • Andrew J
    Andrew J over 2 years ago

    I’m definitely interested in seeing the reviews and working setups of these suggestions.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • scottiebabe
    scottiebabe over 2 years ago in reply to shabaz

    Being able to use your existing tips is definitely a hug plus! The price point is pretty impressive!

    The pine64 appears to use a BL702 wifi/BT RISC-V SOC from

     image

    I think I have herd of it before but certainly never tried it. There appears to be a number of esp32 like wifi modules based on the bl702 so perhaps sometime I will have to play with one of those!

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • scottiebabe
    scottiebabe over 2 years ago

    If one was proficient in the mechanical side of things, you could DIY your own USB soldering iron (others have). I just tried heating up one of my weller tips which like the TS80P use a 3.5 mm TRS jack.

      image

    It only needed about 2.6W (2.35V @ 1.1A) to get the tip to a temperature where solder melts.

    image

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • Cancel
  • beacon_dave
    beacon_dave over 2 years ago in reply to scottiebabe
    scottiebabe said:
    I just tried heating up one of my weller tips which like the TS80P use a 3.5 mm TRS jack.

    Just don't mistake them for your ear buds... 

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • Cancel
  • scottiebabe
    scottiebabe over 2 years ago in reply to beacon_dave

    usb powered heated q-tips! Heart eyes lol

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Cancel
  • cstanton
    cstanton over 2 years ago

    If I ever get to go to DEF CON I think I'll have to take one of these with me for some badge life hacking. I wonder if airport security will care much for it.

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Cancel
  • baldengineer
    baldengineer over 2 years ago in reply to cstanton

    Everyone that takes gear to DEF CON worries about their local airport security. There are almost no stories of anyone having to give up tools.

    I've traveled around the world with various electronics tools and have never had an issue. In fact, the ONLY thing I've ever traveled with that caused issues was a microphone. Nearly every security checkpoint would ask me to remove it. I asked a friendly agent why. He showed me the x-ray image. On the x-ray it looked like a hand grenade.

    That said, it's not hard to find a free station in the hardware village--even when it seems totally packed! But, I would still at least bring supplies.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • cstanton
    cstanton over 2 years ago in reply to baldengineer
    baldengineer said:
    There are almost no stories of anyone having to give up tools.

    The UK certainly has more excitement with regards to confiscations.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • baldengineer
    baldengineer over 2 years ago in reply to cstanton

    The "keep it charged" reminds me of pre-2001 travel in the US. You could walk through a metal detector with your phone in hand. (In fact, you had to, maybe? Or you put it in a bowl next to the metal detector.) Then you had to show the agent that the screen "worked."

    That was enough for them.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
<>