Personal Blogs
  • Community Hub
  • More
Personal Blogs
Legacy Personal Blogs DAC8775 Quad-Channel DAC EVM - part 5: HART Interface
  • Blog
  • Documents
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: Jan Cumps
  • Date Created: 3 Aug 2018 8:54 PM Date Created
  • Views 5151 views
  • Likes 8 likes
  • Comments 21 comments
  • firmware
  • industrial
  • dac8775
  • hart_network_connectivity
  • ti_rt
Related
Recommended

DAC8775 Quad-Channel DAC EVM - part 5: HART Interface

Jan Cumps
Jan Cumps
3 Aug 2018

For the Instrumentation, Automation and Industrial Application fanboys.

And for anyone interested in communication protocols that are widely used but not commonly known.

 

I'm checking the Highway Addressable Remote Transducer Protocol interface on the DAC8775.

image

 

 

HART Protocol

 

The HART protocol communicates info on a current loop by adding a small AC component to the current loop.

The frequency of that component defines that you're sending a mark (1200 Hz) or space (2200 Hz).

That's all I'll tell about the protocol. The blog is not about how it works, but how to use it with the DAC8775.

Secretly I hope this gets you interested in a widely used industrial communication protocol,

 

DAC8775 and HART

 

From the DAC8775 datasheet:

DAC8775 is also implemented with a Highway Addressable Remote Transducer (HART) Signal Interface to superimpose an external HART signal on the current output.

 

The HART peripheral is only useful in current mode. The HART signal is a communication component added to the current output that DAC is set to.

The DAC8775 implements the physical layer. It doesn't know HART protocol or data handling, but can generate the compliant signal on its output.

In essence, it accepts a sinusoidal signal of 0.5 Vpp, either 1200 or 2200 Hz, and translates that in an AC current component on the output of 1 mA

image

The image above, from the DAC8775 datasheet, shows how the DAC, when set to a  6 mA DC output current, mixes a HART signal of 0.5 mApp to it.

 

EVM Board Modification

 

The evaluation kit used in the element14 Road Test has no breakout point for the HART inputs. On each of the 4 DAC channels, that pin is coupled to ground via a capacitor.

image

I'm using channel A, so I have removed the capacitor for that module's HART input - C58, and soldered a patch wire to the PCB.

imageimage
imageimage

 

 

The HART input signal has to be capactive coupled. The HART pins on the DAC8775 have a DC bias. I used a 0.470 µF capacitor.

According to the data sheet, a value between 10 and 20 nF is recommended. I wasn't in the mood to go look for one.

 

 

Testing the HART Interface

 

There are two things you have to do:

  • enable the HART interface on the DAC in your firmware
  • provide the HART input signal. A sinus of 0.5Vpp, with 1200 or 2200 Hz frequency.

 

To enable the HART interface, you need to set bit 13 of the DAC Config register 0x04.

 

image

In our initial example, we were setting the bit 12 high, because we enabled the DAC output.

So we only have to change that part of the code, and instead of sending 00010000b (0x10), we send 00110000b (0x30).

 

    TX_Data_Master[0] = 0x04;
//    TX_Data_Master[1] = 0x10; // output on, default slew rate without HART
    TX_Data_Master[1] = 0x30; // output on, default slew rate with HART
    TX_Data_Master[2] = 0x05; // slew rate off, 0 - 20 mA mode
    /* Initiate SPI3 Transmit and Receive through Polling Mode */
    spiTransmitAndReceiveData(spiREG3, &dataconfig1_t, 3, TX_Data_Master, RX_Data_Master);

 

We're setting an output current of 10 mA. Or range is from 0 to 20 mA, so we need to set the half of 0xffff: 0x07ff.

 

    TX_Data_Master[0] = 0x05;
    TX_Data_Master[1] = 0x7f;
    TX_Data_Master[2] = 0xff;
    /* Initiate SPI3 Transmit and Receive through Polling Mode */
    spiTransmitAndReceiveData(spiREG3, &dataconfig1_t, 3, TX_Data_Master, RX_Data_Master);

 

That's all for the firmware. If you run it, the HART intrface for Channel A is enabled.

 

I simulate the HART signals with a generic function generator. I set it to sinus 1200 and 2200 Hz. I used my oscilloscope to set up a 500 mVpp output after the coupling capacitor of 0.470 µF.

Then I inserted the signal into the DAC and checked the output. Just like in the previous blog, I used an EEVBlog µCurrent as a load. It translates the DAC's output current into a voltage.

I attached channel 2 of my oscilloscope to the output of the µCurrent.

 

 

image

 

The yellow signal is the HART input, generated by the function generator. It's 500 mV, 1.2 kHz.

The blue signal represents the DAC's output current. Each mA is a mV on the Oscilloscope display.

You see the DC component of 10 mA, and the 0.5 mVpp AC component superposed by the HART interface.

 

For the reader, this isn't spectacular. But in industrial installations, this can be used (and is regularly used) as a digital communication path over the commonly used analog instrumentation current loops.

 

 

 

Related Blog
DAC8775 Quad-Channel DAC EVM - unlicensed roadtest part 1: Raw SPI
DAC8775 Quad-Channel DAC EVM - part 2: Firmware
DAC8775 Quad-Channel DAC EVM - part 3: Slew Rate Control
DAC8775 Quad-Channel DAC EVM - part 4: Current Mode
DAC8775 Quad-Channel DAC EVM - part 5: HART Interface
  • Sign in to reply

Top Comments

  • Jan Cumps
    Jan Cumps over 8 years ago in reply to jc2048 +2
    jc2048 wrote: ... Just like in the previous blog, I used an EEVBlog µCurrent as a load. It translates the DAC's output current into a voltage. Why not just use a resistor to convert the current to a voltage…
  • Jan Cumps
    Jan Cumps over 8 years ago in reply to jc2048 +2
    jc2048 wrote: This HART stuff is interesting. Wonder why they chose a modem standard from 1960-something? ... I can only guess. The 1200 - 2200 Hz standard (imposed on a current) has proven to be reliable…
  • DAB
    DAB over 8 years ago +2
    Nice update Jan. Thanks for showing how to use this embedded communications port. DAB
Parents
  • Jan Cumps
    Jan Cumps over 8 years ago

    The same measurement with a 2.2 kHz signal.

    image

    The amplitude of the HART output dropped with 76 mVpp ... That's 0.13 mA ...

     

    At 3 kHz, we're at 364 mV

    image

     

    edit: and 10 kHz. This is an order of magnitude above the operational range for this chip. Just for kicks ...

    image

     

    for all these captures, I've inverted the HART signal to show the delay better ...

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • Jan Cumps
    Jan Cumps over 8 years ago

    The same measurement with a 2.2 kHz signal.

    image

    The amplitude of the HART output dropped with 76 mVpp ... That's 0.13 mA ...

     

    At 3 kHz, we're at 364 mV

    image

     

    edit: and 10 kHz. This is an order of magnitude above the operational range for this chip. Just for kicks ...

    image

     

    for all these captures, I've inverted the HART signal to show the delay better ...