Personal Blogs
  • Community Hub
  • More
Personal Blogs
Legacy Personal Blogs MIT App Inventor and Arduino Part 2 - send data from Arduino to Android and display
  • Blog
  • Documents
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: neilk
  • Date Created: 18 Jul 2014 4:06 PM Date Created
  • Views 13694 views
  • Likes 4 likes
  • Comments 53 comments
  • android
  • bluetooth
  • hc06
  • mit
  • arduino_tutorials
  • arduino tutorials
  • appinventor
  • arduino_tutorial
  • arduino tutorial
  • arduino
Related
Recommended

MIT App Inventor and Arduino Part 2 - send data from Arduino to Android and display

neilk
neilk
18 Jul 2014

MIT App Inventor and Arduino Part 2 - send data from Arduino to Android and display


I found numerous links via Google for this example; unfortunately a lot of them were the same tutorial posted in different places by the same person. None of them included the Arduino sketch! However, the sketch tuned out to be entirely trivial

 

I won't bother giving any of the links, because the the whole thing is unbelievably simple!

 

Here is the Design screen for the App:

 

                                                              image

The screen is very similar to the previous app, except the On and Off buttons are replaced by 2 Labels: Label2 has the default text of "Data from Arduino" and Label3 is given the default text of "0", in Red with a larger font.


As in the previous App, there is a  Bluetooth Client and we also need to add a  Clock component to act as a timer.  These are both non-visible on the display and are shown below the bottom of the Android device screen.

 

In the Blocks screen we retain the 2 Blocks relating to selecting and connecting to Bluetooth and the Block responsible for disconnecting  from Bluetooth. We  dispense with the Button Blocks.


We then add the following new Block to receive and display the data:

image

In the Design screen, I left the default timer interval on the Clock at 1000mS because we want to have time to actually read the Android display.

 

The Arduino Sketch turned out to be very simple:

 

/*   Demonstration sketch to send data to an Android App via Bluetooth - essentially simple; this is just serial output of integer data.

     The Bluetooth module is connected across the Arduino Rx and Tx lines as before.

      A 10k pot is connected across +5v and ground; the slider is connected to analog input 0, to supply varying data.

 

     Neil Kenyon

     15 July 2014

*/

int potPin = 0;                                  // Define the Analog input

void setup()

{

  Serial.begin(9600);

  pinMode(potPin, INPUT);

}

void loop()

{

    int value = analogRead(potPin);    // read the value of the Analog Input

    Serial.println(value);                     // Print the value; can also be seen on Serial Monitor

    delay(1000);                                   // Don't send too fast or the Android buffer will flood - this worked for me

}

 

This seems to work well enough to demonstrate the ease with which we can send data from the Arduino to the Android App.


Edited on 10 August 2015........problems can arise if the Arduino Transmission and Android Receive delay times are set identically. This wasn't a problem for my set up, but seems to be for others. If you leave the Arduino delay at 1000mS, then reduce the clock/timer delay in App Inventor to 950mS, it should be good image



There are two attachments; the second one - Data_from_Arduino_A.zip does some extra error checking which some Android devices seem to need more than others.

Attachments:
Data_from_Arduino.zip
Data_from_Arduino - A.zip
  • Sign in to reply

Top Comments

  • e14 Contributor
    e14 Contributor over 11 years ago +2
    Thank you for all your help, I have now (after some playing) successfully able to receive accelerometer data via bluetooth to an android device!!!!! Thanks!
  • e14 Contributor
    e14 Contributor over 11 years ago +2
    I found that the following youtube video was very helpful: https://www.youtube.com/watch?v=DkGGilznfG8
  • e14 Contributor
    e14 Contributor over 11 years ago +2
    Hey everybody... Could You Do Me a Favour? I got problem here when I'm trying to make android app using AppInventor2. I'm going to make android app to showed data "TempValue", "MoistureValue", "ldrvalue…
Parents
  • e14 Contributor
    e14 Contributor over 10 years ago

    Sir Neil .... I need help i cant separate the data for humidity and temperature. I want my label3 = Hdata and label4=Tdata image when i run this code humidity and temperature data will display in label3 only image

    imageimage

    #include "DHT.h"

    #include <SoftwareSerial.h>

     

    #define DHTPIN 26     // what pin we're connected to

    #define DHTTYPE DHT11 // DHT 11

     

    DHT dht(DHTPIN, DHTTYPE); //means dht(26,DHT11)

    SoftwareSerial mySerial(10, 11); //means mySerial(Rx,Tx)

    int led = 8;

    int tempmax = 31;

    int tempmin = 30;

     

    void setup()

    {

      Serial.begin(9600);

      mySerial.begin(9600);

      Serial.println("DHTxx test!");

      pinMode(led, OUTPUT);

      dht.begin();

    }

     

    void loop()

      {

        // Reading temperature or humidity takes about 250 milliseconds!

        // Sensor readings may also be up to 2 seconds 'old' (its a very slow sensor)

        float h = dht.readHumidity();

        float t = dht.readTemperature();

      

        // check if returns are valid, if they are NaN (not a number) then something went wrong!

        if (isnan(t) || isnan(h))

        {

          Serial.println("Failed to read");

        }

        else

          {

          //Serial Monitor is available

          

            if (!Serial.available())

            {

              Serial.print("Humidity: ");

              Serial.print(h);

              Serial.print(" %\t");

            

              Serial.print("Temperature: ");

              Serial.print(t);

              Serial.println(" *C");

            }

          

          //Bluetooth Connected to android

            if (!mySerial.available())

            {

              mySerial.println(String(h));

              delay(2000);

              mySerial.println(String(t));

              delay(2000);

            }

          

          }

           // condition for maximum temperature and to ON cooling fan

        if (t == tempmax )

        {

          digitalWrite(led, HIGH);

          delay(1000);

        }

     

        // contition for minimum temperature and to OFF cooling fan

        if (t == tempmin)

          {

            digitalWrite(led, LOW);

            delay(1000);

          }

      }

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • neilk
    neilk over 10 years ago in reply to e14 Contributor

    Hi jefferson.cejas

     

    The problem of sending 2 or more data items from Arduino to Android App and displaying in 2 or more different labels has been addressed in another of my blog posts:

     

    http://www.element14.com/community/people/neilk/blog/2015/02/02/mit-app-inventor-and-arduino-part-4--send-more-than-1-data-item-from-arduino-to-android-and-display

     

    Have a look at that post and reply in that thread if you need anymore help.

     

    Neil

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • neilk
    neilk over 10 years ago in reply to e14 Contributor

    Hi jefferson.cejas

     

    The problem of sending 2 or more data items from Arduino to Android App and displaying in 2 or more different labels has been addressed in another of my blog posts:

     

    http://www.element14.com/community/people/neilk/blog/2015/02/02/mit-app-inventor-and-arduino-part-4--send-more-than-1-data-item-from-arduino-to-android-and-display

     

    Have a look at that post and reply in that thread if you need anymore help.

     

    Neil