Personal Blogs
  • Community Hub
  • More
Personal Blogs
Legacy Personal Blogs The Art of Noise
  • Blog
  • Documents
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: jc2048
  • Date Created: 22 May 2021 10:41 AM Date Created
  • Views 8507 views
  • Likes 14 likes
  • Comments 36 comments
  • transistor
  • 2n3904
  • noise
  • analog
Related
Recommended

The Art of Noise

jc2048
jc2048
22 May 2021

22nd May 2021

 

image

 

I've just been playing with a very simple noise generator and that's the result.

The digital phosphor of the oscilloscope presents multiple traces of the waveform as though it were sketched with a pencil or crayon.

 

In case it's of any interest, here's the circuit:

 

image

 

The internet is full of variations, with either a Zener, reverse-biased LED, or reverse-biased base-emitter junction as the avalanche 'noise diode'.

 

image

 

 

For these traces I used a reverse-biased base-emitter junction (the transistor on the left with two pins connected - the other transistor is working as a common-emitter amplifier)

and it produced a very good level of noise out on a 12V supply.

 

At lower frequencies (the scope is AC-coupled for these), the noise looks quite noise-like. Like this:

 

image

 

but if I go back to the start and show you a single trace of the first waveform, we see this

 

image

 

so we're now looking at a time scale where we can see the avalanching stopping and starting.

 

Update 4th June 2021

 

What started as a throwaway blog about an interesting/amusing waveform seems to have taken on a life of its own.

 

Thanks for all the useful comments below. They've had the useful effect of forcing me to rethink some of this.

 

1. The original circuit that I copied had an integrator (low-pass filter) in the feedback of the common-emitter stage

[the 27k and the 10uF] to set the DC bias voltage. That means that the resulting overall transfer characteristic will

be high-pass [the inverse]. I should have considered that a bit more at the time. If I simulate it with this following

circuit (I've substituted a simple signal generator, with an 8V DC offset on it, for the 'noise diode' which is the input to the circuit)

 

image

I get this for the response

 

image

That won't be entirely right - the simulation is small-signal and the generator is working large-signal - but it lets us

see in a rough way what's happening and understand it in general terms. It falls off from a few hundred Hertz downwards.

That means I'm going to see very little of the low frequency noise as the circuit will integrate it away. Indeed, if I had wanted

to use the generator circuit for audio, it would probably have been better if I had moved the low end cut-off down by

another decade [100uF might do instead of the 10uF].

 

At the top end, that plot shows quite nicely that the response is determined largely by the amplifier transistor running

out of steam and that will depend to some extent on the individual transistor.

 

2. In my reply to Shabaz in the comments, I suggested that seeing the noise decline as I filtered it with the 'scopes

noise filtering meant that it wasn't white noise. That is quite wrong and I need to correct it. Since random noise level

is a function of bandwidth, if I restrict the bandwith, I lessen the noise seen. That doesn't mean that it's necessarily

'white' noise [equal power per unit of bandwidth], but it most certainly doesn't mean the opposite [that it's not].

 

In Motchenbacher and Fitchen, they suggest that avalanche noise is white but that there is also excess noise

in the form of multistate noise that is predominently l/f. This is in a section comparing the noise performance

of zener and avalanche diodes, though I presume a reverse-biased base-emitter junction is similar.

  • Sign in to reply

Top Comments

  • geralds
    geralds over 5 years ago in reply to shabaz +6
    shabaz wrote: Hi Jon, Very interesting blog post, I had not known noise could be generated at these levels with such a simple circuit! Yes, that's an age-old way of creating noise. Simply operate a transistor…
  • fmilburn
    fmilburn over 5 years ago +5
    By coincidence I became interested in these circuits recently, mostly with the idea of making a random number generator. Horowitz and Hill have one in the Art of Electronics but I also found a good article…
  • Jan Cumps
    Jan Cumps over 5 years ago in reply to shabaz +5
    My Tektronic TBS2xxx scope had a reasonable spectrum display. Not magic, but (almost) workable in that frequency range. I gave it away to a makerspace here in Belgium, so that avenue is closed. A SA is…
Parents
  • michaelwylie
    michaelwylie over 5 years ago

    Interesting. Can you show us a spectrum of the noise generated? Maybe 30 seconds worth?

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • jc2048
    jc2048 over 5 years ago in reply to michaelwylie

    This is the low end [10 seconds]

     

    image

     

     

    This is the top end where the gain is rolling off

     

    image

     

    Both of these are dc coupled.

     

    My 'scope is just an old MSO2022B. The FFT isn't all that easy to use and I'm not sure how much I'd trust it.

    • Cancel
    • Vote Up +4 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • michaelwylie
    michaelwylie over 5 years ago in reply to jc2048

    Is the M Channel 25 Hz per division and 500 kHz per division, or is it the entire length?

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • jc2048
    jc2048 over 5 years ago in reply to michaelwylie

    It's per division. The low frequency one is fairly meaningless because of all the aliasing from signal components above the Nyquist limit set for the FFT.

     

    If I enable the noise filter at its lowest setting of 60Hz, we get this

     

    image

     

    which shows us better the artefacts from the resampling of the FFT because we see the interaction with the filtering.

     

    As a way of looking at a low frequencies it's all seems a bit useless (not helped by my own uselessness and lack of understanding, which I'm proudly displaying for all to see!).

    Could I be doing this better, or is this simply the limits of what you can do with FFT on a [moderately] cheap 'scope?

     

    I suppose the best approach to seeing the low frequency end would be to physically filter, before giving it to the oscilloscope.

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • shabaz
    shabaz over 5 years ago in reply to jc2048

    Hi Jon,

     

    I think on that 'scope since 1 Mpoints can be captured, capturing them programmatically and then using (say) Matlab or GNU Octave could be an option, but it's (relatively) a lot of work to do that!

    It seems only the newest 'scopes like the GW Instek one that Frank reviewed recently, have a much better built-in FFT capability.

    Recently I was thinking of finding an alternative way too by coincidence! and looked around for sound cards that could accept down to near-DC input. There are some sound cards like that, but each one had different limitations such as obsoleteness or cost issues : ( so I tried creating a schematic for one. I've completed that, but need to layout the PCB for it, so it's still ongoing slowly! Rainy-day project : )

    Any PC sound card could be feasible, although it would still need the low-pass filtering as you mention, and might have a 10 or 20 Hz cutoff.

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • jc2048
    jc2048 over 5 years ago in reply to shabaz

    I had assumed that a more expensive oscilloscope would do it better.

     

    If I use the 'noise filter' alone, I see this for various filter cut-off frequencies [I missed 1.4kHz, but you get the general idea]

     

     

    image

    image

    image

    image

     

    The noise from the circuit declines as the frequency comes down, and in the area Michael was interested in there looks to be very little at all [practically all aliasing and no actual signal!]. Some [all?] of that is going to be down to the electrolytic that's holding the average bias voltage that the 'noise diode' is then working against to drive the base of the amplifier transistor. As a circuit, it's not looking too good for producing white noise.

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • jc2048
    jc2048 over 5 years ago in reply to shabaz

    I had assumed that a more expensive oscilloscope would do it better.

     

    If I use the 'noise filter' alone, I see this for various filter cut-off frequencies [I missed 1.4kHz, but you get the general idea]

     

     

    image

    image

    image

    image

     

    The noise from the circuit declines as the frequency comes down, and in the area Michael was interested in there looks to be very little at all [practically all aliasing and no actual signal!]. Some [all?] of that is going to be down to the electrolytic that's holding the average bias voltage that the 'noise diode' is then working against to drive the base of the amplifier transistor. As a circuit, it's not looking too good for producing white noise.

    • Cancel
    • Vote Up +3 Vote Down