Personal Blogs
  • Community Hub
  • More
Personal Blogs
Legacy Personal Blogs TI Hercules LaunchPad: using an SD Card Part 3
  • Blog
  • Documents
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: Jan Cumps
  • Date Created: 8 Oct 2015 6:24 PM Date Created
  • Views 4900 views
  • Likes 4 likes
  • Comments 25 comments
  • hercules_launchpad
  • spreadsheet
  • spi
  • texas_instruments
  • sdcard
Related
Recommended

TI Hercules LaunchPad: using an SD Card Part 3

Jan Cumps
Jan Cumps
8 Oct 2015

I'm about to close a long outstanding task: Make SD Cards work on a Hercules LaunchPad.

I've done several half-baked attempts since November 2013. Thanks to persistence (not mine, martinvalencia's), it's finally working now.

 

   image

 

 

This last part of the blog series shows how to enable write to the SD Card. We'll change our project from the previous blog and write some info to the disk.

 

image



Enable the String Write Functionality

 

When you look at the source of the default download of the FatFS library, you'll see that the string functions are grayed out (see screen capture below).

image

 

That's because the lib is configured that way. If you check the ffconf.h file, you'll find this line of code:

 

#define    _USE_STRFUNC    0
/* This option switches string functions, f_gets(), f_putc(), f_puts() and
/  f_printf().
/
/  0: Disable string functions.
/  1: Enable without LF-CRLF conversion.
/  2: Enable with LF-CRLF conversion. */

 

By changing this to:

 

#define    _USE_STRFUNC    1

 

we have access to the string functions.

 

You don't have permission to edit metadata of this video.
Edit media
x
image
Upload Preview
image

 

Writing Data

 

We'll add a little bit of code to the SDTest function that does the write.

A full version of the file is attached at the end of this blog. Use that, because it contains the open_append() function that's missing from the version you installed in Post 1.

 

This code will run at the startup of the controller. So you can read back the data from the command line of your terminal.

 

Look for this code in sd_card.c, at line

 

    // Enter an infinite loop for reading and processing commands from the

 

Paste this write function just before it:

 

#define TEST_FILENAME    "WSLOG.TXT"
    FRESULT res;                /* FatFs function common result code */


    // write some info
    FIL fsrc;                /* File objects */


      /* Open  the file for append */
      res = open_append(&fsrc, TEST_FILENAME);
      if (res != FR_OK) {
          /* Error. Cannot create the file */
          while(1);
      }


      // if file empty, write header
      if (! f_size(&fsrc)) {
          res = f_printf(&fsrc, "temperature;humidity;uv\n");
        if (res <0) {
            /* Error. Cannot write header */
            while(1);
        }
      }




      res = f_printf(&fsrc, "%08u;%08u;%08u\n", 1, 2, 3);
      if (res < FR_OK) {
          /* Error. Cannot log data */
          while(1);
      }


      /* Close the file */
      res = f_close(&fsrc);
      if (res != FR_OK)
      {
        /* Error. Cannot close the file */
        while(1);
      }

 

That's it. When you execure the project,

the code will first see if WSLOG.TXT exists in the root of your card.

If it doesn't, it will create it. Then it opens the file in append mode.

 

If the file is empty, we write a line of header information to it, else we skip that step.

 

Then we create one line of data, and we close the file.

 

image

 

You can see if this worked correctly by typing

 

ls

 

and

 

cat WSLOG.TXT

 

in the terminal.

 

Each time you execute the program from start, the file will grow with one line.

This is how it looks like on my LaunchPad:

 

/> cat WSLOG.TXT
temperature;humidity;uv
00000001;00000002;00000003
00000001;00000002;00000003
00000001;00000002;00000003
00000001;00000002;00000003
00000001;00000002;00000003
00000001;00000002;00000003
00000001;00000002;00000003
00000001;00000002;00000003
00000001;00000002;00000003
00000001;00000002;00000003
00000001;00000002;00000003
00000001;00000002;00000003
00000001;00000002;00000003
00000001;00000002;00000003
00000001;00000002;00000003
00000001;00000002;00000003
00000001;00000002;00000003
00000001;00000002;00000003
00000001;00000002;00000003
00000001;00000002;00000003
00000001;00000002;00000003

 

You can import this file in your spreadsheet program, and it'll show nicely in 3 columns

image

 

Enjoy!

 

Related Blog
TI Hercules LaunchPad: using an SD Card Part 1
TI Hercules LaunchPad: using an SD Card Part 2
TI Hercules LaunchPad: using an SD Card Part 3
Attachments:
sd_card.c.zip
  • Sign in to reply

Top Comments

  • Jan Cumps
    Jan Cumps over 9 years ago in reply to tonofre +1
    The Hercules that I'm using here is not related to the TM4C family - the peripherals are different and work different. My code and explanation in this blog is specific for Hercules family of safety microcontrollers…
  • Jan Cumps
    Jan Cumps over 9 years ago in reply to tonofre +1
    I'm afraid I have no more info for you, Thiago. What's in the blog is what I know. For sd_defs.h: have you downloaded the fatfs sourcecode? Don't use the links in my first post because - as indicated …
  • Jan Cumps
    Jan Cumps over 9 years ago in reply to tonofre +1
    The sd_defs.h that I'm using is available (for RM48 Hercules Controller) in the first link of section: Libraries and Dependencies in the first blog of this series. The link point to a zip archive. The…
Parents
  • caw4
    caw4 over 8 years ago

    Hi Jan,

     

    I'm using the RM48L952 along with HALCoGen and CCS (possibly newer versions but that should be fine) and the SanDisk EDGE 4GB microSD. Anyways, I have managed to get all the way through part 2 of your walkthrough. I can successfully connect through SCI, and I am attempting to communicate with the microSD card. However, when I run my code I get an error message returned to me in my terminal: "f_mount error: FR_NOT_READY". It's fairly obvious that the code is failing when it calls SD_Test(); because that is the only place where "f_mount" is used. FR_NOT_READY is defined by "(3) The physical drive cannot work", which brings me to my question/concern. Does this error message mean that my SD card is ruined? Or does it mean that the commands I'm trying to use are incorrect with respect to the SD card that I am using?

     

    Any clarity that you could provided regarding this issue would be greatly appreciated!

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • Jan Cumps
    Jan Cumps over 8 years ago in reply to caw4

    Calvin, I'll check where and when the error is thrown in the sd card library.

    I'm not an expert in the matter. It just happened to work in my case image.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • caw4
    caw4 over 8 years ago in reply to Jan Cumps

    !So I've worked about as much as I can tonight without my eyes falling out of my head on this project lol. I figured out that I'm getting a response of 0x77 to CMD8 for some reason; too tired and going to bed. Hopefully I can figure this out tomorrow image

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • caw4
    caw4 over 8 years ago in reply to Jan Cumps

    !So I've worked about as much as I can tonight without my eyes falling out of my head on this project lol. I figured out that I'm getting a response of 0x77 to CMD8 for some reason; too tired and going to bed. Hopefully I can figure this out tomorrow image

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
Children
  • Jan Cumps
    Jan Cumps over 8 years ago in reply to caw4

    Can you zip up your CCS project and upload it somewhere where I can download it? I'll have a look.

    I don't have the same Hercules so I will not be able to test it. But sometimes a new pair of eyes can help...

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • caw4
    caw4 over 8 years ago in reply to Jan Cumps

    I LIVE! Anyways... here's a link to a .zip of the CCS project. The main differences to point out are that I am using SPI3 (because that's the hardware I have; not using the HDK) and probably a different microSD card (SandDisk EDGE 4GB). Also, regarding the SPI3 port, I am using CS[5]. Because of this I changed the value in the DESELECT() and SELECT() functions from 0x01 to 0x20 (which I believe is how CS[5] is represented bitwise). I feel a bit overwhelmed and have been stressing about this for about a week now... so thank you for investing your time and offering to help!

     

    https://github.com/TexasInnovations/Capstone/blob/b202738aff7bf8fc7e6d0e99c63aecb4fcee7757/SCI_rti.zip

     

    Just click download from the github page.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • caw4
    caw4 over 8 years ago in reply to Jan Cumps

    Just a quick update! My partner and I managed to figure out that cmd41 is the problem. Also I was wondering, what the 1UL refers to in the arg parameter of send_cmd(CMD41, 1UL << 30 == 0) in the disk_initialize() function of mmc-hercules.c. Any info regarding this topic would be great.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • Jan Cumps
    Jan Cumps over 8 years ago in reply to caw4

    I'll rebuild my setup and try.

     

    We'd have to get a MMC protocol document to find out what's happening and why. Same as you, I have no clue.