Personal Blogs
  • Community Hub
  • More
Personal Blogs
Legacy Personal Blogs YAPS Part Twelve - Design revisited: reworking the layout and PCB
  • Blog
  • Documents
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: Andrew J
  • Date Created: 11 Aug 2019 7:22 PM Date Created
  • Views 3684 views
  • Likes 9 likes
  • Comments 29 comments
  • bench_power_supply
  • bench power supply
Related
Recommended

YAPS Part Twelve - Design revisited: reworking the layout and PCB

Andrew J
Andrew J
11 Aug 2019

Two things became very clear to me once I got into the detailed testing of the project:

  • I have completely stuffed up the grounding and layout of the components.  In particular the Switching Regulator has a convoluted route back to Vin -ve and the route it does have takes it right under the sensitive components (until I bodged in a couple of wires).  Layout is too far apart for many components, including the bypass and decoupling caps, and non-conducive to managing noise.  There are no test points with the result that I have blown a number of components including 3 ports on the very expensive 4Duino.
  • I really didn’t have enough knowledge about DC-DC Switching Regulators - I sort of hinted at this in my design post - which becomes clear as you read the answers to some of the advice being given.  In some respects that might be a good thing as maybe I wouldn’t have started on this!  However, I apologise to those who have graciously helped out nonetheless and hopefully I've at least made a start in remedying that.

 

On the plus side, testing showed that functionally it works so I can get my 0-15V, 0-3A out.  I set about sorting out my understanding so that I could properly layout the board, but also have a much better understanding of how that part of the circuit is working so I can properly probe and test it.  There is excellent coverage of the subject from Micro-Rohm, starting with Switching Regulator Basics, that covers DC-DC switchers in some detail but at the same time keeps the language easy to follow.  There are also a multitude of papers from TI and Analog and the data sheets for buck converter ICs have been helpful - the LT1624 datasheet is still confusing though.

 

The design is still basically the same, with most changes to the Switching Circuit and Linear Regulator Circuit.

 

Switching Circuit

Essentially the same but with the following changes (annotated in red):

 

image

  1. Test points for the LTC1624 pins and output at the inductor
  2. A placeholder on the gate driver (pin TG) for a small resistor, R2, to adjust the rise time of the MOSFET to help counteract ringing if necessary.
  3. A placeholder for a boost resistor, R3, (pin BOOST) at the switching node to help with ringing there, if necessary.  Possibly a ferrite bead rather than resistor.
  4. A placeholder for a Snubber at the switching node, R5 and C9 ( to help with switching noise if necessary.
  5. A placeholder for a ceramic capacitor on Vout, C15, if I want to experiment with adjustments there.
  6. Upsized the sense resistor to a 1206/500mW part, same 10mOhm resistance.  Takes a bit more area but should be more resilient than the 0805, particularly as I’ve blown it up 3 times!  I’m mostly thinking of ease of replacement.
  7. Upsized the inductor to 50uH: the part I’ve chosen has better specs for resistance, self resonance frequency and saturation current than the original 10uH part (although in fairness, the other part’s specs should have been ok.)  LTSpice simulation shows that ripple on the output - and through the Feedback Circuit - is significantly improved.
  8. The MOSFET is now a SMD component - IRF8721 - with the same (slightly better) specs than the TO220 IRLB8721.

 

The main concern for the MOSFET was a power dissipation characteristic of only 2W.  I did some soak testing for temperature gain of the existing MOSFET and calculated wattage from that - see below.  The TO220 package doesn’t take up a lot more space than the SMD component (considering just the leg soldering area) but it is a lot more awkward to position and route to.  I did vacillate a bit on this as I know the existing part works : I’ve replaced the existing Mosfet 3 times - once when I blew it up, once when I swapped it for a better part, and once when I de-soldered it for testing when I thought I might have damaged it.

 

The resistor placeholders R2 and R3 will be populated with a 0 ohm (<5mOhms) resistors initially; R5 and C? will remain unpopulated.  Depending upon what I see during the testing I can populate one of more of these placeholders with actual resistors/ferrite beads and resistor and capacitor in the case of the Snubber.  My understanding is that care is needed with changing the MOSFET timing (BOOST and Gate resistors) as it will increase the switching losses.

 

MOSFET Temperature Soak Testing

I ran the existing circuit at a range of volts and amps for an hour - 50 mins with the 5Ohm load as I had to leave to do something else and didn’t want to leave it unattended - and captured temperatures at 10 min intervals.  I took the peak temperature for the IRLB8721 MOSFET and using the original Ambient Temperature and the MOSFET’s Tja specification, calculated the power from the temperature rise (temp diff / Tja).  Even in the worst case temperature rise, power dissipation was 0.333mW, well within the replacement's power dissipation rating even after de-rating to 150C.

image

image

image

I’d be very interested to hear feedback on this.  I could switch it back to the TO220 package before I get the board made if I’ve messed up the calculations.

 

Linear Regulator Circuit

Again, essentially the same but with the following changes (annotated in red):

 

image

  1. Test points for the LT3081 pins
  2. Placeholders for addition ceramic capacitors at the input to the regulators, C18 and C19
  3. Placeholders for Ferrite Beads,  R13, R18 and R19, to help with ripple and frequency noise, if necessary.  These will initially be populated with 0Ohm resistors.
  4. Moved the Schottky Diode from the Current Source circuit into the Linear Regulator circuit.

 

The placeholders for Ferrite Beads are interesting because I have to take into account component sizes as well as their placement on the high-current path.  Scanning around on Farnell, CPC, RS, Digikey, getting a correspondence of size between 0Ohm resistors and Ferrite Beads (at this stage I don’t know if I need them nor what specs if I do) is nigh-on impossible.  So I’ve gone with a 2512 (6.4mmmx3.2mm) size resistor and custom-sized the pads so that 1812 ferrite beads can be used - this seemed to give me the best tradeoff in size correlation.

 

PCB

Hopefully the images I've pasted are viewable but I've attached the Gerbers as well.  With the layout needed, I've gone with a 4-layer board to achieve it - it's a bit more expensive but for the sake of £20-ish it feels worth it given the difficulty of trying to do this with 2-layers, at least that's how I perceive it.  It's also resulted in a slightly larger board at 100mm x 95mm (current version is 100mm x 75mm.)

 

Layer Stack

Top: components, high current traces, high current ground traces, signal traces

Layer 2: Shield Ground

Layer 3: Signal Ground

Bottom: Signal traces

 

Test Points

I’ve added in pins for testing of components that have caused me great difficulty in the past:

  • The Switching Regulator pins: I’ve separated out the Switching and Boost pins from the more sensitive pins.
  • The Mosfet gate pin: I will want to be measuring ringing and noise at this point.
  • The Linear Regulators
  • The Current Sense INA260: both Vin and Vout from that chip

I’ve taken the approach of using pins that I can actually either clip a probe to or stick the probe tip into; each has an associated ground pin into which I can insert the short, springy probe ground to avoid have a large ground wire affecting measurements.

 

Ground Plane vs Star Ground

Before I get into the layers in more detail, I want to start off with this as it’s come up a bit in comments.   As I researched this it became clear that TI, Analog, Micro-Rohm and others all recommend ground plane; however I cannot also ignore Gene’s comments and advice, which comes from experience, to avoid these and use Star Ground.  So where does that leave me: I don’t yet have the experience of implementations (of both approaches) to determine which would be best nor can I make multiple boards with different configurations - the costs are just too high.

 

So, I have to make a decision and what I’ve gone with is the advice from TI, Analog, Micro-Rohm:

  • All high current ground traces are on the top layer except for two places where I had to go down to layer 2
  • Layer 2 is a Shield Ground which connects solely by the -Ve PCB terminal for Vin.  There are no other connections to this layer.  However, there are vias and through-holes plus the two high current traces that needed to be routed off the top layer.  There is also a Keep-Out underneath the Inductor (L1).
  • Layer 3 is a Signal Ground layer which connects solely by the -Ve PCB terminal for Vin.  There are no other traces on this layer but there are, obviously, connections for all low-current components.   There are also through-holes and vias and a Keep-Out underneath the Inductor (L1).

How does one avoid creating TH 'slots' (holes in a row) in these layers?  I have no idea.  Quite a few come from the test points I’ve incorporated: even using SMD points would require vias for the ground pins unless I avoided those.

I’ve avoided Thermal Vias as testing to date shows that’s not necessary and it would make more holes through the layers.

 

Check list

Now I have a better understanding of the Switching Regulator, I’ve been able to take a better understanding of layout practices from my reading of data sheet layouts from TI and LT (Analog) as well as the explanation and points presented by Micro-Rohm:

  • Keep the bypass capacitor (Cby1) as close to VDD of the switching regulator as possible.  TICK
  • Keep the loop consisting of Input Cap (Cin1), Sense Resistor (R4), Mosfet (Q1), Schottky Diode (D1) as short as possible.  TICK
  • Keep the loop consisting of Schottky Diode (D1), Inductor (L1) and Output Cap (Cout1) as small as possible.  TICK
  • Traces carrying high currents off the ground plane and away from the sensitive feedback circuit.  TICK
  • Keep the Switching Node - SW pin, D1, L1 and Q1 Source small.  TICK.
  • Use kelvin connections from the feedback circuit connected just after the Output Capacitors.  Vfb should connect directly to the resistors.  TICK
  • Feedback circuit should be connected to the + plate of Output capacitor.  TICK - actually, there are more than one output capacitor and it connects just after the last one as per TI advice.
  • Keep the connections from feedback resistors to the Vfb pin (R6 and R7 - and really also Q2) short and away from the Switching Node.  TICK
  • Gate drive trace should be as close as possible to the Mosfet (Q1) gate.  TICK.  in my opinion - given ‘close’ is relative and I can’t physically get the larger parts any closer!  Part manufacturers don’t help with their pin layout either.
  • Signal and Power Grounds separated.  TICK
  • Does the input capacitor (Cin1) +ve connect to Sense Resistor (R4) as closely as possible. TICK
  • Does Cin1 connect as close as possible to GND pin of Switching Regulator.  TICK - in as much as this makes zero sense as their grounds are meant to be kept seperate!
  • Is ground of Cin1 and Cout1 separated by at least 1-2cm. TICK
  • Is the Inductor (L1) close as possible to the Switching Regulator.  TICK
  • Is the wiring to the Inductor input as small as possible.  Is the wiring distance between the Inductor terminals as great as possible. TICK
  • Are there no ground or signal traces under the Inductor.  Is the Ground Plane kept from underneath the inductor. TICK
  • Are the Inductor and Output Capacitor (Cout1) as close as possible.  TICK
  • Signal and Power Grounds must be kept separate.  TICK
  • Top Layer Power Grounds and Inner Layer Power Grounds must be connected by numerous vias.  TICK (there are only two places where I have routed Power Ground to the inner layer.)
  • Power Ground should be connected to a common ground or signal ground near an Output Capacitor.  NO TICK - grounds and ground planes are connected at one point only near the Power in terminal, based on discussions/advice here.  I believe this point is based on the grounds for the Switching Regulator only, not the 'load circuit' - I have done that with the feedback circuit and IC GND connections.

 

Quite a substantial checklist but I think I’ve hit them all including the last point.  The grounds are tied at the -Ve pin for VIn but in Kicad I can only do this with a Net tie component - it’s not possible to specify a pin or pad as belonging to multiple nets.  You can see the Net tie in the PCB top layer by the -Ve pin of the PCB terminal.  I think this is ok - any noise from power ground that hits the Shield Ground would route out here.

 

Silkscreen and Solder Mask

To make it easier to see some of the following images, here's just the silkscreen and solder mask:

image

 

Top Layer

image

(Green traces are bottom layer traces)

High Current traces, shown with green arrows, route along the right, bottom and right side.  Ground traces, shown with cyan arrows route in a similar manner: where I have ducked down to layer 2, dashed cyan arrows, (the Shield Ground) I have used vias to connect the traces - I've just noticed that the fourth short arrow at U3 should be a dashed one.  These are 0.508mm diameter with 0.254mm drill but would it be worth making them bigger?  The check list calls for “numerous” but could I do with fewer of them to reduce via holes through the layers?

 

Components are placed quite close to each other - much closer than in the last version.  It looks do-able hand-soldering.  In particular, the feedback circuit is well away from the power traces and route through traces to just past the output capacitors.  You can see that I route the GND return under the power ground (on the signal layer) to connect there by the output capacitors as well - it is equally possible to connect at the point it ducks down but I’ve kept the traces together as recommended by the check list.

 

Shield Ground Layer

image

This is intended to keep noise away from the non-power components although I could well have misunderstood the concept.  Nothing directly connects to this layer except the NETTIE so it isn’t directly used by anything as a path to ground.  Should I have limited the area to under the high-current traces only?

 

Signal Ground Layer

image

This is used as a ground plane by the non-power components - i.e. those not directly related to carrying high-current to Vout.  There are multiple connections on this layer but no traces.  All the cheaper manufacturing companies preclude the use of blind or hidden vias so they all route through 4 layers.

 

Bottom Layer

image

This carries signal traces that can’t route on the top layer.  There’s not that many of them really.

 

Summary

I think I’ve made a much better job of laying out and routing the design this time.  The first version was so bad it wasn’t even worth trying to start dealing with the sources of noise but my hope is this will prove capable of proper measurement and action: the placeholders for ferrite beads/capacitors/resistors can at least allow some modifications to be made as a result and the test points will prevent me blowing components up.  I'm more than happy to provide additional information if anyone is interested.

 

A summary of my questions:

  1. Would it be advisable to swap the MOSFET back to the TH version I used before which is more capable of dissipating power?
  2. Is the use of TH pins for the GND connection with my test points - so I can use the short GND wire on my probe - better than removing those holes through the planes?  Alternatives would be to use SMD test points with vias (smaller diameter) or doing away with GND test points and using the longer crocodile clipped GND wire.
  3. Layout guidance uses a lot of relative terms such as ‘close’ and ‘as possible’.  Is the trace from the Switching Regulator (U1) to the gate of the MOSFET (Q1) too long?
  4. The GND connections for the feedback circuit, Switching Regulator and the ITH/Run pins route around to connect to PWRGND just past the Output Capacitors (one piece of advice read.)  Would it be better to route these directly to the +ve and =ve pads of Cout1 - the 100uF output capacitor (another piece of advice read.)
  5. They don’t just connect to PWRGND just past the output capacitors, they also route under PWRGRND to do so: I could avoid doing that and connect at the point the trace jumps down.  Is it better to leave as-is?
  6. The PWRGND traces all route back on the top layer to the -Ve pin on VIN.  Very close to this point is the single connection for Shield Ground and Signal Ground.  Would it be better placing this nettie close to -Ve pin on Cout1?
  7. The Shield Ground is the full size of the board.  Should I just place this under the high-current routes or does it not make any difference?
  8. From experience, does this look hand-solderable if care is taken with the order of placement of components.
  9. I have no copper fills on the front or back layers.  If I added these and tied them to the nearest ground plane the vias would pass through all 4-layers.  Ultimately, I don’t know if it would improve anything so I didn’t bother as more holes in the layers seems ‘a worse thing’ but am I wrong?

 

I’d be very interested in thoughts and observations on my approach so I don’t make the same mistakes as last time.  In particular, given that grounding was a major issue in the current version, what’s your views on how I’ve done this time.

 

Next: Part Twelve Reprise - Design revisited

Back: Part Eleven - Further Testing

Attachments:
YAPSv12Gerbers.zip
  • Sign in to reply

Top Comments

  • shabaz
    shabaz over 7 years ago in reply to Andrew J +4
    Hi Andrew, Given the tip size and iron rating, your settings are in the right ballpark for SOIC.. maybe the temperature can be raised slightly. I too use a ~1mm tip, and set to 330 degrees C, for 2 or…
  • Andrew J
    Andrew J over 7 years ago in reply to shabaz +4
    Thanks - I'll give it some thought along with what I'm going to do. At the moment, it's not going well enough for those to help I have the circuit re-assembled and I can now get 15V /1.5A with the 10Ohm…
  • shabaz
    shabaz over 7 years ago in reply to Andrew J +4
    Hi Andrew, I think they could all be related to one issue perhaps, because things like the linear regulators should be behaving identically, since it's the same circuit for each of them, just paralleled…
  • jc2048
    jc2048 over 7 years ago in reply to Andrew J

    It's not easy. I still don't find grounding, shielding, and all this kind of thing straightforward. That's

    because you quickly move away from a schematic that shows simple topology [how things join together] to having to

    get your head around physical, 3D structures where you have to imagine the voltage fields or magnetic fields that

    exist because of the physicality of it and understand how charge distributes itself.

     

    I was actually focussing on it in an EMC kind of way - you look for the noise sources and then at how they might

    radiate (possible aerials) or conduct (paths to longish cables). So I was quickly taking you to the top of the

    list for noise sources. With EMC you think in terms of power, so a high current or a large voltage swing

    switching fast is an obvious candidate.

     

    There's EMC literature that's relevant to what you're doing and might help you, so you ought to consider reading

    more widely than just the applications stuff on switchers.

     

    As to Vin [and the output to the linear regulators and their input capacitors, which an extension to the output

    loop], you have to take a view as to how good a job you've made of the converter's input and output capacitors in

    terms of capacitance and ESR [and layout]. Ideally the switched circulating current doesn't come from the input,

    but only from the input capacitors, with the input current being more continuous, with the current either

    assisting the loop or recharging the capacitor. Of course that's a bit of a fiction, but it's what you should be

    trying for, even if you're going to fall short.

     

    "as a rhetorical side thought, is it reasonable to think the AC noise would follow under the forward trace back

    to the nettie, away from sensitive components, rather than head direct like DC?"

    Yes. I didn't spot that [I've just failed the exam, haven't I!]. The top will try for the same path (or vice

    versa) to minimise the loop inductance if it can, but it's not perfect and if there's a plane (rather than a

    track where the path of the electrons is forced) there is some spread [imagine it as like a normal distribution

    with the top of the curve under the track above, but then spreading either side]. Also, the vias aren't very good

    at carrying rf signals, so that mess things up somewhat and so, all in all, I don't think the path on the shield

    would be as clean as your line suggests. There's also the problem under the controller where your ground

    constricts. That's going to look inductive and I suspect many of the high frequency photons will balk at that and

    just cheerfully skip the corner (not sure what effect that would have underneath in the shield).

    How the path establishes itself is interesting to think about. I suppose it is like a transmission line where the

    signal and the return work their way along with a displacement current at the head of the wavefront. When they

    get to the via, if there's a way through they take it, and if not the signal will reflect. In this case the vias

    aren't too wonderful at conducting the fast edges, so there will be a fair reflection. That process isn't limited

    to the path to the vias, so presumably you have signals shooting off wherever there are tracks to carry the top

    current, reflecting off of deadends and so forth, so it's not surprising that the spike noise is so disruptive.

     

    It doesn't seem to me, thinking like this, that your shield is doing much for you at all - it's actually

    supporting all this mayhem. It does shield the layer below it, but then a power plane would, too - that's just

    thickness of metal and resulting absorbtion.

     

    I'll have a think about the layers business during the day. Semiconductor manufacturers tend to be focussed on

    designs on boards with high-speed logic where power planes are absolutely necessary and the converters then have

    to work in with that. But you don't have to follow that as it's not a constraint for you, so you might consider

    something more innovative with the return (power ground) on a layer under. But I think what will get you is the

    behaviour of the vias - what you would gain by having the return underneath minimizing the inductance, you

    probably more than lose with the via inductance. [Wouldn't it be wonderful to have the money, and the time, and

    the right test equipment to try out all the possibilities and find out how much truth there is in all this

    blather I'm churning out.]

     

    Back to layout, here's how I would have initially sketched out a possible design if done on the top layer. Hope

    that's clear - the green lines outline the areas of copper.

     

    image

     

    Here it is again with the current loops on it

     

    image

     

    That minimises the loops fairly reasonably. It gets the controller and the feedback circuit out of the way. The

    gate drive and the Kelvin sense aren't too bad. Leaves an issue with the controller ground and where it ties in.

    If you had it on a board with planes, you could have a bunch of vias in the middle of the ground area to tie it

    down to the board ground planes - that then gives you a single-point ground for the converter's power.

     

    Aside: I think you can get sense resistors in a low inductance package (the connections will be to the long edges

    rather than the short ones). That might be worth looking at. Alternatively, you could have two in parallel to

    reduce the inductance a bit.

     

    Do you have a reference for the not-putting-the-capacitor-grounds-too-close thing handy? I'd like to read it.

     

    Does your rationale for moving to a much slower converter still hold given that you now have a board full of

    surface mount parts?

     

    Final quick thought - the LT board had areas of copper next to the MOSFET tied with vias. That looked to be

    heatsinking for the MOSFET - couldn't see any other purpose for it (though I thought the bulk of the heat

    normally came via the source connections, so it doesn't quite add up). You might want to make sure your part can

    handle the dissipation by itself [bearing in mind you only have 5V of gate drive and won't necessarily achieve

    the headline Rds(min) figure].

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • Andrew J
    Andrew J over 7 years ago in reply to jc2048

    Thanks Jon - I would never read it as a ‘lecture’ so don’t worry, I get a lot out of your responses.  And if it helps, I’ve been cramming a lot on this and can tell you you’re right about the loops.  Almost image  There are three (blue) loops - Vin, Cin and Bypass - formed when the MOSFET is on, and one when it is off (Yellow.)  In retrospect, it would have been useful to have put these on originally.

    image

     

    The trick, worthy of The Great Mephisto, is to keep ALL on and off loops as small an area as possible AND keep the switching node (your yellow loop) as small as possible AND have power components away from the sensitive circuits AND have the bypass cap butted up to the Regulator by its VIN and GND pins(!) AND keep the gate trace short AND connect the IC to PGND and SGND simultaneously AND AND AND….  At some point tradeoffs get made: notwithstanding The Great Mephisto, the trick I need to get right is to make the right tradeoffs and not the wrong ones!

     

    You’ll see from the above image I’m still playing with layout and I’ve been thinking about it all day whilst wandering around some dead person’s country pile.  However, one of the no-nos is to have Cout too close to Cin - there's that relative term again, but in this case close means 1-2 cm.  This is to prevent high-frequency noise passing through Cout into the output.  Having said that, my first thought to play with at the moment is to shift the test terminals, flip the inductor -90deg put the Cout Caps there and drag it all in somewhat - pretty much what you say about getting Cin and Cout closer together, but not too close!   Except no matter how I route it, those Ground traces are going to bend unless I route it down a layer and I was really trying hard to avoid that in the Switching Regulator part of the circuit.  You know, when you read this stuff and they image their recommended layout, the imaginary Regulator they choose to use to do so has the pins in precisely the right location to make it work!  Little @£$!$.

     

    However, what you have highlighted in particular, is the yellow stalk (or the green arrows on my image) - as a rhetorical side thought, is it reasonable to think the AC noise would follow under the forward trace back to the nettie, away from sensitive components, rather than head direct like DC?  Would it/could it couple back up a layer again into sensitive circuits (none are connected to that Shield layer)?  I’m still researching the Shield Ground (and grounding/layout in general for SMPS) as I’m still not sure what it is when it is referred to.  Actually, the real problem is, fundamentally, that there is ZERO consistency in approach recommendations by anyone, even TI have two different recommendations: ground traces on the top only and use a ground plane.  However the consistent message I do read and do understand but still have to constantly bang my head on the desk to get it to sink in is that currents will return to their source.  I’d put the Shield Ground in precisely to pick up capacitive, or otherwise coupled, noise (which is what I had interpreted it as ) and route it back out, again failing to bang my head on the desk long and hard enough that the source isn’t always the +Ve and -Ve terminals.  So any noise coupled to Shield Ground HAS to go to that net tie to get back to source (my green arrows): not dissimilar to one of the problems with my original design.

     

    I did laugh at the brilliant or awful comment though: and you’re right again - either there’s no noise on that layer and it doesn't matter or it’s bonkers and I’m back to square one.   Anyway, it needs sorting in case it is a problem.   I’m still researching and still think that  top level traces are a good recommendation but that Shield Ground needs tieing at different points.  Specifically, I’m looking into advisability (or not) of tieing it at the output capacitors and Schottky and Input capacitors although that will turn it into an actual ground plane which would negate the purpose of return traces on the top layer - which unsurprisingly is both for and against recommendation depending who one is reading!  Anyway, in summary, looking into making these pesky electrons go where I want them to rather than it being a galactic free for all on my board.  The Signal Ground is connected to components so it doesn’t matter so much that the nettie is at the power in terminals - I think, I’m still looking into tieing it in at Cout (least noisiest point in theory) - I just need to track and if necessary adjust the traces vs ‘slots’ on the bottom layer so there is a clear route to source.

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • jc2048
    jc2048 over 7 years ago

    So 'Z' grounds are good after all?

     

    I don't know if this will help the discussion, but I've drawn the switching currents for the regulator circuit on your layout in orange.

     

    image

     

    This is my understanding of what's going on, but I'll just say I wasn't taught this stuff formally so don't rely on what I'm saying and feel free to question it. Like many engineers, I ended up having to deal with switching circuits but haven't gone much beyond using them as POL on digital boards and as LED drivers [in both situations you tend to follow recommended layouts and do a bit of extra filtering to get past EMC, and neither is as challenging as the more analogue-like thing you're trying for

    here]. This will sound like a lecture but believe me it isn't.

     

    The small 'dashed' arrows indicate where the switching currents switch on and off. The continuous stretches are where the current ramps up and down giving current ripple (assuming it's working in continuous mode). There are two loops corresponding to whether the MOSFET is on or off - remembering that the Schottky is also a switch (albeit not controlled directly by the controller) - a large loop and a small one. To keep the noise down, you need to minimise the inductance which you can do by minimising the area of the loop. You particularly need to try and minimize the inductance in the large loop you have here. You need to minimize the inductance because it's going to generate a voltage spike when the current abruptly stops [the parasitic inductance will get rid of its stored energy by generating an emf and coupling the energy elsewhere].

     

    The other major noise generator is the switching node which I've outlined in yellow. The voltage waveform there has an amplitude of the full supply voltage and is driven with a high current so the edges will readily capacitatively couple to anything it can develop a voltage field with. In your case that's mostly the 'shield' layer. I'm very unsure of the next bit, but I think that might result in charge mainly moving across the shield from/to the tie point [yellow line], so potentially there might be coupling back up in the area you've marked as feedback. I'm unsure because I can't really quantify it. The plane is metal and a low impedance but it takes time for the change to propagate across. The edge rate will be crucial to all this and given the reverse capacitance of the Schottky it probably can't move fast enough to give the kind of problem I'm envisioning. And now we have a current on the go - remember currents flow in loops - we need to think what is driving it and where does the return go on the top surface.

    The return presumably either flows through the power ground, 'through' the output capacitors, to the other end of the coil when it's that that's driving the change or to the input capacitors when the MOSFET is driving the change. You can see how convoluted this stuff gets and how you tie yourself in knots with it. Anyway, what you've done with the shield may be brilliant or it may be awful (but I'm not sure the input is the place to tie it).

     

    To be more practical, rather than analyse this to death, I'd suggest you might try alternative layouts on a piece of paper. You could probably manage something where the grounds of the input and output capacitors were much closer together and not at the extremes of a 'Z'.

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • Andrew J
    Andrew J over 7 years ago in reply to genebren

    I appreciate you pointing it out as there were other things to tidy up there which were less noticeable until I removed that bit of the trace!  A 1.9mm width trace over that distance results in a 7mV drop with a resistance of 2mOhms but as it's a ground trace I don't think I need to worry too much about that. 

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • genebren
    genebren over 7 years ago in reply to Andrew J

    Andrew,

     

    When I was looking at the routing, I was doing it without any measurements.  I just noticed what looked like some bottle necking in the area under U1.  If the trace width is sufficient for a 10c rise, then that should be good enough.  My personal experience is temperature rise is only one aspect of trace width.  As the trace width decreases, the resistance rises, as the resistance rises, the current spikes are able to create great voltage drops, which in turn increases noise.

     

    Given all of the issues with the prior PCB, I would exercise caution.  I would have rules (recommendations) that I follow, i.e. keep high current ground routing on the top surface .  If you have doubts about transferring the signal (under U1) into the shield ground layer, then do not do it.  It would be easier to beef up the trace later (with a wire bridge) than to remove one from the inner layer.  Vias have issues, and they thin out the outer layer trace (like swiss cheese), so I'd say play it safe and avoid them unless absolutely necessary.

     

    Good luck!

    Gene

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • More
    • Cancel
<>