Personal Blogs
  • Community Hub
  • More
Personal Blogs
Legacy Personal Blogs
  • Blog
  • Documents
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New

Legacy Personal Blogs

Please Note:

This blog contains the legacy personal blog posts of our members, other than our Top Members whose content has been migrated into individual blogs in this area. Our new platform does not have personal blogs so this is how we have preserved the personal blog posts of our members from the Jive platform. No new posts will be permitted in this blog. Instead, if you wish to create blog content, please post it in the blog in the most appropriate topic area.

  • Tags
  • Subscribe by email
  • More
  • Cancel
  • led 25w

    e14 Contributor
    e14 Contributor
    Although the LED is a current device - led power 10w  is no exception, but the car tail lights, brake, turn signal lighting applications can still benefit from the voltage drive structure.Efficient LED available, retail and residential LED inter...
    • 11 Jun 2012
  • Inductive Sensors

    e14 Contributor
    e14 Contributor
    15 Series - Inductive Sensors WERNER'S 15 series inductive sensors offer innovative, high quality to meet almost any application in automation and process control industries. Our rich experience, flexibility and exceptional customer focus continues ...
    • 11 Jun 2012
  • Wireless Remote Controllers

    e14 Contributor
    e14 Contributor
    66 & 67 Series - Wireless Remote Controllers WERNER's 66 & 67 series wireless crane controllers provide the highest quality combined with ruggedness, usability and flexibility in the industry. The rugged remote controllers have been a gr...
    • 11 Jun 2012
  • Une victoire de plus au Palmarès !

    Polyjoule
    Polyjoule
    Bonjour à tous !  Après ce retour de Rotterdam perturbé par les examens (faut-il le rappeler nous ne sommes que des étudiants !), une petite publication pour vous faire parvenir nos résultats finaux avec quelques images ! Mais avant toute c...
    • 11 Jun 2012
  • led 400w

    e14 Contributor
    e14 Contributor
    The reason is nothing more than the two cases:First, the LED leakage current caused by the PN junction failure, so the point of LED light does not shine, this generally does not affect the work of other LED lights;Second, disconnect the internal conn...
    • 9 Jun 2012
  • LED Floodlight 80W

    e14 Contributor
    e14 Contributor
    After 2011, the LED gradually to enter the interior lighting, this also means that march to civilian families. On the one hand, this is a happy occasion, because the civilian market is very large; the other hand, is a very serious challenge, particul...
    • 9 Jun 2012
  • led 550w

    e14 Contributor
    e14 Contributor
    Light-emitting diode (LED) lighting for the unconventional, comfortable and customized open a new world. These design opportunities in the rapidly enhance the extent and speed of the application of LED in the car. When the led 1w   in the c...
    • 9 Jun 2012
  • led 20w

    e14 Contributor
    e14 Contributor
    Want to do high power led  lighting products are the most critical part is I do not know, that is equipped with optical, structural, electronic, popular with light, structure, electronic jargon expression as follows: optical properties, thermal ...
    • 8 Jun 2012
  • led floodlights 40w

    e14 Contributor
    e14 Contributor
    Blue LEDRefers to the blue light-emitting diodes. The center of the emission wavelength is around 470nm. For lighting fixtures and indicators shown in blue part of the light source, the blue light of LED display and LCD panel back-illuminated light s...
    • 8 Jun 2012
  • led floodlights 10w

    e14 Contributor
    e14 Contributor
    Point of view twenty billion global light bulb market aspiring cut-off in the incandescent lamp in 2012, the lock-up the specifications on the road, despite the penetration of energy-saving fluorescent lamps (CFL) still prevail, and then in the globa...
    • 8 Jun 2012
  • LED 40W

    e14 Contributor
    e14 Contributor
    First, the status LED North American standardsLED energy-saving lamps, as a new product, the current North American product safety standards do not specifically for this type of technology requirements, testing of LED products become a topic in the i...
    • 7 Jun 2012
  • LED Spotlight 30W

    e14 Contributor
    e14 Contributor
    The manufacturers of most of the publicity is the LED Floodlight 80W  lamp life of 50,000 hours, the whole lamp life of 35,000 hours. Practical application to be influenced by many factors, not reach the theoretical value. With the non-stop prog...
    • 7 Jun 2012
  • LED 30W

    e14 Contributor
    e14 Contributor
    The data from the Guangzhou International Lighting Exhibition displays, led 1w become one of the venture capital and private equity investment is the most favorite in industry, only Wu Sonny and he led by GSR Ventures has invested 8 LED business. Bu...
    • 7 Jun 2012
  • LED strip lights

    e14 Contributor
    e14 Contributor
    The light-emitting diode (LED) is used for building the next generation of lighting and interior lighting components, light-emitting energy efficiency incandescent lamp is much higher, however, must be dedicated electronic driver circuit to ensure no...
    • 6 Jun 2012
  • LED Flood light 20W

    e14 Contributor
    e14 Contributor
    To note that the anti-moisture and dumped into the specifications, protection class of IP (INTERNATIONAL PROTECTION) by the IEC (INTERNATIONAL ELECTROTECHNICAL COMMISSION) the drafting of led driver 120w     applications. Fixtures will...
    • 6 Jun 2012
  • led power 35w

    e14 Contributor
    e14 Contributor
    The light-emitting diode (LED) is used for building the next generation of lighting and interior lighting components, light-emitting energy efficiency incandescent lamp is much higher, however, must be dedicated electronic driver circuit to ensure no...
    • 6 Jun 2012
  • led power 25w

    e14 Contributor
    e14 Contributor
    Compared with the vehicle's interior and exterior lighting solutions, LED lighting has many advantages such as higher performance, longer life, lower cost, this way of lighting and automotive lighting aesthetics and performance. However, want a car b...
    • 5 Jun 2012
  • led floodlights 20w

    e14 Contributor
    e14 Contributor
    Today, the white LED is still the existence of luminous uniformity is poor, the closed material life is not long, but can not play to the advantages of LED Flood light 10W  applications are expected. Demand perspective, not only the general ligh...
    • 5 Jun 2012
  • led 30w

    e14 Contributor
    e14 Contributor
    TV backlight growth has slowed down, and cost issues, as well as a huge consumer awareness of the lighting market is still completely open, the led 1w   industry is facing the most difficult time. CHINA SSL as the global semiconductor light...
    • 5 Jun 2012
  • LED Spotlight 30W

    e14 Contributor
    e14 Contributor
    LED lighting market opportunity is huge, broad space for development. LED lighting applications has been developed from past outdoor landscape lighting LED interior lighting applications. According to the analysis of the next five years, led driver 1...
    • 4 Jun 2012
  • High Power LED 50W

    e14 Contributor
    e14 Contributor
    With the herd phenomenon of the market, as consumers, use LED remains to be calm, scientific analysis, the choice of the best cost-effective light sources and lamps, here are several basic performance of the LED:1, the brightness of the led 1w &...
    • 4 Jun 2012
  • Raspberry Pi - enabling SSH by default to make life easier.

    GreenYamo
    GreenYamo
    Well, slightly longer time than I hoped for a second post, but here it is at last. If you are a mainly windows user, you may not have come across telnet or ssh (more here) however in the Linux and Unix world they are very useful, and will make m...
    • 2 Jun 2012
  • led driver 80w

    e14 Contributor
    e14 Contributor
    The development of high-power LED lighting solutions manufacturer currently experiencing the biggest design challenge is the thermal design and thermal overload protection, they must overcome 's LED light source is sensitive to heat problems, and wil...
    • 2 Jun 2012
  • led driver 150w

    e14 Contributor
    e14 Contributor
    LED driver selection discussion  LED driver IC characteristics and selectionUser question: led driver 120w  must use a dedicated LED driver IC? What are the advantages and disadvantages compared with ordinary IC?Re: the advantages of ...
    • 2 Jun 2012
  • led power 250w

    e14 Contributor
    e14 Contributor
    led power 50w   is very common, especially in some high-end portable light flashlight used widely. This type of flashlight commonly used single-cell alkaline batteries or nickel-metal hydride rechargeable battery-powered, so the volume is v...
    • 2 Jun 2012
<>