Personal Blogs
  • Community Hub
  • More
Personal Blogs
Douglas Wong's Blog CHIP Computer - they are shipping
  • Blog
  • Documents
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: dougw
  • Date Created: 14 Feb 2016 10:10 AM Date Created
  • Views 1369 views
  • Likes 4 likes
  • Comments 11 comments
Related
Recommended

CHIP Computer - they are shipping

dougw
dougw
14 Feb 2016

This is a quick unboxing and power up of a $9 CHIP computer in case anyone had doubts about the Kickstarter promises....

For some reason I cannot insert a video in a blog since the site upgrade, so you will have to follow this link:

CHIP Computer is Shipping

  • Sign in to reply

Top Comments

  • clem57
    clem57 over 10 years ago +1
    dougw Thank you for unboxing video. Other than play, do you have project(s) in mind? Can you provide link for vga display? Thanks in advance, Clem
  • clem57
    clem57 over 10 years ago +1
    dougw I was considering the CHIP computer until I realized: They are only providing VGA support at $9. The upcharge for HDMI was about $15. They charged $5 for each computer ordered. Really? The ram is…
  • dougw
    dougw over 10 years ago in reply to clem57 +1
    The Pine looks like a great little computer and there are other interesting modules out there as well. I was looking for the absolute lowest cost way to get a full color VGA display, including LCD. I was…
  • dougw
    dougw over 10 years ago in reply to e14 Contributor

    June - wow, they must have a lot of orders - the whole point of the Kickstarter was to get into high volume low-cost production. The campaign had 39,000 backers last time I checked (over $2M). If most of them are getting 2 units, the volume is definitely starting to get up there and it should rapidly become a pretty healthy user community. They did ship mine on the schedule they predicted and they came with an extra clear case already installed - which was a pleasant surprise.

    It took Beaglebone Black about 7 months to sell 100,000.

    It took Raspberry Pi about 12 months to sell 1 million.

    This module has more features (WiFi & Bluetooth) and it is much easier to get running and it costs much less.

    Of course Pi Zero is even cheaper and also sells so fast they can't produce enough to meet demand.

    It is great to see the trend...

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • e14 Contributor
    e14 Contributor over 10 years ago in reply to dougw

    Thanks... Ordered one of everything... they say the computer won't ship until June...

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • dougw
    dougw over 10 years ago in reply to e14 Contributor

    1pcs DC DC Adjustable Stepup Boost Power Converter Module XL6009 Replace LM2577 | eBay

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • e14 Contributor
    e14 Contributor over 10 years ago

    Do you have source for dc to dc converter?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • dougw
    dougw over 10 years ago in reply to clem57

    This little computer has a lot of built-in features and computing power in a tiny form factor, including WiFi and Bluetooth. This makes it a great platform for high performance mobile or wearable devices or small embedded applications, and the hardware is open source. One of the reasons I bought the small display is in anticipation of mobile applications. I don't have specific projects in the works yet - still getting familiar with features and programming environment.

    I got the display on ebay - it is a 5" 800x480 rear-view display for vehicles. There are many to choose from in the $17 range, just make sure to check the resolution. I use a $2 DC-DC module to boost USB voltage to 12 volts for the display.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
<>