Personal Blogs
  • Community Hub
  • More
Personal Blogs
Frank Milburn's Blog PCB for a Kelvin (4-Wire) Milliohm Meter
  • Blog
  • Documents
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: fmilburn
  • Date Created: 18 Oct 2018 5:49 AM Date Created
  • Views 12128 views
  • Likes 13 likes
  • Comments 112 comments
  • kelvin measurement
  • current source
  • 4 wire measurement
  • milliohm measurement
  • op amps
Related
Recommended

PCB for a Kelvin (4-Wire) Milliohm Meter

fmilburn
fmilburn
18 Oct 2018

EDIT 24 Oct 2018  The schematic in this post contains an error.  It will be reposted after receipt of the PCB and testing.

 

I am developing an inexpensive but reasonably accurate meter for measuring resistance in the milliohm range.  The previous posts are listed in the related links at the bottom.  In this post the design for the working prototype is expanded to include a second current source for measuring resistance up to 400 ohm and provision made for future auto-ranging.  A new schematic and a PCB design are presented along with an update on meter options.

 

Revised Schematic

The revised schematic is shown below:

image

The added current source is identical to the first but designed for 1 mA current.  A dual N-Channel MOSFET with pull-down resistors is connected just above ground to allow selection of a source.  It will add maybe an ohm to ground.  There are jumpers and bypass resistors so that the second current source and MOSFETs can be omitted if desired.  This has not been incorporated into the working prototype so a second eye and comments on the design are welcome.  An additional 5V set of pins was added so a source other than the USB connection could be used as well.  Thanks for ideas and suggestions shabaz  image.

PCB Design

The PCB was done in KiCad (5.0.0) which is a new version for me and I am still finding my way around the changes.  The layout was done with ease of hand soldering in mind which led to what I consider poor routing so I may redo it and hope send it to the board house tomorrow.  There were a couple of unfinished wires when the renders below were made but those are finished now and it passes electrical check.

image

image

 

Panel Meters and Alternate Current Sources

The panel meter I ordered from China came in earlier in the week but they were a disappointment.  Although they advertised 5 digit resolution they are not much better than 3 and show zero when down in the low millivolt range so they aren't much use for this project.  There is a zeroing procedure which I tried without much luck and a small pot which doesn't seem to do much.  I also ordered a ammeter but haven't had a chance to really test it.  It looks like I will be using patch cables and a multimeter for the display.

image

 

I also finally got the other current sources I was going to test for the project but time is running out and the LM334 really works good so I will put those aside for a later time.

 

Next Steps

This week I also plan to finish preparation of the BOM and order the parts that aren't in hand but there probably won't be any more posts until after the PCBs are back in about 2 weeks time.  As always, comments and corrections are appreciated.

 

Related Links

Testing Current Sources for a Kelvin (4-Wire) Milliohm Meter

More on Current Sources and a Kelvin (4-Wire) Milliohm Meter

Even More on Current Sources and a Kelvin (4-Wire) Milliohm Meter

Working Prototype of a Kelvin (4-Wire) Milliohm Meter

  • Sign in to reply

Top Comments

  • fmilburn
    fmilburn over 7 years ago +7
    Hi Shabaz, From you description, it looks like I ordered the wrong meter... Could also have a particularly bad sample. I spent a fair amount of time trying to calibrate it again this evening without luck…
  • shabaz
    shabaz over 7 years ago in reply to fmilburn +7
    Hi Frank, Some good news, and some uncertainty : ) The good news is that it is assembled, it was a breeze using the PCB. Also it is just the right size for the enclosure, it all fits hopefully : ) I've…
  • shabaz
    shabaz over 7 years ago +6
    Hi Frank, Sorry to hear the panel meters were no good : ( I'll check the ones I have, in case any function better. (By the way from the back of it, if there is a 5 or 6-pin SOT-23, that should have been…
Parents
  • andbro
    andbro over 6 years ago

    Hi,

     

    Does this project is aborted?

    Where we can find the latest schematic and Gerber files?

     

    Thank

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • shabaz
    shabaz over 6 years ago in reply to andbro

    Hi Andre,

     

    The project works well, with typical error of around 1 mohm.

    I like using it because it has low current (10 mA max, so it doesn't heat up much the resistance-under-test) unlike some other projects which use 100 mA).

    Making it is straightforward, they are all low-cost parts (no high-accuracy parts are needed, although low ppm resistors are preferred), and a single trimmer is adjusted after completion, by using the project to measure a known resistance (two trimmers are used for two ranges).

    The values I used for the early revision PCB are in the blog post Frank referred to, but there is a newer revision ( fmilburn I'd misplaced it, but I've finally found it and can assemble it).

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • fmilburn
    fmilburn over 6 years ago in reply to shabaz

    This project is a great example of one that grew without much planning and was left without the best of documentation :-).  I can’t access things right now but will try and find the latest gerbers within the next week or so when I am able.  The performance of the new version is similar to the first version but has accommodation for further tweaking and testing.  It has been on my backlog to revisit the project but not something I can get back to right away. 

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • fmilburn
    fmilburn over 6 years ago in reply to shabaz

    This project is a great example of one that grew without much planning and was left without the best of documentation :-).  I can’t access things right now but will try and find the latest gerbers within the next week or so when I am able.  The performance of the new version is similar to the first version but has accommodation for further tweaking and testing.  It has been on my backlog to revisit the project but not something I can get back to right away. 

    • Cancel
    • Vote Up +3 Vote Down