Personal Blogs
  • Community Hub
  • More
Personal Blogs
Hardware De Soldering
  • Blog
  • Documents
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: mcb1
  • Date Created: 22 Jan 2017 5:37 AM Date Created
  • Views 5755 views
  • Likes 11 likes
  • Comments 35 comments
  • solder_braid
  • duratool
  • top_members
  • smd
  • solder-iron
  • denon
  • de-soldering
  • rework_stations
  • solder_wick
  • solder_pump
  • smd soldering
Related
Recommended

De Soldering

mcb1
mcb1
22 Jan 2017

Some time in 2015 there was a discussion about Soldering and De-Soldering, and what some members owned or used.

 

At work we have PACE desoldering stations, but they are rather large, and the consumables are relatively expensive.

Personally I find them less than ideal, however that could be because it isn't my own and consequently there are some areas that need attention.

 

 

I decided this was an ideal topic to discuss some tricks I've picked up over the years.

 

 

Back in time

Further back in time (no ... not the beginning of time! ) I had an earlier version of a Denon desoldering gun similar to this.

image

   photo from Denon site.

 

They are a brilliant device.

They are easy to use, have good suction, fit into your toolbag, and the motor is in the handle so there is some vibration transferred to the joint you are trying to desolder.

 

We had issues with the tips (which weren't cheap) and it may have been linked to our techniques, rather than the tips themselves.

The other issue we experienced, was the control board and a tendency to burn out a resistor.

 

Sadly mine killed the resistor and I have no longer have any good boards to compare the value to.

Pricing a replacement board from the company some years ago, brought more than tears to my eyes, and I haven't found a schematic.

 

Eventually that model got replaced with the 7000 which seems to use the same tips, filters and camber.

The price has climbed to something that makes it unreasonable for me to justify.

 

 

So my desoldering had to wait until I was at work, or use other techniques.

 

 

PACE

I have nothing against PACE as a company, but I do have troubles with the de-soldering stations we have at work.

We have earlier versions and the newer models.

While the control side has changed, the basic principle and 'hot' end hasn't really changed much.

 

The large part contains the power supply, temperature control and vacuum (or blow) pump, and this model has a controllable soldering iron.

 

image

   photo stolen from Farnell

The handpiece contains the switch along with the heated end and a collection tube to hold the recovered solder.

 

image

 

     photo from JENSEN Tools + Supply | Products and Services for Electronics Manufacture, Assembly, Diagnosis, and Repair

 

The tube (3) holds a bent piece of aluminium (4) to collect the solder and a filter (5) at the end to trap solder particles and most of the flux.

A secondary filter was fitted at the end of the vacuum tube to ensure no particles went through the pump. (17)

 

 

Earlier containers were glass, with a rubber end that fitted around the end of the tip.

The clear tube allowed the amount of solder collected to be viewed, and the rubber end made a good seal to ensure all the vacuum went via the tip.

 

 

For some reason the glass tube got replaced by a cardboard tube.

image

They are cheaper, but you only ever broke the tube by rough handling or WAY too much solder causing localised overheating.

However there is this Health and Safety in the workplace and it could be this that has resulted in our work using these instead.

 

They are more difficult to clean out since you can't stick something in the other end to push out the bent aluminium 'catcher'.

Perhaps they aren't designed to be cleaned out.

 

What this picture is not showing is the end is rounded and pushed back on itself to form a rounded end that goes around the end of the tip.

The glass tube seemed to seal better around the end of the tip.

 

In both models the handpiece is 'in line' so you hold it like a very large pencil.

 

 

As I said, the PACE units aren't mine, so it's very likely that there are some tweaks to make, or the end seal needs to be changed.

 

 

Whatever the reasons, I've never had much luck de-soldering stuff at work using these.

The results have been frustrating, plus it seems to take a lot longer due to the double and triple de-soldering plus mechanical manipulation (see later).

 

 

Other techniques

You can use a hand held De-Soldering Pump to suck the solder out.

imageimage

   photo stolen from Farnell

These work well on one or two joints, but can be a pain to use.

 

To use them, you press down the plunger to compress the spring.

Heat up the joint and bring the nozzle as close as you can, then press the release button.

As the plunger is released it sucks the hot solder up inside the pump.

 

Obviously the closer the nozzle is to the joint, the more effective it is.

 

 

One little trick with any de-solder pump/plunger is that you can stretch the spring.

Make sure the O-Ring is clean and lubricated and check the nozzle is not damaged, and it should perform well.

 

 

The best model I have is a Phillips branded version that is slightly smaller than others, and utilises a smaller nozzle.

This means you're not fighting the soldering iron for the same space, and the suction velocity is higher.

 

I should have brought three or four at the time, because they aren't available that I can find, so I'm looking after mine.

 

 

Something to watch for is models where the nozzle is inserted from the outside.

When you push the plunger down fully, it protrudes through the nozzle to clean out any solder lodged on the sides.

With the external insertion type nozzle, they can be pushed out.

Models with softish nozzles can deform rather than clean out properly ...

 

I prefer the screw together models. I've seen the other 'twist lock' style versions fly around the room at the most inopportune moment.

 

 

It's rather hard to see all these things from a catalogue, so don't be afraid to ask, or buy different types until you find the one you want.

If you have smaller hands the length can also be very important as they are meant to be used with one hand.

(I'm happy to do some road tests on different types ...but send spare nozzles as well)

 

 

 

 

 

De-Solder Braid/Wick

I've heard people swear by this, and I've heard people swear.

It works for surface mount, but isn't very useful on thru hole components.

image

   photo stolen from Farnell

It is very useful for cleaning up holes .... but then so is the solder pump.

Don't be fooled, they come in different widths, and the cheap stuff may not work as well.

 

This soldering guide is rather good, and they use the braid/wick to clean up the joint.

https://www.sparkfun.com/tutorials/96

 

The thru hole soldering guide is here

https://learn.sparkfun.com/tutorials/how-to-solder---through-hole-soldering

 

 

The whole SMD guide is here, and it includes reflowing using the frypan/skillet along with a toaster oven.

https://www.sparkfun.com/tutorials/category/2

 

 

 

What else

The last thing you want to do is damage the board.

It may be worth sacrificing the $1 component by cutting off the legs and then removing each leg seperately.

This works well for ICs, and is a must for header pins or other sockets.

image

   photo https://www.sparkfun.com/tutorials/97

 

Personally I'd use sidecutters to nip each leg, rather than risk cutting the board.

 

 

For headers or sockets you need to be careful not to damage the platethru part of the hole.

Generally the hole is snug, so it's important to seperate the pins.

image

   photo https://www.sparkfun.com/tutorials/339
Step 1, cut the pins

Step 2, heat and remove each pin.

 

 

 

You can use a Rework Station to heat larger areas and then remove the component.

There are low temperature solders that can aid that technique.

image

photo https://www.sparkfun.com/tutorials/98 

 

 

 

Stubborn joints

Removing what solder you can, and then resoldering the joint can help.

I guess it breaks up the surface oxidation and allows all the solder to flow when you come back to desolder it.

 

Sometimes a little sideways pressure can break the small bridge of solder that is resisting the component from exiting the board.

 

I've also fitted the board into a holder and applied heat to one side, and a solder pump to the other side.

 

 

Whatever you do, avoid excess heat to small pads, or you'll lift them from the substrate, and then have problems putting the replacement component back in.

 

 

 

2015

I was lucky enough to go to England in August of 2015 and meet some of the other members of element14, along with a visit to the Leeds distrbution centre.

Just prior to this a few of us were having a conversation about desoldering stations and when I mentioned the issues I had, Problemchild kindly offered to obtain one of these for me.

DURATOOL D00672

I can only find them on the cpc site http://cpc.farnell.com/duratool/d00672/desoldering-station-uk-eu-plug/dp/SD01384

 

Along with the station we decided a spare handpiece, tips and filters would be useful.

 

Luckily I didn't have any desoldering jobs to do, so it sat under the workbench waiting for that special day.

 

When I powered it up to use it, I had some issues with a distinct lack of suction.

As it was new I had no reference point, so a process of elimination began.

 

The suction pump worked, and there was suction at the collection tube.

The tip was clean and free with no restrictions.

The collection tube has a filter inside, plus an end plate that floats, and I thought it might be blocking the end.

 

As you applied suction and blocked the flow, the pump note changed to a deeper 'growl' but when it was assembled it sounded like it had flow.

Unlike the PACE models, the output of the pump ends inside the unit, so you don't get a 'blow' port to check.

 

By now you will be assuming that I opened up the manual ...... but that would be cheating !.

BTW I have since checked the instruction manual, and it inlcudes a diagram that doesn't match the collection tube, but no other useful information that would help.

 

Collection tube

The tube on this is similar to the Denon and PACE. It fits between the tip and the suction line.

image

 

except this one contains loose bits....the photo below shows what I mean.

 

image

 

When I first opened the handpiece to see the collection tube, the various bits came out.

 

The aluminium disc is supposed to catch the solder, and the holes around the outside allow the air to flow.

The issue is nothing is tight in the tube, so as you return the collection tube to the handpiece any suction wants to take the path of least resistance.

image

 

At the front there are two rubber like seals. The larger one fits the tube, but the smaller one was just floating.

image

 

In the end I fitted the smaller seal over the end of the protruding tip.

I figured it was either going to smell bad as the material cooked, or it would seal around the tip.

 

My later assumption was correct and it sealed the 'leak'.

 

So this unit now sucks very well, and easily cleaned up the solder joints.

 

My next minor issue is that I'm not happy with the loose nature of all the internals.

The spring tries to push the disc and filter out the suction end whenever you open it.

 

I'm thinking that a bent piece to collect the solder on and a larger disc that holds the filter and increases the exposed filtering area would help.

 

In the meantime I am a happy camper, but I do need to find a spare end seal along with the tube and tube seal just to make sure the whole unit outlasts me.

 

 

Cheers

Mark

  • Sign in to reply

Top Comments

  • Problemchild
    Problemchild over 6 years ago in reply to jw0752 +3
    Hi John , long time no see ;-) For Reference you can get the Duratool one for £70-80 all day at CPC and like £49 on a sale which they do often ... In fact I bought the one fro Mark when he came over way…
  • COMPACT
    COMPACT over 9 years ago in reply to jw0752 +2
    Mine works perfectly well without any mods. The dross pops out without any dramas. One hint with desoldering technique - keep the trigger depressed and the tool sucking after removing the tip from PCB…
  • Problemchild
    Problemchild over 6 years ago in reply to dubbie +2
    Hi there dubbie I have braid which I use to clean up excess solder on SMD parts or after doing a bit of drag soldering , I use a manual solder sucker for occasional joins if I cant find the vacuum desolder…
Parents
  • jw0752
    jw0752 over 9 years ago

    Hi Mark,

    I have a desoldering station that is the same as the one you describe in the last part of your blog. Here are a couple tips I have discovered to make it work better.

     

    I put a light coating of talcum powder on the black front seal so that the chamber doesn't stick to it and pull it out when I remove the solder collection chamber.

     

    I have had the stainless central tube become clogged when solder is drawn in early in the operation. The stainless wires that are provided to clean out the solder do not work well as they do not conduct heat to the clog. I have taken a piece of 14 gauge copper wire and used that to clear the tube. The heat travels down the copper wire and melts the clog making the clearing process quick and easy.

     

    I made quite a few modifications to my unit and I am very pleased with how well it works now.

     

    John

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • mcb1
    mcb1 over 9 years ago in reply to jw0752

    jw0752

    Thanks for those tips.

    The front seal has got stuck, so I might add that to the blog later ...thanks

     

    Haven't had a clog (yet) but I learnt early to keep sucking for a short period after you lift and that might be also worth adding.

     

    Mark

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • jw0752
    jw0752 over 9 years ago in reply to mcb1

    The continuation of sucking is a good technique. The clog however usually occurs when I start too soon and the tip is ready by the heat hasn't traveled fully down the tube to the chamber. As such the solder hits the cooler tube and solidifies. The other technique to clear this is to over heat the gun and pound away with the cleaning tools. This use to be a challenge but since I started using the copper wire for the problem it is easy and doesn't require running the heat so high.

     

    John

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • COMPACT
    COMPACT over 9 years ago in reply to jw0752

    I'm puzzled at that statement because the heating element is in the barrel and the soldering tip is at its coldest extremity.

    As most know I'm very successful at using low temperatures and I use 280 deg C for 60/40 Pb/Sn.

    You have to remember that if the PCB pad you're desoldering is connected to a power or ground plane it could take a while for it to reach the correct heat.

     

    Have you tried operating it upside down for Gravity assist to see if it operates better?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • jw0752
    jw0752 over 9 years ago in reply to COMPACT

    Hi Compact,

     

    We may have different units as mine has the heater in the barrel with the heat concentrated near the tip where it will do the most good. There is an intentional and expected heat gradient in the suction tube so that the small black rubber seal that Mark was talking about doesn't melt. The inner tube in mine is built of stainless steel which doesn't conduct heat very well. I am certain that if I had your expertise I would not ever get a clog but since I have experienced them from time to time I developed a quick fix ( Piece of Copper Wire). It is unlikely you will ever have any problem like this but just in case you are welcome to give my technique a try.

     

    John

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • jw0752
    jw0752 over 9 years ago in reply to COMPACT

    Hi Compact,

     

    We may have different units as mine has the heater in the barrel with the heat concentrated near the tip where it will do the most good. There is an intentional and expected heat gradient in the suction tube so that the small black rubber seal that Mark was talking about doesn't melt. The inner tube in mine is built of stainless steel which doesn't conduct heat very well. I am certain that if I had your expertise I would not ever get a clog but since I have experienced them from time to time I developed a quick fix ( Piece of Copper Wire). It is unlikely you will ever have any problem like this but just in case you are welcome to give my technique a try.

     

    John

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
Children
  • mcb1
    mcb1 over 9 years ago in reply to jw0752

    jw0752  COMPACT

     

    This is an interesting discussion that we should include into the original blog.

    It would seem that technique may have more to do with the problem than the design issues.

     

     

    I'm mindful that the tip opening size is usually much smaller than the tube size, so I wouldn't expect it to stick to the sides, but then John has 'supercharged' his and it may be causing the rear of the tube to cool more than our ones do.

     

    I know we had blockages in the Denon version and that had a very long tip assembly.

     

     

    Mark

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • COMPACT
    COMPACT over 9 years ago in reply to mcb1

    I think we're comparing apples with apples.

     

    Here's a picture of my desoldering gun accompanied with a solder stalagmite from its filter.

    The momentum of the solder makes it collide into the centre of the metal filter cover forming an elongated stalagmite over time.

    The suction comes from the four open edges of this filter cover.

    image

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • jw0752
    jw0752 over 9 years ago in reply to COMPACT

    Hi Compact,

    Actually I agree, we are comparing Apples to Apples. For an experiment I set up a replacement element for this gun and put 15 watts of power on it and let it stabilize. I then used a Fluke IR temp sensor to read the temperatures on different positions of the element. As you can see the bulk of the heat is concentrated at the interface to the tip. The temperature gradient is near 200 degrees F from the tip to the exit into the solder capture chamber. Incidentally the temperatures are all displayed in Fahrenheit. If you want to convert to C the formula is C = (F-32)/1.8.  Keep in mind I am applying 5 volts at about 3 Amps to the element and the temperatures generated are for illustration only and may not match normal operational temps. A further observation on why I may be having occasional blockages and you may not is that I have had my unit for over a year and I frequently salvage older circuit boards. I believe there has been some pitting of the inside of the stainless tube by salts or other chemicals in the different fluxes that have been pulled through. This pitting combined with the lower temperatures down tube cause a constriction that eventually clogs. Your use and application of your unit hopefully may not ever have this problem. Below are the picture that I took of the temperature gradient down the side of the heater.

     

    image

     

    image

     

    image

     

    image

     

    John

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • Problemchild
    Problemchild over 6 years ago in reply to jw0752

    John do /did you use the pin that comes with the unit to clean it out ?

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • jw0752
    jw0752 over 6 years ago in reply to Problemchild

    Hi John,

     

    The cleaning rods that come with the unit are stainless steel and as such they do not conduct heat well. I am sure they were chosen so that the solder in the pipe would not wet them and stick but as it turns out this is a disadvantage. I like to use pieces of solid copper wire, 16 or 18 GA (I think) as this conducts the heat well and melts any clog of solder that might exist as I push them through. In my experience the clog usually happens at the end of the suction tube closest to the catch reservoir. It also usually happens at the start of a desoldering session before the gun has had time to really heat up the exit end of the suction tube. I used to use the supplied rods to try to pound out the clog but since I have been using the copper rods the clogs are very easy to eliminate.

     

    John