Personal Blogs
  • Community Hub
  • More
Personal Blogs
John Wiltrout's Blog 0 to 150 Volt AC Bench Power Supply Build
  • Blog
  • Documents
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: jw0752
  • Date Created: 14 Apr 2019 4:29 AM Date Created
  • Views 8288 views
  • Likes 14 likes
  • Comments 15 comments
  • variac
  • ac bench power supply
Related
Recommended

0 to 150 Volt AC Bench Power Supply Build

jw0752
jw0752
14 Apr 2019

A week or so ago I wrote a short blog about a variable AC isolated bench power supply that I wanted to build. See the following Blog:

 

An Extreme Ripple Power Supply Build

 

The idea was just a seed and a pile of assorted resources. Just as I hoped, four of my friends here on element 14 stepped up and gave me some great advice and collaboration on the build. I want to specially thank: genebren , Gough Lui , three-phase , and jc2048 without whose suggestions and ideas I could not have completed the project as successfully.

 

The purpose of this build was to produce a bench AC power supply with 160 volts output at 2 or 3 amps. It seems that weekly, one project or another needs an AC source of one voltage or another. My present AC power supply is about 50 years old and it is time for an update.

 

I began with a rough draft of a schematic which I published in the previous blog. There were mistakes and improvements to be made as pointed out by my collaborators. Here is the schematic of the final build of the power supply:

 

image

Some of the great ideas that were suggested to me were to add an MOV to the input to protect against spikes, add fuses in the secondary and output of the unit, provide a voltage fail safe so that the unit could not be powered on while set to a lethal voltage level, and a high voltage alert light. The final build has all of these features.

 

As usual I began this project with a slow trip through my parts graveyard looking for resources. I almost never produce a design and then look for the parts. It is always find the parts and then design an interface between them. The central parts central to the build were a transformer, where 115 VAC on the primary would give me an isolated 130 VAC on the secondary, a small variac, and a salvaged case from a piece of 1960s vintage dental equipment.

 

  
imageimage

Here are the transformer and the variac in the early proof of concept experiments. It is important to bread board or jumper wire experiments of the build before proceeding so that one will eventually get the desired results.

 

imageimage

The case was hopefully going to be big enough to house everything. It was a heavy steel case with an old fashioned chassis inside. The chassis would have to be substantially modified before it would properly hold the components. I began by spray painting the case a nice off white color. The front panel was a piece of black opaque plexiglass. I have used this type of front panel on many of my builds as it is easy to work with and when labeled with white on clear label tape it looks good enough for me.

 

image

Here is the painted case and to the left is the chassis where I have mounted the isolation transformer and the variac. For the variac I had to cut the floor of the chassis and fold it up to make an extension of the front metal. This made room for the body of the variac as well as providing extra support for the front plate. As the project continued this was the first of several cuts and bends that needed to be done to the chassis. In the front left you can see the preliminary layout of the front panel. At this time the front panel meters had not come and so I had estimated their dimensions. Time would prove that I had greatly underestimated their size and many of the challenges to finishing this project revolved around how to integrate them into the case. Eventually I had to cut more of the front of the chassis out and extend the square hole that you can see in this picture to the left, almost all the way to the variac plate.

 

Once I had the primary components on the chassis I began to populate the unit with minor components and finally I began the initial wiring.

 

  imageimage

In this picture you can see the fuses for the primary, secondary and output circuits that were recommended by my element 14 collaborators as well as an AC relay that will be used in the circuit that will prevent the unit from being turned on if the variac is not in the low voltage position. In the lower right corner of the picture you can see the microswitch , better picture to the right, that senses the zero volt position of the variac. When the wiper of the variac comes to the full off position a small epoxy ramp on top of it actuates the microswitch. If this switch or the override switch is not closed the relay will not actuate and latch. When I installed the microswitch it was necessary to cut slots for the mounting screws so that the position relative to the variac wiper could be adjusted.

 

image

To get the 12 volts DC that would power the voltmeter and ammeter circuits a small power supply board was built. This board was powered by a separate transformer. You can see it on the chassis at the back in later pictures. Since there was adequate room on the board the components for the high voltage sense circuit were also added. This power supply also drives the power on indicator LED.

 

image

The small circuit board was mounted on standoffs near the front panel so that it would be close to the meters and indicator LEDs.

 

The meters for the unit finally arrived and with them the surprise that they were much bigger than I had assumed.

 

image

Here is a picture of the ammeter. The larger size forced me to return to the plan for the front panel and begin searching for every millimeter of space. The front panel on which they were to be mounted had conflicts with the chassis and there was the ultimate need for everything to fit inside the bezel of the outer case. It was very close and don't tell anyone but in the end the fit inside the bezel of the outer case is not perfect. Fortunately the black plastic panel hides the slight gap very well.

 

Another challenge that I left for the arrival of the meters was the fact that the ammeter was designed to measure up to 100 amps and the most I anticipated measuring was 3 amps. This would mean that I would not be making good use of the range of the ammeter and that my current measurement accuracy would suffer. The ammeter came with a huge current transformer.

 

image

Here you can see the current transformer mounted to the chassis. Fortunately once I got away from the crowded front panel there was lots of room in the body of the unit. I decided that I would put two windings on the current transformer and install a SPDT toggle next to the ammeter so that I could choose between the single 0 to 100 amp display on the meter to a more detailed 0 to 10 amp display. As you can see on the right side of the current transformer I have wound the current carrying conductor 10 times to produce the compressed range. On the left side of the transformer we have the single pass through of the 0 to 100 range. I experimented briefly with moving the decimal point on the meter but total lack of technical information made this a difficult and risky modification. In the end I decided to make use of a unit of current that is seldom encountered. "The Deciamp". Yes, when the toggle is switched to the 0 to 10 amp range the meter displays the current in deciamps. While not totally desirable it adds some character to the unit and it is worth the extra accuracy that is displayed by the meter. These meters were quite inexpensive, less than $15 each and while they work well for this application they take their time reading and displaying the voltage and current. I think they refresh twice a second and the 1 to 100 amp range will sometimes take 3 to 4 seconds to settle on the correct display. In the short video at the end of this blog you will see when I switch from 4.6 deciamps to amps the display reads 2 then 3 and while I don't wait for it to get there it will eventually display 4.

 

   imageimage

Here is the front control panel prior to labeling. The second picture shows the tightness behind the control panel and the way it was necessary to cut into the chassis so that the back of the meters had room.

 

image

Here is the underside of the chassis behind the front control panel.

 

When I finished the build at 2 AM last night I did not dare turn it on and test it. I have made this mistake in the past and if anything doesn't work correctly I would find myself pulling an all nighter trying to find my mistakes and debug the unit. It is much better to assume the best and go to bed and test it in the morning. Fortunately the morning light brought smiles as the unit worked as planned. The front panel was labeled as well as the back fuse plate of the unit. I enlisted the help of the boss to make a short demo video which is posted below.

 

You don't have permission to edit metadata of this video.
Edit media
x
image
Upload Preview
image

 

Finally thank you to element 14 for providing this site where I can get help from friends in England, USA, and Australia on my projects.

 

John

  • Sign in to reply

Top Comments

  • fmilburn
    fmilburn over 7 years ago +7
    Hi John, Great build as usual. I would not even think of trying to build something like this - it reminds me of why I choose to stick with low voltage and for the most part digital. It is best to leave…
  • genebren
    genebren over 7 years ago +6
    John, That is another high quality build that you have done. Everything looks great and works very well. A very handy piece of equipment! Well done! Gene
  • shabaz
    shabaz over 7 years ago +6
    Hi John, This looks like an excellent piece of equipment! Very clever trick with the relay too, it's a really neat safety idea. This project looks awesome all-round, and very flexible, that's a great adjustable…
  • clem57
    clem57 over 7 years ago

    Maybe old, but I bet really useful as well made too.

    Thanks jwvdst

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • three-phase
    three-phase over 7 years ago in reply to jw0752

    No, I do not believe it would save you from having to adjust the ammeter itself. The input of the ammeter is 5A and has been calibrated to convert that 5A into a 100A reading. Thinking about this, if the CT ratio is changed from 100/5A to 10/5A, it will just mean that you will only need 10A primary current to read full scale, which will still be 100A. You have effectively achieved this by wrapping the 10 turns around the CT.

     

    Besides, looking at the price of these meters, they are less than a 10/5A CT.

     

    0 to 10A meter

     

    0 to 10A Current transformer

     

    Kind regards

    • Cancel
    • Vote Up +4 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • jw0752
    jw0752 over 7 years ago in reply to ralphjy

    Hi Ralph,

     

    Proof I followed up on your suggestion.

     

    image

     

    John

    • Cancel
    • Vote Up +4 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • Gough Lui
    Gough Lui over 7 years ago

    That's one massive CT. Glad you managed to fit everything into the box in the end. Definitely a nice looking, relatively bulletproof build. Congrats!

     

    - Gough

    • Cancel
    • Vote Up +5 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • jw0752
    jw0752 over 7 years ago in reply to three-phase

    Hi Ralph,

    The transformer has a 5A secondary. Does this mean I can substitute a 10A primary with a 5 amp secondary and not have to recalibrate the meter?

     

    When I build I always take pictures and save all the paperwork that I generate, combining it into a manual of sorts. Builds that are important to me get more documentation and perhaps a rudimentary operation guide.

     

    John

    • Cancel
    • Vote Up +5 Vote Down
    • Sign in to reply
    • More
    • Cancel
>