Personal Blogs
  • Community Hub
  • More
Personal Blogs
John Wiltrout's Blog Back Up Battery failure inspires new test tools.
  • Blog
  • Documents
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: jw0752
  • Date Created: 27 Nov 2018 5:07 AM Date Created
  • Views 1733 views
  • Likes 12 likes
  • Comments 13 comments
  • process duration timer
Related
Recommended

Back Up Battery failure inspires new test tools.

jw0752
jw0752
27 Nov 2018

The computer in my lab is very important to me. This of course is very subjective as its contents and utilities are understood and utilized only be me and so someday, when I can no longer use it, it will go directly from my lab to the computer recycle facility. In the meantime I do everything in my power to keep it clean, backed up, and with a protected UPS power supply. The original battery of the 650 Watt UPS is long since failed and when it did I bought a car battery and rewired things so that I can monitor the voltage of the battery and the discharge rate when it is being used.

 

image

Here is the battery in its case with the volt/ammeter mounted in the cover. Every couple months I pull the mains electrical plug and let the system run for an hour or so. Two nights ago I performed this routine test but within 10 minutes the UPS was beeping frantically for power and before I could get to the mains plug it died.

 

I took the battery case and opened it to find that while I was checking everything else I had not been monitoring the water level of the battery and 3 years of constant float charging had finally dropped the fluid level to about an inch of the bottom. This is not a good situation and there was not much else to do except to replace the battery. This time I got a battery with ADM maintenance free technology and an 8 year warranty. We will see how that goes.

 

I am not one to give up too easily and my thoughts went to the possibility of resurrecting the old battery. Just to show how bad the water situation had gotten the battery took almost 3 liters of distilled water before it was full again. I put the battery on a small charger and left it to charge.

 

The next problem that caught my attention was how I was going to test and measure the health of the car battery. When I have this problem with small batteries I hook them up to the Process Duration Timer

 

https://www.element14.com/community/videos/22548/l/first-test-of-process-duration-timer?sr=search&searchId=f826766b-bfaf-4e39-bdc2-afd26ffc3843&searchIndex=4

 

Short video of the Process Duration Timer (PDT) unit in operation. You can also search on this site for the original 4 blog series if you want to know more about the Process Duration Timer build.

 

The size of this battery however seemed likely to strain my present test abilities. One thought that seemed to make sense was that I would use a spare UPS Backup unit with a 75 Watt incandescent bulb and use that for the load.  The next problem would be how to interface the PDT to the system so that I could time the draining of the battery until the shut off voltage (which I didn't know) of the UPS was reached.

 

This was the inspiration that I needed to build an Interface for the PDT. As it sits the Process Duration Timer (PDT) was designed to monitor and time a voltage level and respond by stopping the clock when the monitored voltage level drops below a given threshold.

 

At its core the Interface is very simple with an LM393 comparitor, a MOSFET output and the required resistors and hardware needed to allow a sensor  to monitor a given process by watching other physical changes in the system and reporting back to the PDT with a High or Low voltage output which in turn is used to stop the timing of the process.

 

Here is a schematic for the Interface:

 

image

It was my plan to build the Interface and let its ability to monitor a light level watch the 75 Watt bulb on the output of the UPS that was being powered by the damaged battery. As long as the bulb was lit the interface would send 15 volts to the PDT and it would happily keep on timing the process of battery discharge. As soon as the battery level dropped below critical for the UPS operation however the bulb would go out and the interface would send a Low voltage signal to the PDT and the timer would stop and wait for me to return and read its output.

 

Before I get to the actual battery test however here are some picture of the Interface:

 

imageimage

 

imageimage

 

I am using a DPDT toggle switch on the unit to give me the flexibility to transition from High output to Low output on the Interface in either direction, Light to Dark, or Dark to Light. The LED tells the state of the output and the potentiometer allows the operator to adjust the sensitivity to fit local light conditions.

 

image

 

Here is a picture of the experiment set up. The battery has been charged for several hours and is showing all the signs that it is bad. The UPS is hooked to the battery and has a 75 Watt bulb plugged into one of its outlets. In a preparatory experiment I have measured the current demand on the battery to power the 75 Watt bulb. This turned out to be about 8.5 Amps. For some reason I don't understand right now the UPS's power demand is not stable but fluctuates +/- 1 amp while it is working. If anyone knows why please clue me in. The photo resistor sensor of the PDT Interface is pointed towards the 75 watt bulb. The Interface is set so that the output will transition from High output to Low output when the sensor no longer sees the light.

 

The PDT has been set to watch the Interface which should put out about 14.86 volts and continue timing the process until it sees less than 5.81 Volts.

 

image

The timer indicates that we are 1 minute 23 seconds into the test at this point.

 

image

We really did not have long to wait as 12 minutes and 30 seconds after the process started the battery gave up. If we do the math for 8.5 Amps over 12 minutes and 30 seconds we get about 1.7 Ah of power. For a battery that should have upwards of 45 Amp Hours this is a clear indication that the low fluid level has permanently damaged this battery beyond redemption.

 

Since I was still in the mood to upgrade the Interface I also made a Thermistor Sensor for it. The thermistor was chosen to work with the Interface in the range of 40 C to 130 C as I guessed that this might be a range that would be usable for me. Now I will be able to monitor and time processes that involve things that gradually heat up or cool down.

 

image

 

The sensitivity control was labeled with approximate transition temperatures for future use of the thermistor sensor.

 

Overall I am pleased with the added flexibility of the PDT that the Interface has provided. It is the silver lining of the cloud that was the failure of the backup battery.

 

John

 

 

  • Sign in to reply

Top Comments

  • Gough Lui
    Gough Lui over 7 years ago +7
    Flooded lead acid cells are fairly bulletproof, but indeed, every three or so months, topping up is highly recommended. Unfortunately, once the plates are exposed to air, I believe they oxidise and the…
  • Gough Lui
    Gough Lui over 7 years ago in reply to jw0752 +5
    That actually reminds me of a funny moment where I thought I could beat the system and ended up making a fool of myself. I thought having a UPS meant I was invincible (for at least 10 minutes with a beefy…
  • jw0752
    jw0752 over 7 years ago +4
    I should probably start a new blog for this but you are all probably getting sick of my Process Duration Timer so I will add it to this stream. After I finished with the interface I saw another simple…
Parents
  • three-phase
    three-phase over 7 years ago

    Nice project, I do like the process duration timer build, I shall go and find those blogs in due course and have a read through.

     

    Loss of water in a flooded cells causes sulfation of the plates, seen as a crystalline deposit across them. This reduces the active area of the plate and hence the capacity of the cell. If sulfation is not present, then you can have measured success with replacement of the acid and equalising charging, but it can be very difficult and time consuming and is often easier and more cost effective to get a new battery.

     

    The electrolyte also allows for even heat dissipation throughout the cell, without this the plates can overheat and deform / buckle altering the distance between adjacent plates and again affecting the performance of the cell. Once plates are deformed, then there is no chance of recovery.

     

    Sealed lead acid, is obviously 'maintenance free', however sealed cells are much more vulnerable to heat than flooded cells. So the 8 year nominal life specified for the battery will be for a certain temperature, usually 20 Deg C. For every 5 Deg C increase in temperature, the battery life will halve. Looking at the setup you have for the UPS, it looks quite enclosed, so you may want to verify the ambient temperature conditions for the battery.

     

    Impedance testing is a well practiced on sealed cells, the nominal impedance is given by the manufacturer and a doubling of that impedance is an indicator for a discharge test to verify the capacity.

     

    You can pretty much run whatever you like of a UPS, you just need to size it for the capacity you require, we run whole control rooms with all their associated computers and controlled systems from either centralised UPS or multiple UPS units feeding individual aspects - as usual, there is a solution if your budget allows. UPS autonomy can be increased by using parallel battery banks, up to what the charger can handle, remembering that it has to charge the battery and supply the load under mains operation.

     

    Kind regards.

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • three-phase
    three-phase over 7 years ago

    Nice project, I do like the process duration timer build, I shall go and find those blogs in due course and have a read through.

     

    Loss of water in a flooded cells causes sulfation of the plates, seen as a crystalline deposit across them. This reduces the active area of the plate and hence the capacity of the cell. If sulfation is not present, then you can have measured success with replacement of the acid and equalising charging, but it can be very difficult and time consuming and is often easier and more cost effective to get a new battery.

     

    The electrolyte also allows for even heat dissipation throughout the cell, without this the plates can overheat and deform / buckle altering the distance between adjacent plates and again affecting the performance of the cell. Once plates are deformed, then there is no chance of recovery.

     

    Sealed lead acid, is obviously 'maintenance free', however sealed cells are much more vulnerable to heat than flooded cells. So the 8 year nominal life specified for the battery will be for a certain temperature, usually 20 Deg C. For every 5 Deg C increase in temperature, the battery life will halve. Looking at the setup you have for the UPS, it looks quite enclosed, so you may want to verify the ambient temperature conditions for the battery.

     

    Impedance testing is a well practiced on sealed cells, the nominal impedance is given by the manufacturer and a doubling of that impedance is an indicator for a discharge test to verify the capacity.

     

    You can pretty much run whatever you like of a UPS, you just need to size it for the capacity you require, we run whole control rooms with all their associated computers and controlled systems from either centralised UPS or multiple UPS units feeding individual aspects - as usual, there is a solution if your budget allows. UPS autonomy can be increased by using parallel battery banks, up to what the charger can handle, remembering that it has to charge the battery and supply the load under mains operation.

     

    Kind regards.

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • More
    • Cancel
Children
  • jw0752
    jw0752 over 7 years ago in reply to three-phase

    Hi Donald,

     

    Thank You for the excellent supplemental information on why I couldn't revive the old battery. The UPS I am using is only 650 Watts and float charges the battery to 13.6 Volts. When the power is off the normal current draw from the battery is about 6 to 7 Amps. The case looks sealed but it is quite open to the environment as the cover has 3mm X 7mm openings at either end. I will take a base line temperature reading of the battery tonight compared to the room temp but I suspect with the very low current float charge of the UPS there is no real energy to have to dissipate. I wish I lived near you as I would love a tour of some of the large scale systems that you often describe.

     

    John