Personal Blogs
  • Community Hub
  • More
Personal Blogs
Nico teWinkel's Blog
  • Blog
  • Documents
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New

Nico teWinkel's Blog

  • Tags
  • Subscribe by email
  • More
  • Cancel
  • Video for Crazy Countdown Timer

    ntewinkel
    ntewinkel
    So, heh, I didn't see that little video icon that is at the top of every blog post editor until just now  So without any further ado, here is my project in action! players.brightcove.net/.../index.html
    • 30 Aug 2011
  • The Crazy Countdown Timer is complete!

    ntewinkel
    ntewinkel
    This morning, I put the finishing touches on my project: The Crazy Countdown Timer. This project emulates the cheesy "time bomb" that is often seen in movies. The hero finds the bomb, and then is faced with the decision of which wire to cut.The ...
    • 30 Aug 2011
  • Motion Detector

    ntewinkel
    ntewinkel
    Part of my crazy countdown timer is that I want to detect if someone is moving it, so I need to work with the accelerometer. So I created a new app and made it tic-toc between 2 spokes on the star LEDs. This is mainly to show that the app is sti...
    • 28 Aug 2011
  • Accurate timing

    ntewinkel
    ntewinkel
    I've incorporated the use of a timer to my countdown timer. This makes the clock much more accurate. I basically copied the millisecond_delay function and modified it a bit so that it would time for a second while updating the clock display. It ...
    • 27 Aug 2011
  • Countdown timer

    ntewinkel
    ntewinkel
    Now that the clock hardware is working, I can add a lot of functionality just by coding. It didn't take long to modify the code from my previous blog post to make it display a proper time value, and to make it into a countdown timer. At thi...
    • 24 Aug 2011
  • Clock display is running

    ntewinkel
    ntewinkel
    I gave up on the button issue for the time being, and started from scratch with a new project file to work on my clock display.  I created a new project pretty much using the exact steps as outlined in the document XL_STAR_Introduction.pdf ...
    • 24 Aug 2011
  • New application

    ntewinkel
    ntewinkel
    I created a new application from scratch today, using the demo as a guide. To save reinventing the wheel, I copied a lot of the LED functions from the demo. I also copied the buttons function, changing the global variables to just use one variab...
    • 23 Aug 2011
  • A bit of soldering

    ntewinkel
    ntewinkel
    I did a bit of soldering tonight to add headers to the XL_Star board, as well as to a couple of display options.This will allow me to hook the board up to the displays so I can then start programming them... and I'm hoping I can make them do some fun...
    • 16 Aug 2011
  • Time time time

    ntewinkel
    ntewinkel
    It's been a while since I last posted. The update is that there is no update!I've been spending my time getting a few other things done (mostly work stuff). I'm confident that today is the day to get 2 of those projects completed, with another projec...
    • 9 Aug 2011
  • Communication issue solved.

    ntewinkel
    ntewinkel
    As it turns out, the communication issue was a very simple one - there is an on/off switch near the top usb port that needed to be "off" and my board had it "on". It's possible I may have moved it when I took it from the package. Note to element...
    • 27 Jul 2011
  • No communication

    ntewinkel
    ntewinkel
    This is the story of the world, isn't it? Lack of communication being the root of all problems... To sum up what I've done so far... I installed all the software and drivers into a VirtualBox virtual machine running Windows XP, using the ea...
    • 27 Jul 2011
  • Package received

    ntewinkel
    ntewinkel
    Today I received the XL_STAR package at my door, from UPS. Unfortunately UPS charged me an extra $15 - an insane amount of money to get a free package across the border - but hey, small price to pay for geeky goodness! (ps, I highly recommend av...
    • 26 Jul 2011
  • The Plan

    ntewinkel
    ntewinkel
    Welcome to my blog! This is where I will be writing everything to do with my Summer of Design project for the XL_STAR development board from element14.com. My plan is to build a charge controller which maintains a battery using a solar pane...
    • 26 Jul 2011
<