Personal Blogs
  • Community Hub
  • More
Personal Blogs
Ralph Yamamoto's Blog Genmitsu CNC 3018-PRO - becoming useful
  • Blog
  • Documents
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: ralphjy
  • Date Created: 9 Aug 2019 5:46 AM Date Created
  • Views 10148 views
  • Likes 9 likes
  • Comments 24 comments
  • genmitsu cnc 3018-pro
  • cnc router
Related
Recommended

Genmitsu CNC 3018-PRO - becoming useful

ralphjy
ralphjy
9 Aug 2019

I had a minor victory on my road to figuring out how to use my new CNC router.

 

I received the 0.5mm carbide end mills that I bought on Amazon and used one to successfully shorten a proto PCB that I need for my LoRaXes project.  The mill has about 4 mm of cutting depth.  The PCBs that I'm cutting are nominally around 1.6 mm thick.  Not a very impressive looking cutter but it worked.  I increased the spindle speed to 3000 RPM and reduced the feedrate to 80 mm/min and set the cutting depth to 0.15 mm per pass.

 

image

 

Here is the shortened PCB next to one that is uncut:

image

 

The cut edges are very smooth but you can see that they are not quite straight.  Not sure if I can improve that with tweaking or if that's the inherent limitation of an inexpensive router and cheap end mills.  Only time and experience will tell.  Anyway, I'm pretty satisfied with the outcome.  The tool did what I needed it to do. 

  • Sign in to reply

Top Comments

  • Fred27
    Fred27 over 7 years ago +5
    Welcome to the world of CNC. It's fun, isn't it? You may know this already, but PCBs are particularly may to cut. They will blunt your endmills and the dusty is abrasive and nasty. For that particular…
  • Fred27
    Fred27 over 7 years ago +4
    I originally got a CNC mill (well, converted a mill myself) in order to mill PCBs. I ended up moving to etching as milling anything smaller than SOIC starts to get impractical. https://0xfred.wordpress…
  • balearicdynamics
    balearicdynamics over 7 years ago in reply to ralphjy +3
    The laser is controlled by PWM and there is a lot of relatively low power spindle and small diameter. The z-axis is not easy to be adapted (maybe with some 3D printed adjustment. The software I use is…
Parents
  • balearicdynamics
    balearicdynamics over 7 years ago

    Welcome on the CNC world image Do you plan to use it for PCB only or also something else? What kind of model? Some photos? If you need help, just ask.

     

    BTW... Maybe it is worth to open a group on CNC milling techniques, eventually finalized to the electronic design and prototyping support?

     

    Enrico

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • ralphjy
    ralphjy over 7 years ago in reply to balearicdynamics

    Hi Enrico,

     

    I did a blog post earlier when I first assembled this printer: Genmitsu CNC 3018-PRO

     

    I got the CNC mill to help with my electronic projects, so I'm hoping to also use it for things like small panels or face plates made out of plastic, acrylic, wood, or aluminum.  Hopefully will improve the quality and appearance of my builds.  There is also a low power (5.5W) laser module available that could be used for engraving (not sure if that is enough power to cleanly cut wood or acrylic).

     

    SainSmart is supposed to have a very active support community for their CNC products, but it's on Facebook and I really dislike Facebook.

     

    I'd support a group on Element14 if others would also like to start one.

     

    Ralph

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • balearicdynamics
    balearicdynamics over 7 years ago in reply to ralphjy

    Hello Ralph,

     

    thank you for the link I will read it in detail. I have a reasonable experience with a bit bigger CNC machine, the RS2030 and 2040 with which I have done many things and PCB too. As it weight 70 Kg and I have already fixed it in my lab in Spain together with a hand-made water cooling system for the spindle, a vacuum plane for some kind of milling and a vacuum plant to keep clean the working plate I had to leave it at home in Spain. Now here I have a couple of laser cutter and engraver including the z-axis I have assembled and modified with tome upgrades I plan to use one to make a PCB only mill machine. The Aluminium structure has a usable surface of about an A3 size and uses a three-axis controller based on Arduino. I think it is sufficient to replace the laser with a small shaft. What do you think of this idea?

     

    Enrico

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • ralphjy
    ralphjy over 7 years ago in reply to balearicdynamics

    Hi Enrico,

     

    I like the idea of repurposing equipment.  The Devil is always in the details though.  I think the hardest part will be mounting the spindle, so it probably depends on how the laser module is mounted.  And of course you'll need to get a power supply for the spindle, but it seems that a lot of spindles are sold with the power supply.  It sounds like you have a lot more experience with this type of equipment than I do.  Let me know how it goes if you decide to do it.  Oh, I guess you'll also have to add the speed control for the spindle motor since your controller probably doesn't have that. Might just be easier to replace the whole control board.

     

    Ralph

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • balearicdynamics
    balearicdynamics over 7 years ago in reply to ralphjy

    The laser is controlled by PWM and there is a lot of relatively low power spindle and small diameter. The z-axis is not easy to be adapted (maybe with some 3D printed adjustment. The software I use is the T2 Laser by Zac. This guy (I also interviewed him for a series of tips on laser cutting and engraving for a series I am publishing on a magazine) and his software works fine with the z-axis in positive and negative. I mean: when you laser cut, z-axis should start from highest value and goes down decreasing instead while you are engraving or milling, z-axis starts from zero and goes to negative values, at least by convention but, as a matter of fact, you can set up the vertical path as you prefer.

     

    His program works with GRBL (and is possible to update the GRBL firmware on an Arduino using his software too. The software supports the milling settings too, where it is expected that the g-code for the milling has come different parameters like speed instead of laser intensity.

     

    I have already found on Amazon several spindles sold (not super cheap but should be super precise so the price is correct) together with the motor controller as well as the Aluminium support that as I mentioned above it is not difficult to adapt to the z-axis. I have already modified one of the z-axis to support the laser I am using that is 7W and considerably bigger than the standard 2,5W max sold with the Eleks laser (I will use the structure of this laser engraver as I have already assembled and used three models of different sizes and it seems stable (laser needs also a high precision and repeatability.

     

    Instead about the board, it is not difficult to replace the signals of the actual board (It is Mana 2 SE) to manage the spindle with the speed controlled via PWM instead of the laser. You are also right about the power of the spindle (the one in the link example is about 4KW) but as well as the laser, excluding the PWM speed controlled by a logic signal, the power of the tool is independent. So probably this may not be a serious issue.

     

    Frankly, I prefer the program MACH 3 I use on the big CNC machine but the problem is that this software runs only with the parallel interface while the advantage of the T2 Laser is that it runs on USB.

     

    This is the actual scenario, I think that soon I will buy the spindle and start making tests to see what is preferable but I see hard to manage a parallel interface. I become crazy to set up a dedicated desktop Windows computer supporting the standard Parallel interface on the board. And – before you ask– the USB to parallel adapter is not accepted and the parallel won't work. This is the first thing I tried when I have assembled the other device.

     

    Enrico

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • shabaz
    shabaz over 7 years ago in reply to balearicdynamics

    Hi Enrico,

     

    There's another approach, that could be worth exploring. I too started to explore it last Xmas time, but have not progressed so much yet : (

    It concerns using BBB for the CNC controller. There is existing software for this, however the control board is not really open source : ( There's a firm selling the board, but it cost $100 or so from memory.

    So, I was trying to figure it out from the old schematic for it (a bit like the raspberry pi, an older schematic was available) what the connections to the BBB are, so that there can be an open source PCB that anyone can make, to plug on the BBB.

    I managed to map out the pins, but I still have to design the interface board to the stepper driver modules. Also, some legacy-type boards appear to need a lot of wiring, or need expensive DB9 type connections, I hoped to eliminate it mostly, using Ethernet or phone-like cables (not for the power, just for the control), from the interface board to the stepper drives (and have a little adapter PCB at the stepper drive end, for the least amount of wiring possible). I'd not figured out what connector to use for power, ideally something with ready-made cables, to reduce wiring effort with power too.

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • shabaz
    shabaz over 7 years ago in reply to balearicdynamics

    Hi Enrico,

     

    There's another approach, that could be worth exploring. I too started to explore it last Xmas time, but have not progressed so much yet : (

    It concerns using BBB for the CNC controller. There is existing software for this, however the control board is not really open source : ( There's a firm selling the board, but it cost $100 or so from memory.

    So, I was trying to figure it out from the old schematic for it (a bit like the raspberry pi, an older schematic was available) what the connections to the BBB are, so that there can be an open source PCB that anyone can make, to plug on the BBB.

    I managed to map out the pins, but I still have to design the interface board to the stepper driver modules. Also, some legacy-type boards appear to need a lot of wiring, or need expensive DB9 type connections, I hoped to eliminate it mostly, using Ethernet or phone-like cables (not for the power, just for the control), from the interface board to the stepper drives (and have a little adapter PCB at the stepper drive end, for the least amount of wiring possible). I'd not figured out what connector to use for power, ideally something with ready-made cables, to reduce wiring effort with power too.

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • More
    • Cancel
Children
  • balearicdynamics
    balearicdynamics over 7 years ago in reply to shabaz

    Sounds interesting, Shabaz. I know that the BBB is better than ever for this kind of applications. And here I have a couple of them, one with the WiFi onboard and one without. And the LinuxCNC shows good explanations on this device. But I know LinuxCNC and when I tested it it was light-years far from the Mach 3 software. About the connectors using the Rj45 for Ethernet is a great solution I already saw in other professional CNC for cheaper and reliable connectors.

     

    I am still in the evaluation of the possibilities phase so this can be considered, you are right. What kind of board it is what you mention?

     

    Enrico

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • shabaz
    shabaz over 7 years ago in reply to balearicdynamics

    Hi Enrico,

     

    The existing boards are listed here, but most of them are paid options. I wouldn't mind paying if they looked like they really met my needs, but with all the effort tailoring them, and wiring them, I hope it will be easier to just design a custom board. I tried thinking what I would like if I had a choice, and decided to have a larger board than BBB, so BBB becomes the daughter board, and an edge connection method for expansion if needed (i.e. with a separate backplane board) although it should work standalone. Also the connectors with ready-made cables, to reduce cable assembly.

    I'll try to sketch some system design, maybe we can turn it into some implementation if it looks worthwhile. I don't really know the quality compared to Mach 3, so that is another factor to consider as you say.

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • balearicdynamics
    balearicdynamics over 7 years ago in reply to shabaz

    If we don't try, we can't know. And at the end of the project sure we have a better knowledge than before. And I am almost sure that the machine will work.

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • genebren
    genebren over 7 years ago in reply to shabaz

    Nice link shabaz !  There are some interesting looking boards/capes there.  It should not be too difficult to come up with a nice universal machine driver board.  I have been a big fan of driver-less approaches to machine control like these:

     

    https://www.teknic.com/products/clearpath-brushless-dc-servo-motors/  - a little on the pricey side, but these motors are great performers, I used these on a high-end machine to polish gem stones.

    https://www.trinamic.com/company/news/news-detail/tmcm-1210-miniaturized-stepper-driver-module/ - simple to network (RS485), I have used these (or similar types) on several stepper based motion control systems.

     

    But, for a machine, with a limited number of axis, the more conventional approach of a non-distributed driver might make more sense.

     

    Sounds like fun!

    Gene

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • balearicdynamics
    balearicdynamics over 7 years ago in reply to genebren

    It was a long long time ago, 2009-2010 when I started studying how to make a mill machine. The video below shows the first working prototype.

    You don't have permission to edit metadata of this video.
    Edit media
    x
    image
    Upload Preview
    image

     

    The controller was a custom board based on Arduino with a series of ULN2003 and 2004 half-bridges and some other components. The spindle (here is shown a primitive test just to see if the principle was working) was controlled by PWM using a DC brushless motor. This can be considered my starting point from where I started playing with motors. When I built the prototype I have also developed – approach then abandoned – a non-standard language in Processing. From the pc a graphical interface was able to draw/engrave a PCB surface starting from the DXF of the layer. Then I evolved, done other choices and done more serious approaches to this problem, working with more standardized and complete software and hardware. But this first project created from scratch hardware, software and mechanics was very useful to go in-depth in the problems and issues that should be solved and considered when approaching a custom design for a PCB router.