Personal Blogs
  • Community Hub
  • More
Personal Blogs
Ralph Yamamoto's Blog Genmitsu CNC 3018-PRO - becoming useful
  • Blog
  • Documents
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: ralphjy
  • Date Created: 9 Aug 2019 5:46 AM Date Created
  • Views 10148 views
  • Likes 9 likes
  • Comments 24 comments
  • genmitsu cnc 3018-pro
  • cnc router
Related
Recommended

Genmitsu CNC 3018-PRO - becoming useful

ralphjy
ralphjy
9 Aug 2019

I had a minor victory on my road to figuring out how to use my new CNC router.

 

I received the 0.5mm carbide end mills that I bought on Amazon and used one to successfully shorten a proto PCB that I need for my LoRaXes project.  The mill has about 4 mm of cutting depth.  The PCBs that I'm cutting are nominally around 1.6 mm thick.  Not a very impressive looking cutter but it worked.  I increased the spindle speed to 3000 RPM and reduced the feedrate to 80 mm/min and set the cutting depth to 0.15 mm per pass.

 

image

 

Here is the shortened PCB next to one that is uncut:

image

 

The cut edges are very smooth but you can see that they are not quite straight.  Not sure if I can improve that with tweaking or if that's the inherent limitation of an inexpensive router and cheap end mills.  Only time and experience will tell.  Anyway, I'm pretty satisfied with the outcome.  The tool did what I needed it to do. 

  • Sign in to reply

Top Comments

  • Fred27
    Fred27 over 7 years ago +5
    Welcome to the world of CNC. It's fun, isn't it? You may know this already, but PCBs are particularly may to cut. They will blunt your endmills and the dusty is abrasive and nasty. For that particular…
  • Fred27
    Fred27 over 7 years ago +4
    I originally got a CNC mill (well, converted a mill myself) in order to mill PCBs. I ended up moving to etching as milling anything smaller than SOIC starts to get impractical. https://0xfred.wordpress…
  • balearicdynamics
    balearicdynamics over 7 years ago in reply to ralphjy +3
    The laser is controlled by PWM and there is a lot of relatively low power spindle and small diameter. The z-axis is not easy to be adapted (maybe with some 3D printed adjustment. The software I use is…
Parents
  • balearicdynamics
    balearicdynamics over 7 years ago

    Welcome on the CNC world image Do you plan to use it for PCB only or also something else? What kind of model? Some photos? If you need help, just ask.

     

    BTW... Maybe it is worth to open a group on CNC milling techniques, eventually finalized to the electronic design and prototyping support?

     

    Enrico

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • ralphjy
    ralphjy over 7 years ago in reply to balearicdynamics

    Hi Enrico,

     

    I did a blog post earlier when I first assembled this printer: Genmitsu CNC 3018-PRO

     

    I got the CNC mill to help with my electronic projects, so I'm hoping to also use it for things like small panels or face plates made out of plastic, acrylic, wood, or aluminum.  Hopefully will improve the quality and appearance of my builds.  There is also a low power (5.5W) laser module available that could be used for engraving (not sure if that is enough power to cleanly cut wood or acrylic).

     

    SainSmart is supposed to have a very active support community for their CNC products, but it's on Facebook and I really dislike Facebook.

     

    I'd support a group on Element14 if others would also like to start one.

     

    Ralph

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • balearicdynamics
    balearicdynamics over 7 years ago in reply to shabaz

    Sounds interesting, Shabaz. I know that the BBB is better than ever for this kind of applications. And here I have a couple of them, one with the WiFi onboard and one without. And the LinuxCNC shows good explanations on this device. But I know LinuxCNC and when I tested it it was light-years far from the Mach 3 software. About the connectors using the Rj45 for Ethernet is a great solution I already saw in other professional CNC for cheaper and reliable connectors.

     

    I am still in the evaluation of the possibilities phase so this can be considered, you are right. What kind of board it is what you mention?

     

    Enrico

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • shabaz
    shabaz over 7 years ago in reply to balearicdynamics

    Hi Enrico,

     

    The existing boards are listed here, but most of them are paid options. I wouldn't mind paying if they looked like they really met my needs, but with all the effort tailoring them, and wiring them, I hope it will be easier to just design a custom board. I tried thinking what I would like if I had a choice, and decided to have a larger board than BBB, so BBB becomes the daughter board, and an edge connection method for expansion if needed (i.e. with a separate backplane board) although it should work standalone. Also the connectors with ready-made cables, to reduce cable assembly.

    I'll try to sketch some system design, maybe we can turn it into some implementation if it looks worthwhile. I don't really know the quality compared to Mach 3, so that is another factor to consider as you say.

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • balearicdynamics
    balearicdynamics over 7 years ago in reply to shabaz

    If we don't try, we can't know. And at the end of the project sure we have a better knowledge than before. And I am almost sure that the machine will work.

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • genebren
    genebren over 7 years ago in reply to shabaz

    Nice link shabaz !  There are some interesting looking boards/capes there.  It should not be too difficult to come up with a nice universal machine driver board.  I have been a big fan of driver-less approaches to machine control like these:

     

    https://www.teknic.com/products/clearpath-brushless-dc-servo-motors/  - a little on the pricey side, but these motors are great performers, I used these on a high-end machine to polish gem stones.

    https://www.trinamic.com/company/news/news-detail/tmcm-1210-miniaturized-stepper-driver-module/ - simple to network (RS485), I have used these (or similar types) on several stepper based motion control systems.

     

    But, for a machine, with a limited number of axis, the more conventional approach of a non-distributed driver might make more sense.

     

    Sounds like fun!

    Gene

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • balearicdynamics
    balearicdynamics over 7 years ago in reply to genebren

    It was a long long time ago, 2009-2010 when I started studying how to make a mill machine. The video below shows the first working prototype.

    You don't have permission to edit metadata of this video.
    Edit media
    x
    image
    Upload Preview
    image

     

    The controller was a custom board based on Arduino with a series of ULN2003 and 2004 half-bridges and some other components. The spindle (here is shown a primitive test just to see if the principle was working) was controlled by PWM using a DC brushless motor. This can be considered my starting point from where I started playing with motors. When I built the prototype I have also developed – approach then abandoned – a non-standard language in Processing. From the pc a graphical interface was able to draw/engrave a PCB surface starting from the DXF of the layer. Then I evolved, done other choices and done more serious approaches to this problem, working with more standardized and complete software and hardware. But this first project created from scratch hardware, software and mechanics was very useful to go in-depth in the problems and issues that should be solved and considered when approaching a custom design for a PCB router.

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • balearicdynamics
    balearicdynamics over 7 years ago in reply to genebren

    It was a long long time ago, 2009-2010 when I started studying how to make a mill machine. The video below shows the first working prototype.

    You don't have permission to edit metadata of this video.
    Edit media
    x
    image
    Upload Preview
    image

     

    The controller was a custom board based on Arduino with a series of ULN2003 and 2004 half-bridges and some other components. The spindle (here is shown a primitive test just to see if the principle was working) was controlled by PWM using a DC brushless motor. This can be considered my starting point from where I started playing with motors. When I built the prototype I have also developed – approach then abandoned – a non-standard language in Processing. From the pc a graphical interface was able to draw/engrave a PCB surface starting from the DXF of the layer. Then I evolved, done other choices and done more serious approaches to this problem, working with more standardized and complete software and hardware. But this first project created from scratch hardware, software and mechanics was very useful to go in-depth in the problems and issues that should be solved and considered when approaching a custom design for a PCB router.