Arduino Forum Is it possible to transmit and receive smell?
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
  • Replies 48 replies
  • Subscribers 403 subscribers
  • Views 4905 views
  • Users 0 members are here
  • smell-o-vision
  • electronic_smell_sensor
  • odor
  • mission odor electronics
  • smell
Related

Is it possible to transmit and receive smell?

dixonselvan
dixonselvan over 9 years ago

Odor electronics a possible extension to the current electronics world that would revolutionize the entertainment & safety domains. The integration of odor into the electronic world has only attempts with some success. Also there has been some products in the market.

 

Help me in the progress by your valuable comments below. Share me your experience if you have any image

 

I was able to collect and machine learn smell information and replicating the same in my bachelor's degree project, which I will be posting here soon.

 

I couldn't find time to recover my bachelor's degree project where I had used MATLAB's machine learning package. But I was able to remodel the whole system and using AWS Machine Learning service and Arduino MKR1000, I have developed a much similar project. The details of the same are posted here - Cue System for Anosmia and Smart WheelChair #11 - Machine Learning and Demo [Completed] and here - Cue System for Anosmia and Smart WheelChair #10 - Gas Sensors and Machine Learning in the 'Design for a Cause' design challenge space.

 

 

Message was edited by: Dixon Selvan

  • Sign in to reply
  • Cancel

Top Replies

  • johnbeetem
    johnbeetem over 9 years ago in reply to dixonselvan +7
    Dixon Selvan wrote: Paul Ellison wrote: I've been known to build devices that transmit a burning smell... Could you be more elaborate like what does your burning smell refer to I think…
  • COMPACT
    COMPACT over 9 years ago +5
    Another alternative is to hook up a variety of capacitors, resistors and ICs at the transmitter end and have a matched pair at the receiving end. For the resistors you can pump in enough power for them…
  • dougw
    dougw over 9 years ago in reply to dixonselvan +5
    Esters with low molecular weight often have fragrant odours and are commonly used as fragrances, perfumes, essential oils, food flavourings, cosmetics, etc. Usually, esters are derived from a carboxylic…
Parents
  • neuromodulator
    neuromodulator over 7 years ago

    Smell is the perception of odorants, or airborne chemicals that an olfactory system can detect. There are many difficulties when it comes to representing all possible combinations we can detect. Different humans express different kind of olfactory receptors (olfactory transducers), each human has different olfactory capabilities (put differently, some smells may not be detected the same way (or detected at all) between different humans).  There are hundreds of ORs (olfactory receptors) that a human can express (produce),  each OR gets activated by multiple chemicals. Each ORN (olfactory receptor neuron) expresses a single OR and a single chemical is encoded as a linear combination of ORN activity. Ideally one would want to be able to activate each OR individually, then with a bank of hundreds of chemicals one would be able to simulate each odour, but that's not possible because chemicals activate combinations of ORs. A more practical approach may take fewer odorants which could be combined together to generate a much wider amount of odors, but I'm not sure how many "common" odors could be generated or approximated in this way.



    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • neuromodulator
    neuromodulator over 7 years ago

    Smell is the perception of odorants, or airborne chemicals that an olfactory system can detect. There are many difficulties when it comes to representing all possible combinations we can detect. Different humans express different kind of olfactory receptors (olfactory transducers), each human has different olfactory capabilities (put differently, some smells may not be detected the same way (or detected at all) between different humans).  There are hundreds of ORs (olfactory receptors) that a human can express (produce),  each OR gets activated by multiple chemicals. Each ORN (olfactory receptor neuron) expresses a single OR and a single chemical is encoded as a linear combination of ORN activity. Ideally one would want to be able to activate each OR individually, then with a bank of hundreds of chemicals one would be able to simulate each odour, but that's not possible because chemicals activate combinations of ORs. A more practical approach may take fewer odorants which could be combined together to generate a much wider amount of odors, but I'm not sure how many "common" odors could be generated or approximated in this way.