Arduino Forum Is it possible to transmit and receive smell?
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
  • Replies 48 replies
  • Subscribers 403 subscribers
  • Views 4883 views
  • Users 0 members are here
  • smell-o-vision
  • electronic_smell_sensor
  • odor
  • mission odor electronics
  • smell
Related

Is it possible to transmit and receive smell?

dixonselvan
dixonselvan over 9 years ago

Odor electronics a possible extension to the current electronics world that would revolutionize the entertainment & safety domains. The integration of odor into the electronic world has only attempts with some success. Also there has been some products in the market.

 

Help me in the progress by your valuable comments below. Share me your experience if you have any image

 

I was able to collect and machine learn smell information and replicating the same in my bachelor's degree project, which I will be posting here soon.

 

I couldn't find time to recover my bachelor's degree project where I had used MATLAB's machine learning package. But I was able to remodel the whole system and using AWS Machine Learning service and Arduino MKR1000, I have developed a much similar project. The details of the same are posted here - Cue System for Anosmia and Smart WheelChair #11 - Machine Learning and Demo [Completed] and here - Cue System for Anosmia and Smart WheelChair #10 - Gas Sensors and Machine Learning in the 'Design for a Cause' design challenge space.

 

 

Message was edited by: Dixon Selvan

  • Sign in to reply
  • Cancel

Top Replies

  • johnbeetem
    johnbeetem over 9 years ago in reply to dixonselvan +7
    Dixon Selvan wrote: Paul Ellison wrote: I've been known to build devices that transmit a burning smell... Could you be more elaborate like what does your burning smell refer to I think…
  • COMPACT
    COMPACT over 9 years ago +5
    Another alternative is to hook up a variety of capacitors, resistors and ICs at the transmitter end and have a matched pair at the receiving end. For the resistors you can pump in enough power for them…
  • dougw
    dougw over 9 years ago in reply to dixonselvan +5
    Esters with low molecular weight often have fragrant odours and are commonly used as fragrances, perfumes, essential oils, food flavourings, cosmetics, etc. Usually, esters are derived from a carboxylic…
Parents
  • jw0752
    jw0752 over 9 years ago

    If I have a color document that has information on it like a schematic I can scan it and email it to you and your printer can replicate it. We are not transporting the document like star trek we are analyzing it and turning it into a digital model, transmitting it, and then reassembling a facsimile using a printer. There is no reason that we could not sample an odor in the air with suitable sensors, digitize the data, send it to a suitable machine that could dispense aerosol of any number of chemicals into the air at the receiving end to replicate the odor. I do not see the difference between sending color information as opposed to olfactory information. The difference is only in the importance of the information to present day communications. The colors of the schematic are important to us. Whether the schematic smells like ink, or old wood, or my spilled Old Spice is irrelevant to most of our important technical and interpersonal communications. D_Hersey rightly points out the a lot of our brain mass is dedicated to smell. I do not know why this does't make smell more important in our lives but it probably goes back to evolutionary stages where it "was" more of a survival mechanism. This has evolved into a better discussion than I thought it would.

    John

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • screamingtiger
    screamingtiger over 9 years ago in reply to jw0752

    Right, we have a printer.  We would need a printer for smell, so if I wanted to send you the smell of lemon, your machine must reproduce the lemon molecules.

     

    I suppose it could have numerous chemicals it could combine to make the smell.  But it would be very large and dangerous!

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • shabaz
    shabaz over 9 years ago in reply to screamingtiger

    Hi!

     

    Our sense of taste is not great in some ways. We think we're just evaluating what the tongue senses but part of 'taste' is the smell of something. We easily get confused when we have a cold.

    And I can't tell the difference between what I think nail polish may taste like, and pear-flavoured jelly beans : ) If it wasn't green-coloured I would have no idea what it was, so looks play a part too, as does texture. Plus we have few ways to describe taste except with items, and items have a physical look. (Similarly I couldn't describe a pear smell without saying that it smelt like a pear, or a fruity smell, or a nail polish smell : ). The physical three items - pear, generic fruit, nail polish are completely different. I'd have to find a tangible item basically).

    Basically in real terms when we say "taste", we don't just mean what the tongue is evaluating. We include the extra like smell and vision, so we say that a meal tasted delicious etc., we might say something different if we couldn't see it or if it wasn't juicy when it should be, etc.

    So, probably smell can be confused too without visual prompts. It is maybe possibly that only a subset of smells are needed, and with the right prompts, we can be fooled into thinking it is something it isn't. In other words, if we need a device (can't think why though, but others may have needs for it) that conveys smell, then it could be restricted to a device with fewer chemicals, that needs to be used combined with vision perhaps!

    However this does mean that the sensor device would also need to combine smell with (say) vision in order to transmit the correct data for the

    smell generator..

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • shabaz
    shabaz over 9 years ago in reply to screamingtiger

    Hi!

     

    Our sense of taste is not great in some ways. We think we're just evaluating what the tongue senses but part of 'taste' is the smell of something. We easily get confused when we have a cold.

    And I can't tell the difference between what I think nail polish may taste like, and pear-flavoured jelly beans : ) If it wasn't green-coloured I would have no idea what it was, so looks play a part too, as does texture. Plus we have few ways to describe taste except with items, and items have a physical look. (Similarly I couldn't describe a pear smell without saying that it smelt like a pear, or a fruity smell, or a nail polish smell : ). The physical three items - pear, generic fruit, nail polish are completely different. I'd have to find a tangible item basically).

    Basically in real terms when we say "taste", we don't just mean what the tongue is evaluating. We include the extra like smell and vision, so we say that a meal tasted delicious etc., we might say something different if we couldn't see it or if it wasn't juicy when it should be, etc.

    So, probably smell can be confused too without visual prompts. It is maybe possibly that only a subset of smells are needed, and with the right prompts, we can be fooled into thinking it is something it isn't. In other words, if we need a device (can't think why though, but others may have needs for it) that conveys smell, then it could be restricted to a device with fewer chemicals, that needs to be used combined with vision perhaps!

    However this does mean that the sensor device would also need to combine smell with (say) vision in order to transmit the correct data for the

    smell generator..

    • Cancel
    • Vote Up +2 Vote Down