Arduino Forum Different result if connecting 9V?
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
  • Replies 15 replies
  • Subscribers 405 subscribers
  • Views 1573 views
  • Users 0 members are here
  • tmp 36
  • problem
  • power supply
  • arduino
  • sensor
Related

Different result if connecting 9V?

Former Member
Former Member over 9 years ago

I have done the project in Jeremy Blum "Explorign Arduino" related to the three color LED changing with the temperature. It works right when connected with USB, but it is always red if connected to 9V.

Did I do anything wrong? is it normal? how can I solve it?

The sensor is a TMP-36image

  • Sign in to reply
  • Cancel

Top Replies

  • clem57
    clem57 over 9 years ago +1
    To learn, you need to read the datasheet on the sensor and think what changes with the switch from USB to 9 volt battery. Clem
  • Former Member
    Former Member over 9 years ago +1
    Per John's comment, I'm assuming you're using a 9V barrel adapter. A couple of points: 1. You have to get enough power for the Arduino, the LED, the TMP36, etc. I never use carbon-zinc batteries or cells…
  • clem57
    clem57 over 9 years ago in reply to Former Member +1
    Sensors are very dependant on the voltage provided. Change the voltage, they need to be recalibrated. Try a separate independent power source on the rail to the sensor that is 5V. repeat the experiment…
Parents
  • jc2048
    jc2048 over 9 years ago

    The TMP36 output is 10mV per degree C and is designed to be 750mV at 25C.

     

    The sensor is specced for -40 to +125, which means a voltage range at the output of 0.1V to 1.75V. That range is designed to allow operation off of a low voltage supply like 3.3V or less, but it does mean that in this case you are only using about a third of the A/Ds range.

     

    I'm not really familiar with the Uno, but it looks like the A/D is 10-bit and is operating ratiometrically [taking the supply as its reference voltage]. Let's try calculating the reading for 25 degrees C (ie an input of 0.75V) for two different supply voltages [I've just arbitrarily chosen plus or minus 4% from a nominal 5V]

     

    supply 5.2V, reading 148  (0.75 / 5.2V) * 1024
    supply 4.8V, reading 160  (0.75 / 4.8V) * 1024

     

    Each step from the A/D is equivalent to approximately 1/2 a degree, so that [quite modest] change in the supply constitutes about 6 degrees C in the calculated temperature. Since you are seeing about 2 degrees, it means your supply change is less than that.

     

    Point is, the design is very sensitive to the supply voltage.

     

    If you want it to work accurately regardless of the supply voltage then there are several options:

     

    1) use the internal 1.1V reference of the ATMEGA328. That will be accurate and won't vary with the supply voltage. Limits you to 60 degrees C if you connect the sensor directly. You could get the full range if you use a potential divider on the sensor output.

     

    2) provide your own reference and set the processor to use that rather than the supply. A 2.5V reference into AREF would be appropriate. [It might be that the Uno software would conflict with having an external reference, so have a look around and see if this is generally done or not. If you are still not sure, put a resistor between the reference output and the AREF pin so that you don't have two outputs driving each other directly and look at the voltages either end to see if there is any difference before your own code runs and sets up the processor to use the external reference.]

     

    3) A final alternative would be to amplify the output from the sensor so that it makes better use of the A/D's input range. The effect of any supply change would then decrease in proportion. So if you amplified it 3 times, the effect from the supply change would be a third. If you don't need the full -40 to +125 degree range, you could amplify it even more with just the range you were interested in giving a full 0 to +5V at the A/D pin.

     

    All would require you to change the way the software calculates the temperature from the result- so only try it if you are confident programming, though I'm sure you'd get a lot of help from people here if you wanted to give it a go.

     

    And the TMP36 could do with a decoupling capacitor across its supply pins.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • shabaz
    shabaz over 9 years ago in reply to jc2048

    The same problem is elsewhere too - I just saw this which uses the exact same TMP36 part but with a Raspberry Pi:

    http://raspi.tv/2016/using-mcp3008-to-measure-temperature-with-gpio-zero-and-raspio-pro-hat

     

    The layout shown at that link uses the TMP36 and an MCP3008 but no decoupling : (

    The £25 'experimenters kit' with these ICs contains no decoupling capacitors either.

     

    My basic 'experimenter's kit' is still a bulk pack of through-hole resistors and capacitors from Maplin, and loads of SMD Rs and Cs from Farnell

    and this very nice SMD component containerthis very nice SMD component container - I have several of them. They are the best I've found, if they are dropped the parts don't get

    mixed up like other containers, nor do they leak from gaps if turned upside down. I use small stickers from a stationery store to label them.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • michaelkellett
    michaelkellett over 9 years ago in reply to shabaz

    I just left them (on raspi.tv) a post asking about the decoupling caps - I feel it's such a shame that so many people jumping on the "education" bandwagon seem to know so little about basic practical electronics.

     

    MK

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • michaelkellett
    michaelkellett over 9 years ago in reply to shabaz

    I just left them (on raspi.tv) a post asking about the decoupling caps - I feel it's such a shame that so many people jumping on the "education" bandwagon seem to know so little about basic practical electronics.

     

    MK

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
Children
  • shabaz
    shabaz over 9 years ago in reply to michaelkellett

    Hi Michael,

     

    Good idea, I hope he corrects it, I just saw there was a corresponding kickstarter which achieved >1k backers so quite a number of beginners will be watching those videos..