Arduino
  • Products
  • More
Arduino
Arduino Forum Learning about H-bridges and transistors
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Arduino to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Replies 38 replies
  • Answers 8 answers
  • Subscribers 422 subscribers
  • Views 4746 views
  • Users 0 members are here
  • frontpage
  • h-bridge
  • transistors
Related

Learning about H-bridges and transistors

ovidiub13
ovidiub13 over 10 years ago

I'm trying to learn about transistors and H bridges towards a final goal of controlling a bipolar stepper motor with Arduino.

 

I've done the following half H-bridge in the process of learning:

image

My first question: Why can't I use a single resistor to connect the base of both transistors to ground?

  • Sign in to reply
  • Cancel

Top Replies

  • strb
    strb over 10 years ago +1 suggested
    I'm not sure that this schematic works... the led isn't reverse polarized? Anyway use a pnp as pullup transistor and a npn as pulldown, it's a good thing to put also a limiter resistor to control the current…
  • strb
    strb over 10 years ago in reply to clem57 +1
    Great "how link" clem57
  • mcb1
    mcb1 over 10 years ago in reply to ovidiub13 +1 suggested
    What I'm having issues understanding is how transistors work You can consider a transistor as a switch (in this case they are either ON or OFF) The control part of the switch is the base to emitter (NPN…
Parents
  • ovidiub13
    0 ovidiub13 over 10 years ago

    I fixed it. I think.

     

    I've added a resistor for the LEDs, and 2 bigger resistors for the transistors bases to + to make sure the gates are closed when the button is not pressed.

     

    image

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
Reply
  • ovidiub13
    0 ovidiub13 over 10 years ago

    I fixed it. I think.

     

    I've added a resistor for the LEDs, and 2 bigger resistors for the transistors bases to + to make sure the gates are closed when the button is not pressed.

     

    image

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
Children
  • mcb1
    0 mcb1 over 10 years ago in reply to ovidiub13

    I can't recall you indicating that it stayed ON at any point ... maybe I missed it.

    But adding the 2 x 4k7 resistors are good practice.

     

    If you've been reading our replies, you'll note that Q2 and Q1 never switch ON.

    You can prove this by shorting the Emitter to Base of Q2 and Q1 and you'll find it works exactly the same.

     

     

    Mark

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • ovidiub13
    0 ovidiub13 over 10 years ago in reply to mcb1

    How can I fix this? How can I make them work?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • shabaz
    0 shabaz over 10 years ago in reply to ovidiub13

    There are likely many errors in this circuit but it is difficult to follow because the parts are thrown together on the schematic not even resembling a H-bridge formation since the left side has its ends folded back on itself (why?).

     

    I can't follow the circuit the way it has been drawn (if you've already studied H-bridge circuits which you say you have, then you know that yours is drawn as a mess - not something to show to teachers perhaps if you're a student), so I can't spot all the errors without more effort.

     

    However, one negative is that you're using 4 identical BJT's.

    There is close to a 1V drop loss for lower legs of the H-bridge (and by lower I mean the ones at the bottom if you'd drawn it the correct way up rather than up-side down), plus about 0.2V for the top legs of the H-bridge, so there will be less than 4V available to the LED or motor. As people have mentioned, if you're using LEDs then there should be a series resistor for them.

    The circuit would be better if the lower BJT's were NPN. Or even better if MOSFETs were used.

    And won't work (well or for long) with inductive loads. If you google H-bridge, you'll see how people resolve that.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • mcb1
    0 mcb1 over 10 years ago in reply to ovidiub13

    How can I fix this? How can I make them work?

    prove my point by shorting out the E-B first to confirm the suspicion.

     

     

    A quick check using Google shows this.

    H Bridge motor driver theory & practical circuit using transistors- animation/ simulation: Getting started with Robotics…

    This also explains how it works.

     

     

    We already pointed out that you don't require a bridge to drive a stepper.

    HOWEVER unless you advise what stepper you intend using, then it's hard to help.

     

    shabaz is quite right that your circuit is not designed for inductive loads, and there are plenty of simple IC's that take all the hard work out of it for you.

     

    Mark

     

    edit 3x spelling mistakes .. I blame the keyboard not keeping up.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • clem57
    0 clem57 over 10 years ago in reply to mcb1
    For the how to, read nathandumont.com : H-Bridge Tutorial that explains the how.

    5 days ago my sentiment exactly. Thanks mcb1 for getting back to reality. What goes on above is playing with circuits without understanding them trying to reach H bridges.

    Cheers!

    Clem

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • mcb1
    0 mcb1 over 10 years ago in reply to clem57

    clem57

    Thanks.

    I did look at you links, but it relied on 4 seperate inputs, and given the issues the OP had, I felt he needed something closer to his circuit.

     

    The other danger with two seperate switches, is that if both are on .... bye bye transistors.

     

    Mark

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • not2xs
    0 not2xs over 10 years ago in reply to ovidiub13

    If you want to get on to efficiently and reliably driving the stepper motor then as others have said a chip will be easiest; otherwise you will need to do everything the chip designer did. If you want to learn about H-bridges, the links supplied by mcb1 and Clem show good explanations. If you want to understand how transistors work, here is a quick but somewhat thorough description:

     

    The base to emitter connection works just like a semiconductor diode. Perhaps easiest to think of it as a variable resistor where the resistance changes with the voltage. Like a diode, if you try to drive it "backwards" it behaves like a near infinite resistance, and near no current flows. If you try to drive it "forwards", like a semiconductor diode if the voltage is less than about a half a volt it still behaves like a near infinite resistance, but somewhere a bit above that voltage the resistance starts to drop, until by around 0.7V (for silicon devices) the resistance is very low, nearing zero-ohms (except for that 0.7V lurking inside). The exact voltage between base and emitter where this happens will vary, mostly with temperature. That is why you typically connect an external resistor to the base, to control how much current flows there, otherwise the transistor will allow more than it can handle.

     

    The next thing to know about a transistor is it has a parameter (properly specified as h-subscript-fe if your fonts will allow that) I will abbreviate as h-fe here. This is the ratio of how much current will flow in the collector relative to how much in the base, if the rest of the circuit will allow it. Typically the h-fe will be somewhere around 1000 to 100000, and it will vary wildly with temperature and from individual transistor to transistor (even if they have the same part number). This means that the current in the collector will be 1000 to 100000 times the amount of current in the base - IF THE REST OF THE CIRCUIT WILL ALLOW IT. The current in the transistor's emitter is the sum of the current in the base and collector. However, when using transistors as switches, you usually want to drive them into "saturation". This is where the circuit cannot manage the collector to base current ratio and the collector to emitter voltage goes really low (below half a volt) while the transistor is trying really hard. With very low collector to emitter voltage, not much power gets consumed inside the transistor meaning it does not get as hot and more power is available to go into the load.

     

    There are two common configurations for connecting up a transistor, and you have both in your circuit above. One frequently used way is called "common emitter", here the emitter is wired to some known voltage, the base is wired to have some current flow into it (or not) while considering that 0.7V drop, and the "load" is connected to the collector where a higher amount of current is switched. Another common way is called "emitter follower", where the base is driven to a known voltage, the "load" is connected to the emitter, and the emitter will stay around 0.7V away from the base voltage with any needed extra current to achieve that coming through the collector. To get an emitter-follower into saturation, the base will need to be driven to a voltage beyond the battery voltage for the rest of the circuit. This is why it is most common to suggest combining NPN and PNP transistors into the H-bridge, they can all be wired common-emitter and saturated without using multiple supply voltages.

     

    If you want to use transistors as amplifiers instead of switches it gets more difficult due to having to deal with the variations mentioned above. When dealing with motors or coils you should be aware of the "kickback" voltage spike they produce, hence all the extra diodes (and sometimes capacitors) in well-designed H-bridges.

     

    If this is what you were interested in learning, then good for you.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • jc2048
    0 jc2048 over 10 years ago in reply to not2xs

    "Typically the h-fe will be somewhere around 1000 to 100000"

     

    I would disagree with that statement. A few hundred would be more typical for hFE (datasheets usually quote hFE rather than hfe) for small-signal use (collector current 10mA, or so). 100-600 is a realistic range for real devices you might encounter. With medium- and high-power devices, you'd normally be looking at less than 100 once you get up to collector currents of a few amps.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • Robert Peter Oakes
    0 Robert Peter Oakes over 10 years ago in reply to jc2048

    The gains etc are based on the devices shown in the posted schematics, looking at manufacturer data sheets, to exceed these ratings may be possible but you risk thermal and other damage to the device. But as you say, there are other devices you can use, in my case I would go with MOSFETS or other versions of FETs for the switches , they have other issues to deal with, I just happen to like them image

     

    Peter