Arduino Forum Arduino connection help
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
  • State Suggested Answer
  • Replies 38 replies
  • Answers 11 answers
  • Subscribers 405 subscribers
  • Views 3125 views
  • Users 0 members are here
Related

Arduino connection help

alexparker2002
alexparker2002 over 8 years ago

I have made an integrated arduino monitoring system with 3 sensors....

I have used leds to show their values

But i want to add a lcd to it and an ethernet shield to it..... Is it possible?

Let me tell you that I am a beginner.....

Ive attached the schematics please modify it and tell me...... Please!!!!!!

Attachments:
imageFA5RM0AHX1W2JT3.pdf
  • Sign in to reply
  • Cancel

Top Replies

  • Robert Peter Oakes
    Robert Peter Oakes over 8 years ago +2 suggested
    You should be able to do it but You will need to use a WS5100 type ethernet shield as it will offload some of the software to the hardware. It will plug into the Arduino UNO, it uses pins 10,11,12,13 you…
  • beacon_dave
    beacon_dave over 8 years ago in reply to beacon_dave +2 suggested
    Also perhaps be aware that the power rails on some breadboards are not continuous but instead are interrupted half way along. You may find that you need to place a jumper on your ground rail between block…
  • mcb1
    mcb1 over 8 years ago in reply to alexparker2002 +2 suggested
    alexparker2002 Part of learning is the LEARNING part. Having someone do all the work for you is not learning, but copying . I suggest you explore the examples that are provided in the Arduino IDE. There…
Parents
  • clem57
    0 clem57 over 8 years ago

    The problem is the limited memory resources both SDRAM and flash. Have you looked at how much is currently used? You may want to approach this from another angle. If you tie in a Raspberry Pi 3, you can use UART to communicate and handle the higher level functions on the Pi 3 IMHO.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • clem57
    0 clem57 over 8 years ago

    The problem is the limited memory resources both SDRAM and flash. Have you looked at how much is currently used? You may want to approach this from another angle. If you tie in a Raspberry Pi 3, you can use UART to communicate and handle the higher level functions on the Pi 3 IMHO.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Children
  • alexparker2002
    0 alexparker2002 over 8 years ago in reply to clem57

    See.... In my schematics... Along with the leds i want to display the sensor values on a lcd screen... Is it possible?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • clem57
    0 clem57 over 8 years ago in reply to alexparker2002

    Possible if you look at the above comment

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • beacon_dave
    0 beacon_dave over 8 years ago in reply to alexparker2002

    Perhaps take a look at this Arduino tutorial on LCD displays to get started:

    Tutorial 13 for Arduino: Liquid Crystal Displays

     

    If you want something more graphical then you could perhaps take a look at one of these type of displays:

    Resistive 4.3" GEMmodule

    which off-load the graphics processing onto the display module only requiring the data updates to be sent over a UART serial connection from the Arduino.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • beacon_dave
    0 beacon_dave over 8 years ago in reply to beacon_dave

    As for the Ethernet shield, have you taken a look at:

    https://www.arduino.cc/en/Guide/ArduinoEthernetShield

     

    Tom Igoe has written an interesting book called 'Making Things Talk' which covers this sort of area, so you may want to try and get hold of a copy. The 3rd edition is due to be published soon:

    https://www.amazon.co.uk/Making-Things-Talk-Sensors-Networks/dp/1680452150/ref=la_B001K8AUGU_1_5

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer