Arduino
  • Products & Partners
  • More
Arduino
Arduino Forum Arduino and Transistors Question - RE: School Musical Production
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Arduino to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Replies 126 replies
  • Answers 2 answers
  • Subscribers 421 subscribers
  • Views 11060 views
  • Users 0 members are here
  • raspberry
  • transistor
  • pi
  • arduino
Related

Arduino and Transistors Question - RE: School Musical Production

wallarug
wallarug over 12 years ago

One of the directors has asked me to create a special backdrop for our college musical. This particular backdrop has a particular design (see below) that includes LED strip lighting to give the feel of a 1920s casino sign – similar to what is seen today in Las Vegas.

I  have done up a detailed design for this sign, based off the rough sketch given to me by the director and the dimensions of the backdrop.  On this diagram, the arrangement of the LED strip lighting can be seen.

image

          

The LED Strip lighting that will be bought for this project will be sourced from Jaycar – “Low Cost 5m Flexible Adhesive LED Strip Light – Warm White” (ZD0577).  According to the specifications off Jaycar’s website, these LED lights need 1.1 Amps per metre @ 12 volts.  This means that the longest segments of lights need 1.1 * 1.5 = 1.65 Amps of power (rounded up by 20% for safety: 2.0 Amps @ 12 volts).

 

This would not be an issue if I was just turning these LED Strips on and off with mains power BUT I want to control these LEDs via an Arduino, so that they can do fancy things like flash and chase.  That means that I would need a circuit to control these lights with an Arduino so that everything remains safe and does not blow up.

I have come up with this circuit (below) using a couple of NPN transistors and two power supplies.  In the diagram below, I am aware that the transistor pinouts are EBC.  The ones I am going to buy have a pinout of BCE.

 

image

 

The only problem with this is that I have very little understanding of transistor circuits.  What this circuit has to be able to do is:

  • Using the smallest amount of current from the Arduino (at 5 volts) or a Raspberry Pi (3v3 volts), turn on the circuit to allow the 12 volts that powers the LED strip lighting to flow.

 

I was thinking of using either TIP41C NPN Transistors (in a darlington Array) or TIP122 NPN transistors.

 

This circuit will be replicated 8 times over to accommodate for the number of LEDs I am controlling.

 

 

Can anyone help me:

  1. Design a circuit that will work 100% and will be safe (ie: low heat)
    1. This includes base resistance
  1. Confirm which transistors I should be using for this project.

 

Any help will be much appreciated.

  • Sign in to reply
  • Cancel

Top Replies

  • Robert Peter Oakes
    Robert Peter Oakes over 12 years ago +1
    Sorry the one I suggested wont work, but this one should http://www.jaycar.com.au/productView.asp?ID=ZK8821 10+ current rating and at 0.016ohms it should be good for your needs pdf here http://www.vishay…
  • mcb1
    mcb1 over 12 years ago in reply to jw0752 +1
    John If you are referring to this It means that at a gate voltage of 1.6 typ, a current of 250uA will be flowing in the Drain. If you look here, you can see that from 3 to 3.3v will give you enough to…
  • D_Hersey
    D_Hersey over 12 years ago +1
    Solenoid Whapper:
Parents
  • wallarug
    0 wallarug over 12 years ago

    Thank you everyone for your feedback.

     

    It seems that the best option for this project is FETs (from the above feedback).  Douglas' schematic seems like the way to go except with only one LED strip in the circuit.

     

    1.  Can anyone suggest a suitable FET from Jaycar as this is where I will be sourcing all my materials?

     

    Just to clarify:

    i.  The circuit will power only ONE LED strip.  I will be having 7 of the same circuit on a PCB to accommodate 7 LED strips.

    ii.  Logic voltage will be 5 volts (from arduino)

    iii. Circuit voltage will be 12 volts from an external power source.

     

    Thanks again guys for all the help!

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • Problemchild
    0 Problemchild over 12 years ago in reply to wallarug

    Looks like the  choice isnt that great at least at the UK Jaycar you may consider going for the low power 2n7000 FET on the output of the Logic then have it switch the Gate of the bigger FETS they have using the available 12V supply.

     

    The few IRF transistors are more suited to 5V minimum........

    Doh .....Saw Arduino...

    IRF540 should be OK in that case

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • Problemchild
    0 Problemchild over 12 years ago in reply to wallarug

    If this was a massively inductive or capacitive load this might of been an issue but in this case you are good to operate that PWM at any reasonable frequency you can achieve with the Arduino

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • wallarug
    0 wallarug over 12 years ago in reply to Problemchild

    Sweet.  Thanks for all the help.

     

    I think this is what I am going to go with:

    Arduino (5V) to 2N7000 (driving 12V) to IRF540N which will switch the LEDs on.

     

    I will get back to you if I need any further help.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • mcb1
    0 mcb1 over 12 years ago in reply to Problemchild

    any way no real need for a resistor

    IMO you should add a resistor and a diode up to the 5v, at the Arduino end.

    I've seen fets destroyed and its often the Drain to Gate that goes, dumping the load voltage (12v in this case) up the gate.

     

    However since this is a short use device the risk is minimal.

     

    mark

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • dougw
    0 dougw over 12 years ago in reply to wallarug

    1. The FET suggested by Peter (or the one I suggested) should not get hot or damage anything during low frequency operations. (the solution suggested by John can work as well, but this explanation doesn't cover that solution or associated risks)

    2. A resistor on the gate protects the arduino, but can cause the FET to get hot during high frequency operations (like PWM) so best design depends on how often the FET will get switched. Either resistor in or out should be safe for this application - a low value resistor like 470 ohms is a reasonably even compromise slightly favouring the more expensive arduino component.

    3. These FETs only require about 100 nanoamps to the gate in static states, even with a 2 Amp load. During switching the gate capacitance must be charged and discharged causing transient currents to flow. Atmel seems to use average current to define danger levels (calculated by Voltage x Gate Capacitance x Frequency) Where frequency here would be PWM frequency. This should be under 1 mA for these FETs in this application - well within the arduino output limit.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • Robert Peter Oakes
    0 Robert Peter Oakes over 12 years ago in reply to dougw

    Nice explanation Doug, I quite agree and I just checked my kitchen dimmer which is basically the same circuit and it is using a 1K resistor, I guess it was laying around in my junk box when I needed one, either way it only needs to be enough to limit the current a bit but still way below the limits of the Arduino pins

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • Problemchild
    0 Problemchild over 12 years ago in reply to mcb1

    One thing to note here with the resistor and diode Mark is that the non logic level FETs would not fully turn on or take longer to do so which I believe is what Doug is alluding to when he is talking about the FET heating up during PWM. I figured that his device wasn't out for the long term thus KISS was the order of the day. If Jaycar is the source then I would be more than happy to use a few of those FETs that were specified.

    For the type of application specified I don't see any reason to guild the Lilly. The PWM frequency is likely to be less than a few KHZ no need for more to achieve a good dimming effect. Wallarug should take a few photos and link them on his Blog when he completes the project be nice to see a simple project all nicely executed !

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • mcb1
    0 mcb1 over 12 years ago in reply to Problemchild

    Doug and John

    Yes I agree that too high a resistance will cause problems.

    I'd have suggested a 220 or 270 ohm.

     

    Many years ago I used a 555 to drive a 2N3055 directly in a DC dimming cct.

    I used a capacitor across the resistor to improve the response and it was very happy dimming a 12v 50W lamp with no heatsink.

     

    There are fet driver chips available (I've used them directly to control a motor) but since the OP want to use Jaycar, then this isn't an option.

     

    It would be a good post to add, as I'm sure others will want to emulate it.

    Mark

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • wallarug
    0 wallarug over 12 years ago in reply to Problemchild

    I shall make sure that I do a piece on this on my E14 Blog.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • Robert Peter Oakes
    0 Robert Peter Oakes over 12 years ago in reply to wallarug

    We look forward to it, thanks

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • Problemchild
    0 Problemchild over 12 years ago in reply to mcb1

    This exact question had come up on the Arduino site (probably a hundred other places as well).

    The IRF540 came up time and again, not to mention it's in the kits that many of the EBAY retailers deliver.

    The simple direct drive seems to be used most but several went for an Optoisolator and got full galvanic separation...no dodgy feed back then I bet image!

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • Problemchild
    0 Problemchild over 12 years ago in reply to mcb1

    This exact question had come up on the Arduino site (probably a hundred other places as well).

    The IRF540 came up time and again, not to mention it's in the kits that many of the EBAY retailers deliver.

    The simple direct drive seems to be used most but several went for an Optoisolator and got full galvanic separation...no dodgy feed back then I bet image!

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Children
  • Problemchild
    0 Problemchild over 12 years ago in reply to Problemchild

    I think Douglas means like this:

    image

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Reject Answer