Arduino
  • Products
  • More
Arduino
Arduino Forum How to wire a transistor?
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Arduino to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Replies 18 replies
  • Answers 2 answers
  • Subscribers 418 subscribers
  • Views 2178 views
  • Users 0 members are here
  • transistor
  • circuit
  • wiring
  • wire
  • Design
  • arduino
  • circuitry
Related

How to wire a transistor?

nschreiber0813
nschreiber0813 over 12 years ago

Dear: Element 14

Hello it is me Noah again as you may remember me from my last post I am trying to build an arduino rocket controller and I am at prototyping stage. First of all you should know that I am using transistors BD712 which a pnp transistor that I need to amplify a current. The reason I need it to amplify a current is because I need it to increase 5V to 7.5V and to then send the current to my fixed barrier terminal blocks where it will then detonate the rocket motors. You see first of all in order you need a base resistor that connects to ground. The reason you need that is to prevent the board from short circuiting. I have placed several base resistors at several points and according to wikipedia I think I am doing this right. It says on wikipedia that I should do this.

NPN_common_emitter.svg

And this is what I did.

image

Please can you help me because I am not even sure what a transistor is?

  • Sign in to reply
  • Cancel

Top Replies

  • D_Hersey
    D_Hersey over 12 years ago +1
    It would be useful to know how much current you would need to actuate an ignitior, and if they melt open when actuated. If this is the case, you could use a thrystor. In the more general case of having…
  • D_Hersey
    D_Hersey over 12 years ago +1
    Sure, thank you kindly for asking. I used to play with rockets when I was a kid, but feel free to enlighten me on the topic. A thrystor is a device such as a SCR or TRIAC. These devices turn on well, but…
  • D_Hersey
    D_Hersey over 12 years ago +1
    Model rocket igniters are made with wires made from nichrome, or were when I was a kid. The electric burner on a stove is made out of the stuff AFIK. It is 50/50 nickel and chrome. Hard, low corrosive…
Parents
  • michaelwylie
    0 michaelwylie over 12 years ago

    1. Start with figuring out how much current your load will need and at what voltage (power). Then try linear technologies and look for a regulator that can deliver that output voltage at the rated current.

    2. How much current are we talking about?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • nschreiber0813
    0 nschreiber0813 over 12 years ago in reply to michaelwylie

    Dear: Mike

    I am talking about voltage being in between 7.5V and 9V. Could a regulator do that.

    From: Noah

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • michaelwylie
    0 michaelwylie over 12 years ago in reply to nschreiber0813

    The regulator will take an input voltage and transform it to a new level. You can increase the voltage, or decrease based upon an input voltage. A 7909 regulator can deliver 9 volts at 1 AMP. The output voltage will always be 9 Volts as long as the input never drops below a threshold value. This is a typical linear regulator (old technology). You can also increase voltages using boost regulators.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Reject Answer
    • Cancel
Reply
  • michaelwylie
    0 michaelwylie over 12 years ago in reply to nschreiber0813

    The regulator will take an input voltage and transform it to a new level. You can increase the voltage, or decrease based upon an input voltage. A 7909 regulator can deliver 9 volts at 1 AMP. The output voltage will always be 9 Volts as long as the input never drops below a threshold value. This is a typical linear regulator (old technology). You can also increase voltages using boost regulators.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Reject Answer
    • Cancel
Children
  • nschreiber0813
    0 nschreiber0813 over 12 years ago in reply to michaelwylie

    Dear: Mike

    Thank you for your help. Now I get to build my arduino rocket controller much better now so thanks. Also send me a post if you need help but I highly doubt I could do much.

    From: Noahimage

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • michaelwylie
    0 michaelwylie over 12 years ago in reply to nschreiber0813

    No problem. Since you are new, as you mentioned, always keep in mind when you are regulating or amplifying that devices have power limits. If you exceed these power limits the device will ... well... be destroyed, usually violently. Think of a loud popping sound and a puff of smoke. Just keep this in mind as you design; I only mention it because I've destroyed more than my share of components.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • michaelwylie
    0 michaelwylie over 12 years ago in reply to nschreiber0813

    Oh, I almost forgot, you initial design with transistors was going in the right direction. Look up linear regulator and you'll see how these things are implemented inside the chip.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • nschreiber0813
    0 nschreiber0813 over 12 years ago in reply to michaelwylie

    Don't worry I am already doing that right now so thank you!!!image