Arduino
  • Products
  • More
Arduino
Arduino Forum controlling 3.1 volt steppers with adafruit motorshields v 2.3
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Arduino to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Replies 10 replies
  • Answers 2 answers
  • Subscribers 419 subscribers
  • Views 995 views
  • Users 0 members are here
  • stepper
  • ohm's_law
  • motor_shield
  • adafruit
  • arduino
Related

controlling 3.1 volt steppers with adafruit motorshields v 2.3

e14 Contributor
e14 Contributor over 11 years ago

Hi.

 

I'm quite new to electronics and robotics.

 

I've got two adafruit motor shields and three steppers. The steppers has a rated current of 2.5 A and a phase resistance of 1.25 ohms.

 

I understand from adafruits documentation that it can control motors in a voltage range of 5-12 V dc.

 

My question is can I use my 3.125 V motors if I put a  3.55 Ohm resistor in serie in each phase of each motor?

I calculated the restistance using Ohm's law:

U = I * R

12 V = 2.5 A * (1.25 Ohm + 3.55 Ohm)

 

Have a nice Weekend image

 

- Roar

  • Sign in to reply
  • Cancel

Top Replies

  • Robert Peter Oakes
    Robert Peter Oakes over 11 years ago in reply to clem57 +3 verified
    In most stepper motor controllers (Modern ones), you do not limit the voltage by setting up a divider (R1, R2 ) as they manage the pulse width in the same way as driving an LED with PWM, it is more about…
  • clem57
    clem57 over 11 years ago in reply to e14 Contributor +1
    The voltage divider is better way to go sending one end to ground. I have seen this for 5 volt connections to a 3.3 volt pins on Raspberry Pi. But Too much voltage does not divide well. 12 volts to 3 volts…
  • Robert Peter Oakes
    Robert Peter Oakes over 11 years ago in reply to e14 Contributor +1
    See my other coment but in context to your comment, most motors have a rated current, not voltage and the controller takes care of the difference
Parents
  • clem57
    0 clem57 over 11 years ago

    Why did you pick the Max voltage in the range? Why not average? You really need to show schematic first to see the total picture.

    Clem

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 11 years ago in reply to clem57

    There was no particular reason for the for the voltage choice. I'll try to make a schematic. I've never written one - I've only looked at other peoples schematics.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • e14 Contributor
    0 e14 Contributor over 11 years ago in reply to clem57

    There was no particular reason for the for the voltage choice. I'll try to make a schematic. I've never written one - I've only looked at other peoples schematics.