Arduino
  • Products & Partners
  • More
Arduino
Arduino Forum Measuring speed, angle and height
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Arduino to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 31 replies
  • Subscribers 420 subscribers
  • Views 5104 views
  • Users 0 members are here
  • object
  • flying
  • angle
  • arduino
  • speed
  • height
Related

Measuring speed, angle and height

SGarciaV
SGarciaV over 11 years ago

Hi all,

 

I am discussing a possible project, but I am not certain how feasible it is. The project consists of using an Arduino, plus some sensor (or sensors) to measure the speed, angle and height of a flying object over a 6 x 30 cm surface. Although I am unfamiliar with the details, the object will pass over the surface and the Arduino needs to get how fast it is moving, the angle at which it crosses the surface and the distance from the surface to the object.

 

I posted a rough sketch below.

 

Can some one please provide some feedback as to how feasible this is and what sort of sensor(s) will be needed? Thanks! Salvador

 

image

  • Sign in to reply
  • Cancel

Top Replies

  • dougw
    dougw over 10 years ago +1
    Here is a technique that might work - the accuracy depends on how well it is implemented. start with a narrow beam LED (preferably collimated) or a laser shine it through a section of a cylindrical lens…
  • SGarciaV
    SGarciaV over 10 years ago in reply to bhavikbhansali +1
    Hi Bhavik! Thank you for your reply. The object is a tennis ball traveling at approximately 70 to 90 miles per hour. Salvador
  • SGarciaV
    SGarciaV over 10 years ago in reply to dougw

    Thanks Douglas.I had mentioned to him about using lasers, but my idea consisted of using multiple lasers to create the plane, instead of one laser passing through a cylindrical lens to create the plane. I am intrigued enough by your idea that if I can make the time I might test it out myself.Thanks for your input! Salvador

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • bhavikbhansali
    bhavikbhansali over 10 years ago

    Hello @Salvador Garcia

    If your object size is big then you can interface barometric sensor to calculate height of that object (with respect to celebrated surface) and By using acclerometer and tilt sensor you can calculate its angle with calibrated surface. This things are done with complex programming as per your requirement.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • SGarciaV
    SGarciaV over 10 years ago in reply to bhavikbhansali

    Hi Bhavik! Thank you for your reply. The object is a tennis ball traveling at approximately 70 to 90 miles per hour. Salvador

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • jc2048
    jc2048 over 10 years ago

    Rather than use a camera with it's very limited frame rate, you could use several linear sensor arrays like these:

     

    http://www.digikey.co.uk/product-detail/en/TSL1401CL/TSL1401CLCT-ND/3095283

     

    If you placed a wide angle lens, with a 90 degree field of view, in front of the device you'd have a fan-like view. One at each of the front corners, facing towards each other and up would give you the ability to do triangulation on a plane rising from the front. With another pair at the back, you'd then have enough information to do the timing and the trajectory. Wouldn't work for small objects, but might be ok for your tennis ball.

     

    They'd be much faster than a camera. You'd need a decent a/d. Haven't looked at sensitivity (adaption to varying light levels) and would have problems with background motion (people moving around) if it wasn't screened. Whether you could do all the processing with an Arduino I don't know - I would think not.

     

    Might not be necessary to digitise; if there were enough contrast between the ball and the background (enhance with a filter?) you could use a comparator, with counters to store the start and stop position along the line, perhaps with some adjustment of the reference level to take into account the brightness level. Arduino might manage all that if it's got several seconds after the ball goes through to do the calculations.

     

    Note this is just for discussion. I'm not offering it as a solution.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • amgalbu
    amgalbu over 10 years ago

    HI Salvador

    what about two infrared barriers placed at a certain distance?

    The time it takes for the ball to travel from one barriers to the other gives you the speed, whereas the interrupted beams gives you the angle

     

    Cheers

    Ambrogio

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • balearicdynamics
    balearicdynamics over 10 years ago in reply to amgalbu

    Mmmm.... Ambrogio,

    your idea IMO arises at least a couple of issues. The first is that using beams, by definition these are not lasers but IR lights so for every barer there is a too wide acceptance range and consequently a precision loss. The second is that this means placing fixed position so there is not a full coverage or the real passage angle. I think that with this method you will try to use a well working system to manage a pre-defined targeting measurement system with a unknown behavioural system.

     

    Based on your suggestion - and ignoring the budget aspects as I don't know what are the costs for the  peripherals- maybe the idea of the IR measurement (as well as similar laser application) may work as it works at a specific wavelength range. The most reliable possibility I see to target the precise angle of passage is the use of a linear camera; there are some working well on the IR wavelength and other working in visibile light. Simple OpAmp band-pass filters can isolate only the desired wavelength, that will be the source light for measure. AFAIK (I used linear cameras about 25 years ago) these can be triggered as well as reading data without considering the acquired "images" but just the electric signal variation so I think that also a small micro controller board can do de job.

     

    Enrico

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • bhavikbhansali
    bhavikbhansali over 10 years ago in reply to SGarciaV

    Hello Salvador Garcia..... You have to make a special tennis ball which have barometric sensor  inside it and can transmit data wireless and configure reference surface. By this way you can calculate  height. In cricket ICC and other use snickometer to detect whether edge of bat is touch to bat or not such like you put Barometric sensor inside ball. 

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • amgalbu
    amgalbu over 10 years ago in reply to balearicdynamics

    Hi Enrico

    An IR barrier detects objects that pass in front of the receiver, so the precision is not so bad

    I agree this is not the best solution but in my opinion is an option considered the limited computational resources available on the Arduino board

    Then if one decide to connect a camera that can automatically track objects to Arduino is a completely different approach...

     

    Cheers

    Ambrogio

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • balearicdynamics
    balearicdynamics over 10 years ago in reply to amgalbu

    Hi Ambrogio, it is true. I though to a series of single beams.

     

    About the camera instead, sure to manage data with a poor processing capabilities a hardware pre-processing circuit (cleaning the signal and isolating just what it is needed) maybe a good practice. The camera alone interfaced with the Arduino board ... I see it like an improbable challenge.

     

    Enrico

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • michaelkellett
    michaelkellett over 10 years ago in reply to bhavikbhansali

    Well, actually, the Snicko doesn't work like that  - it uses a microphone to listen for the ball hitting things.

     

    Snicko-Meter

     

    MK

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
<>