Avnet Boards Forums
  • Products
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
Avnet Boards General initial booting
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Replies 20 replies
  • Subscribers 374 subscribers
  • Views 2171 views
  • Users 0 members are here
  • mini-module
  • minimodule
  • zynq
  • mini-module_plus
Related

initial booting

sungyung_lim
sungyung_lim over 10 years ago

We purchased a MMP with zynq 7z100.
Since we followed the simple instruction,
we found that the initial serial connection didn't work.
We used sd card-based booting with factory-installed linux image. Is there any known defect on instruction or linux image? And is there any useful information on it?

Thank you for your consideration in advance.

  • Sign in to reply
  • Cancel
Parents
  • e14 Contributor
    0 e14 Contributor over 10 years ago

    Hello Adrian,

     

    A colleague of mine was able to get an MMP board and was able to verify the issue you observed with the QSPI Flash load. It looks like we have a problem with the pre-loaded QSPI image and will work on that. Thanks for alerting us to the problem.

     

    I am not sure exactly what you are seeing with the Out of Box SD Card image. If you push SW10 the LED brightness application should exit and return to the Linux prompt. You can download the Out of Box SD card image, along with documentation and directions on the LED Brightness demo application from the MMP Reference Designs /Tutorials page here:

     

    http://zedboard.org/support/design/3006/26

     

    We also verified that the image available with the MMP compressed PetaLinux BSP, which you can also download from the same MMP Reference Designs page, works correctly. This image is more up to date than the Out of Box SD Card Linux image and you may want to start with that. The compressed BSP image you download is basically a zip file of a zip file, so use WinZip or similar program to extract twice.

     

    -Gary

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 10 years ago in reply to e14 Contributor

    Hi,
    I pushed SW10 and all the other switches.  Still does not boot.
    I will try downloading the new image and give that a shot.
    Adrian

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 10 years ago in reply to e14 Contributor

    Hi Gary,
    I need assistance.  My board does not boot.  Pressing SW10 does not get me around the Led dimmer issue.
    I would also like your email address and phone number to speed up the process.


    Adrian

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 10 years ago in reply to e14 Contributor

    Hi,
    I tried the new image and it also hangs in the same spot.
    Pressing SW10 does not allow the image to boot.

    Cheers,

    Adrian

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 10 years ago in reply to e14 Contributor

    Hello Adrian,

     

    Once you power up your board and get the Linux prompt could you try entering "/opt/Avnet/led_dimmer.elf" and see if the LED brightness app works correctly?

     

    -Gary

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • e14 Contributor
    0 e14 Contributor over 10 years ago in reply to e14 Contributor

    Hello Adrian,

     

    Once you power up your board and get the Linux prompt could you try entering "/opt/Avnet/led_dimmer.elf" and see if the LED brightness app works correctly?

     

    -Gary

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Children
  • robertleeatavnet
    0 robertleeatavnet over 8 years ago in reply to e14 Contributor

    Hi Gary,

    Just unpacked a fresh spanking new Zynq MMC board.  I'm seeing the same symptom as Adrian.  After a "run sdboot" at the uboot prompt, Linux boot proceeds.  However, the last output is "led_brightness device class registered.", followed by a locked console.  No Linux prompt ever appears.

    Was there a resolution to this?

    ...
    xwdtps f8005000.ps7-wdt: Xilinx Watchdog Timer at f006c000 with timeout 10s

    sdhci: Secure Digital Host Controller Interface driver
    sdhci: Copyright(c) Pierre Ossman

    sdhci-pltfm: SDHCI platform and OF driver helper

    mmc0: SDHCI controller on e0100000.ps7-sdio [e0100000.ps7-sdio] using ADMA

    usbcore: registered new interface driver usbhid

    usbhid: USB HID core driver

    led-brightness : Found device memory resource at 41200000 00000020.

    led-brightness : Char Device Region Registered, with Major: 248.

    led-brightness : led_brightness device class registered.

    p.p1 {margin: 0.0px 0.0px 0.0px 0.0px; font: 11.0px Menlo} span.s1 {font-variant-ligatures: no-common-ligatures}

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • robertleeatavnet
    0 robertleeatavnet over 8 years ago in reply to robertleeatavnet

    Just wanted to document the solution.

    1.  

      The image shipped on the SD card doesn't quite work.  I downloaded "Zynq MMP 7Z100 Out-of-Box Linux PlanAhead 14.5"
         which was the corresponding zip file ZMMP_7100_OOB_Linux_PA14_5.zip. The relevant files are in the sd_card directory.

    2.  

      SW5 settings were documented incorrectly on some reference materials found on the web (which may have been fine for another version of the board.)  The ZMMP_OOB_Linux_Guide_v1.1.pdf bundled with the zip file showed correct SW5[1:5] settings of off, off, on, on, off.

    With the above, the uboot environment variable "modeboot" gets correctly configured to "sdboot" on reset.  Boot proceeds correctly to Linux root prompt.  Running /opt/Avenet/led_dimmer.elf works:

    / # 

    / # /opt/Avnet/led_dimmer.elf 

    **********************************************************

    *                                                        *

    * Zynq Mini Module PLus (ZMMP) - LED Dimmer Application  *

    *                                                        *

    * Pushbutton switches are located on the MMP Baseboard 2 *

    * between the ZMMP and FMC mounting area (JX3)           *

    *                                                        *

    * Press SW8 to decrease LED brightness                   *

    *                                                        *

    * Press SW9 to increase LED brightness                   *

    *                                                        *

    * Press SW10 to exit                                     *

    *                                                        *

    **********************************************************

    GPIO 54 (SW8) set as INPUT

    GPIO 55 (SW9) set as INPUT

    GPIO 56 (SW10) set as INPUT

    p.p1 {margin: 0.0px 0.0px 0.0px 0.0px; font: 11.0px Menlo} span.s1 {font-variant-ligatures: no-common-ligatures}

    ^C