Avnet Boards Forums
  • Products & Partners
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
Software Application Development Run program from flash
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Replies 6 replies
  • Subscribers 364 subscribers
  • Views 962 views
  • Users 0 members are here
Related

Run program from flash

cascade99
cascade99 over 10 years ago

I'm new on using Zedboard, I have simple program using FreeRTOS, I can run it from RAM. I created BOOT.bin on SDK, but after I did "Program Flash", my program didn't run, anyone knows why?  -- Thanks

  • Sign in to reply
  • Cancel
  • e14 Contributor
    0 e14 Contributor over 10 years ago

    Hello Lynn,

     

    You don't really give us enough information to help very much. What version of Xilinx tools/SDK are you using? What is your host OS? Did you change the boot jumpers on the Zedboard to indicate your new boot location?

     

    How did you create your boot image? Are you trying to boot from QSPI Flash or SD Card? A boot.bin image is used to boot from SD Card but you should generate a .mcs image for a QSPI boot.

     

    Even though it is targeting the MicroZed Board this tutorial should be a good place for you to start:

    http://zedboard.org/sites/default/files/design/04_MZPZ_FSBL_Boot_2015_2_01.zip

     

    Just use the fsbl.elf you generated for your zedboard project, along with your system_wrapper.bit file (if you have one) and the .elf file you generated for your FreeRTOS program in the 'Create Zynq Boot Image' application.

     

    Also note that I deleted your duplicate post on this issue. Please to not make multiple forum posts with the same question.

     

    -Gary

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • cascade99
    0 cascade99 over 10 years ago in reply to e14 Contributor

    I'm using freeRTOS, latest SDK, is it possible I load image to QSPI flash directly from PC without using SD card?
    The link is for MicroZed, if I following the step, will it work for ZedBoard?
    Thanks

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 10 years ago

    Lynn,

     

    The tutorial link is for MicroZed but, except for targeting your hardware project to ZedBoard, the flow will work the same. Once you have generated your .mcs image you can use the 'Program Flash' function under 'Xilinx Tools' in the SDK to program the QSPI Flash as is shown in the tutorial.

     

    -Gary

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Reject Answer
    • Cancel
  • cascade99
    0 cascade99 over 10 years ago

    Thanks for the info, now I got idea. One more question is that if I need also load FPGA code(.PL?) to the QSPI, when should I do that?
    Thanks

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 10 years ago

    As shown in the tutorial if your hardware design includes a PL section you would add that by listing the System_wrapper.bit file after the fsbl.elf, but before your FreeRTOS application, in the Create Zynq Boot Image function under the SDK 'Xilinx Tools'. Then the PL code will be part of the .mcs image you program into the QSPI Flash.

     

    You may want to look at the earlier tutorial to see how these files were created:

     

    http://zedboard.org/support/design/1519/10

     

    -Gary

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • cascade99
    0 cascade99 over 10 years ago in reply to e14 Contributor

    Thanks for your help, it works.