Azure Sphere Starter Kit
  • Products
  • Dev Tools
  • Avnet & Tria Boards Community
  • Azure Sphere Starter Kit
  • More
  • Cancel
Azure Sphere Starter Kit
Blog Azure Sphere - Tips to max-out your Starter Kit hardware! (Part 1)
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Azure Sphere Starter Kit to participate - click to join for free!
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: peterfenn
  • Date Created: 7 Aug 2019 1:50 PM Date Created
  • Views 2947 views
  • Likes 8 likes
  • Comments 12 comments
  • azure sphere kit
  • mikrobus click
  • oled
  • azurespherech
  • azure sphere
  • azure sphere mt3620 starter kit
  • oled display
  • azuresphkt
  • azure sphere starter kit
  • mt3620
  • pmod
Related
Recommended

Azure Sphere - Tips to max-out your Starter Kit hardware! (Part 1)

peterfenn
peterfenn
7 Aug 2019

  • Avnet Starter Kit use of MT3620 ISUs (serial interface blocks)
  • Starter Kit use of GPIOs
  • Starter Kit unpopulated Expansion Connectors
    • J11 3-pin header
    • J13 UART/BLE Connector
    • J7  OLED Display Connector
  • For more Information...

image

 

Avnet Starter Kit use of MT3620 ISUs (serial interface blocks)

 

The three ISUs accessible on your Starter Kit are "preconfigured" in that the ISU signals pinned-out of the module were limited for the support of:

  • ISU0: UART0 (4 IOs)
  • ISU1: SPI1 (5 IOs)
  • ISU2: I2C2 (2 IOs)

 

It is possible however within these pinout limitations, to assign the ISU functions as follows:

  • ISU0: use for I2C or UART or SPI
  • ISU1: use for I2C or UART or SPI
  • ISU2: use for I2C only

 

The table below shows in blue text the functions these ISUs are "assigned" to on the Starter Kit, followed by the alternative interfaces that can be supported by these pins

image

 

The serial interface capabilities of the ISUs are documented at:

https://docs.microsoft.com/en-us/azure-sphere/hardware/mt3620-product-status

 

Starter Kit use of GPIOs

 

The table below shows in blue text the functions that other GPIOs have been assigned to on the Starter Kit

image

 

Starter Kit unpopulated Expansion Connectors

 

Additional expansion options are accessible via three unpopulated connector sites on your Starter Kit (see green-colored call-outs in the board view above)

 

 

J11 3-pin header

This pins-out the TXD outputs of the MT3620's two M4-dedicated UARTs, typically for M4 application debugging (via a USB to serial cable)
but can alternatively be assigned for user-defined GPIO functions

image

A good example where an M4-dedicated UART is used for console output (debugging info) for an application, is provided in the UART_RTApp_MT3620_BareMetal sample application from Microsoft
https://github.com/Azure/azure-sphere-samples/tree/master/Samples/UART/UART_RTApp_MT3620_BareMetal

In other real-time samples, the application polls when data is sent via the UART. In this application however memory buffers are used for send and receive of data, and interrupts rather than polling are used.

(This approach makes the UART_RTApp sample a useful starting-point for non-blocking applications)

 

 

J13 UART/BLE Connector

An unpopulated 2x6 connector site is located under Click Socket #2. Designed to accommodate a 2x6 right-angle female socket,
the pinout is compatible with a subset of Pmod peripheral boards available from Digilent and other suppliers

Notes:

  • The four (ISU0) UART pins and GPIO2 are shared with both Click sockets
  • GPIO1 and GPIO17 are shared only with Click socket #2
  • The WAKEUP input pin allows an external device to wake-up the MT3620 SoC
  • All signalling on this connector is at 3.3V levels

image

image

Right-angle Pmod connector (viewed from board edge)

 

 

J7  OLED Display Connector

The pinout and corner mechanical mounting hole were designed to accommodate one of many 3rd-party 128x64 I2C OLED graphic displays

Make sure to select an OLED display with GND and VCC in the correct order! (Some low-cost OLED displays reverse the sequence of the GND and VCC pins!)

This connector site can alternatively be used for easy attachment of an external sensor to the I2C bus

image

image

OLED Display Connector (viewed from above the board edge)

 

For more Information...

 

For detailed information on your Starter Kit's hardware capabilities, refer to the following documents:

  • Hardware User Guide - Azure Sphere MT3620 Starter Kit
  • Block Diagram - Azure Sphere MT3620 Starter Kit
  • AES-MS-MT3620-SK-G_SCH_2019-07-03
  •      Mediatek MT3620 Datasheet and MT3620 Product Brief documents

     http://avnet.me/mt3620-datasheet

 

Take a look at the Avnet Azure Sphere Starter-Kit: Advanced Tutorial for a comprehensive application example that adds an inexpensive OLED display and Click relay board, and offers rapid implementation via a pre-engineered application template for Azure IoT Central dashboard, remote control of LEDs, relays and OLED messages, plus email notifications, etc

 

image

 

Part 2 of this Tips to max-out your Starter Kit hardware! series is available here:

http://avnet.me/azphere-kit-tips-2

  • Sign in to reply

Top Comments

  • peterfenn
    peterfenn over 6 years ago in reply to stevesmythe +2
    Steve, Thanks for pointing this out. The Grove connector on the Azure Sphere Starter Kit is committed for I2C use only For access to ADC inputs you will need to make use of a Click board rather than Grove…
  • stevesmythe
    stevesmythe over 6 years ago +1
    peterfenn The photo at the bottom of this article shows a Grove rotary angle sensor plugged into the Grove socket on the Azure Sphere board. This would require an ADC channel to read the voltage. Is this…
  • peterfenn
    peterfenn over 6 years ago in reply to stevesmythe +1
    Steve, If looking for a rotary control, have you considered a rotary encoder? There are a couple of inexpensive Click boards that encode the position of the control, some with a ring of LEDs to provide…
  • pmossel
    pmossel over 6 years ago

    After reading a post claiming that the board stopped working after someone "soldered in the OLED display" I decided to use a header, soldering the header into the MT3620 and plugging the OLED display recommended by Avnet into the header.  Everything worked well. The only thing I must solve is how to program the OLED to display diagnostic messages. There are some code snippets in AvnetStarterKitOled but the "official"  AvnetStarterKitReferenceDesign GitHub repo only offers the following: "TODO: Add support for OLED display".

    image

    image

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • xeonaj
    xeonaj over 6 years ago

    Thanks!

    But a good PDF file would have been helpful!

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • stevesmythe
    stevesmythe over 6 years ago in reply to peterfenn

    Good idea! That module looks quite cool with the LEDs. Thanks.

     

    Steve

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • peterfenn
    peterfenn over 6 years ago in reply to stevesmythe

    Steve,
    If looking for a rotary control, have you considered a rotary encoder?

    There are a couple of inexpensive Click boards that encode the position of the control, some with a ring of LEDs to provide visual indication of the setting
    https://www.mikroe.com/search?search_query=rotary
    eg.
    https://www.mikroe.com/rotary-r-click

    https://www.youtube.com/watch?v=FtLVviHsWvU  

    -Peter

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • stevesmythe
    stevesmythe over 6 years ago in reply to peterfenn

    Thanks for that clarification. Also, I didn't know about the filter tool on the MikroE website.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
<>