Browse By Tags

  • Azure Sphere Webinar Discussion Forum (Post questions and comments here!)

    I hope everyone that attended todays Azure Sphere Webinar (Session #1) got a lot from the session. Let's use this forum for any questions on the labs, presentations, homework or any other Azure Sphere related questions. Brian
  • Upcoming Azure Sphere Technical Webinar, and Rev2 Azure Sphere Starter kits available for purchase!

    Hi All, I invite anyone interested in IoT and IoT Security to sign up for the upcoming 3-part webinar featuring Microsoft's Azure Sphere MCU starting on Jan 20th. The webinar will take a deep dive into recent development tools that make Azure Sphere…
  • Secure your IoT Solution with Microsoft’s Azure Sphere MCU

    to Coordinated Universal Time
    On24
    Learn about the Azure Sphere solution and how Microsoft has implemented all the security features required to harden your next IoT product. Event Date & Time: 21st of April at 11:00 AM CT // 4:00 PM GMT Security should be the first requirement for any...
  • Azure Sphere Contest Server -> Wi-Fi not configured

    Trying to do the daily "Azure Sphere Starter Kit Sync with Contest Server" thingie When I click on "Read Device", Device IP is "Wi-Fi not configured" ==> the response: "Device ID" is valid "Device MAC" is valid "Device IP" Wi-Fi not configured If I enter…
  • Cannot get WiFi connected

    Today when I tried to connect to the contest page, I got "WiFi not configured". So I tied to enable/disable the definition. Also a restart as well. After all this I am left with the following: SSID : **************** Configuration state : temp-disabled…
  • Azure Sphere – How to generate Leaf certificate?

    Azure Sphere – How to generate Leaf certificate? It is easy to connect first device to IoT Central. There is step by step. By I want to connect second Azure Sphere device to IoT Central. It is added automatically, just because it is in Azure Sphere Tenant…
  • Azure Sphere can't see iPhone Hot Spot

    I was able to get through all the steps of the Azure Sphere setup, up until I need to connect to wifi to get the device updated. I am in a locked down corporate environment, and need to use a phone hot spot for development. I am on the latest version…
  • What is the maximum current the MT3620 GPIO pins can output?

    What is the maximum current the MT3620 GPIOs pins can output? All the pis provide the same current? Can you configure any of the pins to have high drive strength (i.e 20-mA)?
  • Using GPIO2 Baremetal

    So i have been playing around with the Kit a little and i find it quite difficult to find any documentation whatsoever. I pulled the GPIO sample application from https://github.com/Azure/azure-sphere-samples/tree/master/Samples/GPIO/GPIO_RTApp_MT3620_BareMetal…
  • Hello! Does anyone experienced fail to find lms22hh sensor when loading examples from avnet in Microsoft Visual Studio?

    After hours of installing/uninstalling Visual Studio 2017, Azure Sphere SDK, creating Azure acount and tenant,last night a managed to load the example from Avnet first part tutorial. But in the output window it shows me that it failed to find the lms22hh…
  • Question about Error Message when running the Azure Sphere Reference Design

    Hello Everyone, So far I was able to get the kit and the software installed and I was able to create the necessary accounts. Now I am facing an error that I don't know how to address. I am trying to run the reference design following the steps in this…
  • Sphere not powering on

    I had been going through this sample https://www.element14.com/community/groups/internet-of-things/blog/2019/08/01/azure-sphere-starter-kit-advanced-tutorial Everything worked in the end. let the device on all night, sending data to IoT Central successfully…
  • Connection Issues with the Azure Sphere MT3620 Starter Kit

    I have recently received an Azure Sphere MT3620 starter kit and have been going through the steps to get it started. However I soon had an issue where, when performing a lot of different operations I would get the message: "error: The device is not responding…
  • How to access barometer readings?

    I'm a novice in C and in embedded programming. Let's say I started with Azure Sphere as there was an occasion to enter to this field in a cheap way. As a training I have successfully accessed the readings from gyro and accelerometer, but having issues…
  • have a lot of wifi cameras any way of linking to present alarm system

    hi have a mix of wifi and network cameras and a high quality wifi alarm is it poss to link them together? or can i use this end gadget to finally link my alexa to my bedroom fan
  • Wifi help!!!

    Hey guys, im having an issue with the wifi configuration. Please advise. Everything else is connected and displayed.
  • Eagle File for the Starter Kit Board

    I am wondering if Eagle Files (or any other PCB) for Avnet Started Kit Available? I am trying to build a custom PCB for Clicks but not able to find-out eagle file. Please help !
  • Any information on which PMod boards are compatible with the kit?

    The user guide indicates that a subset of PMod boards from Digilent and other vendors are compatible with the PMod connector on the Azure Sphere kit, but it does not indicate which ones or what the criteria for compatibility are. Does anyone have any…
  • Azure Sphere Medical Measurement Reference Design (Part 1)

    Medical Disclaimer This example does not provide medical advice or diagnostic data. It is intended for informational purposes only. It is not a substitute for professional medical diagnostics, measurements, advice, diagnosis or treatment. If you think…
  • Azure Sphere 19.10 - How does this affect your Starter Kit?

    Useful 19.10 Links What is not in the 19.10 Release! Noteworthy 19.10 Features New Sample Applications CMake by Default New and Changed azsphere CLI Commands What Changed in the Previous 19.09 Release? Useful 19…
  • Implementing Direct Methods in Azure Sphere

    Introduction One of the really nice things about developing your secure IoT product with Azure Sphere is that Microsoft has implemented all the hooks and OS Services for your Azure Sphere application to leverage Azure IoT Hub features for Cloud to Device…
  • Avnet Azure Sphere Resources

    Here at Avnet, we've been working hard to create Azure Sphere content to help developers jump start their Azure Sphere projects. I wanted to create this blog to capture all the content we've developed as well as some links to Microsoft resources. As we…