Azure Sphere Starter Kit
  • Products & Partners
  • Dev Tools
  • Avnet & Tria Boards Community
  • Azure Sphere Starter Kit
  • More
  • Cancel
Azure Sphere Starter Kit
Forum Problem Adding Additional I2C Slaves to Azure Sphere
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Azure Sphere Starter Kit to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 18 replies
  • Subscribers 53 subscribers
  • Views 2411 views
  • Users 0 members are here
  • azure sphere kit
  • azurespherech
  • azure sphere
  • azuresphkt
  • azure sphere starter kit
Related

Problem Adding Additional I2C Slaves to Azure Sphere

Sean_Miller
Sean_Miller over 7 years ago

Using the grove connector pins of the Azure Sphere, I'm attempting to add an I2C slave device (TFmini LIDAR proximity sensor).

 

When I connect it and build the default Azure Sphere Kit solution, the accelerometer is no longer found as shown with the error "LSM6DSO not found!".

 

The code then exits execution.

 

Here is the troubleshooting I tried:

  • Ensured the device didn't have an I2C device ID the same as the accelerometer.  It didn't.  It was 0x10.  The accelerometer is 0x6C as found in the code and validated with a log output.
  • Powered the sensor with a separate battery source and linked the ground of it to a ground pin of the Azure Sphere.
  • Checked the wires to ensure SDA was on SDA and SDL was on SDL.
  • Checked to ensure proper voltage was reaching the sensor power (5V).
  • Ensured both the sensor and the Azure Sphere using 3.3V logic signals per their datasheets/block diagram.  They are 3.3V.
  • Reviewed what ID is returned in the initI2C routine using the following additional line of code:  (It returns a zero versus an expected decimal value of 16 which would be 0x10 in hexidecimal.)

// Check device ID

 lsm6dso_device_id_get(&dev_ctx, &whoamI);

 Log_Debug("Sean's Search ID: %d\n",whoamI);

 if (whoamI != LSM6DSO_ID) {

 

  • Removed power from the slave device, but kept its two wires connected.  The problem stayed.  Device ID was returned as 0.
  • With power removed, I disconnected the SDL wire and left the SDA connected.  The problem stayed.  Device ID was returned as 0.
  • With power removed, I disconnected the SDA wire and left the SDL connected.  The problem stayed.  Device ID was returned as 0.
  • With power removed, I disconnected both the SDA and SDL in turn removing the device entirely from the circuit.  The Accelerometer was detected again.

 

I thought that perhaps it was due to baud rate.  The Azure code shows 100000 for bus speed.  Example Arduino code for the device shows 115200 baud rate.  With the slave device powered down and still connected to SDA and SCL, it still caused the problem making me think its not baud rate.

 

I would think that there is a pullup or pulldown already built in to the Azure Sphere's I2C SDA and SDL lines and no need to add one to my slave device.

 

Any thoughts on what else to troubleshoot?

 

Thanks,

Sean

  • Sign in to reply
  • Cancel

Top Replies

  • peterfenn
    peterfenn over 7 years ago in reply to Sean_Miller +4
    Sean According to the TFmini I2C datasheet, the maximum rate for the I2C clock is 400 kbps. I recommend reducing the Azure Sphere I2C setting from 1MHz to 400 kbps to accommodate this. Change line 210…
  • peterfenn
    peterfenn over 7 years ago in reply to Sean_Miller +4
    Sean Two observations: 1) According to the definition of that I2CMaster_Write() function, this returns number of bytes successfully written, or -1 for failure 2) I'd suggest that your my_reset_value be…
  • peterfenn
    peterfenn over 7 years ago in reply to Sean_Miller +4
    Sean For that read data command you were originally trying to send, I'd recommend using the I2CMaster_WriteThenRead() command The format of this command is: ssize_t I2CMaster_WriteThenRead(int fd, I2C_DeviceAddress…
Parents
  • peterfenn
    peterfenn over 7 years ago

    Sean

     

    The primary I2C bus on the Avnet Azure Sphere Starter Kit has 4K7 pullup resistors to the 3.3V rail


    1) Please confirm which TFMini Lidar module you are using? I assume it is this I2C version (not the UART version)

    2) Are you powering the TFMini board from 3.3V or 5V rail?

    3) Via which connector are you attaching the TFMini board? (Grove?)

     

    -Peter

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • Sean_Miller
    Sean_Miller over 7 years ago in reply to peterfenn

    Thanks for the reply.  I have some new developments, but here are the answers to your questions:

     

    1)  I2C Version definitely.  Confirmed using it with Arduino Wire library.

    2)  I am powering using a 5V secondary power source tying the grounds together.  The TFMini datasheet shows it requires a 5V source but has 3.3V logic.

    3)  I am just using jumper cables to attach the board.

     

    I added 4.7K pullup resistors to the lines after studying an I2C grove board.  I figured it couldn't hurt.  I found, though, I had to make the connections with the board completely powered down - a reset of the board after connecting wouldn't work - it had to be unplugged entirely and then everything hooked up.

     

    So, now it does recognize the on board accelerometer while hooked up.  I still haven't been able to talk to the TFMini, yet, but that is due to me fumbling through its means of communicating through I2C.

     

    Thanks for your help.

    Sean

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Cancel
  • Sean_Miller
    Sean_Miller over 7 years ago in reply to Sean_Miller

    I was able to remove my added 4.7K pullup resistors and get the accelerometer to work after all.

     

    However, I cannot access my slave device.  Here is the code:

     

    void seanWriteI2C() {
     uint8_t cmdBuffer[3];
     cmdBuffer[0] = 0x01;
     cmdBuffer[1] = 0x02;
     cmdBuffer[2] = 7;
     int32_t retVal = I2CMaster_Write(i2cFd,0x10,cmdBuffer,3);
     if (retVal < 0) {
      Log_Debug("ERROR: seanWriteI2C: errno=%d (%s)\n", errno, strerror(errno));
     }
     else {
      Log_Debug("Sean:  Worked!\n");
     }
    }

     

    The I2CMaster_Write throws an error that it can't find the address. 

     

    I call this right after the i2c.c file shows the acceleration values.

     

    The address is definitely correct as it works on the Arduino.  Not sure why its not finding it.

     

    -Sean

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • peterfenn
    peterfenn over 7 years ago in reply to Sean_Miller

    Sean

    According to the TFmini I2C datasheet, the maximum rate for the I2C clock is 400 kbps.


    I recommend reducing the Azure Sphere I2C setting from 1MHz to 400 kbps to accommodate this.

    image

     

    Change line 210 of i2c.c as follows:

    image

     

    -Peter

    • Cancel
    • Vote Up +4 Vote Down
    • Sign in to reply
    • Cancel
  • Sean_Miller
    Sean_Miller over 7 years ago in reply to peterfenn

    Thanks for this research.  I hate to burden you with my woes to that extent, but it is appreciated.  I've been giving it the old college try all day, but its slow due to frequent need of reboots due to the Network Adapter dropping out on me or weird things like the LPS22HH suddenly not being found and not coming back until I cycle everything including the PC.

     

    In the code, however, I believe I2C_BUS_Standard is the slower of the 2.  Standard is 100KHz - Not 1MHz.

     

    However, I gave it a try regardless, but unfortunately have the similar results of it not wanting to detect the accelerometer when the TFMini is connected.

     

    I have got it to successfully talk to the TFMini twice out of about 20 tries now, but have no clue what conditions allowed it as all I did was cycle power once again.

     

    When I did get lucky and it detected the accelerometer, the code continued.  I found that the reason it wasn't finding my TFMini address was due to how it was compiling/casting the I2C value of the TFMini.  I changed how I managed that value by declaring a variable as "const uint8_t" and it made it to the "Sean:  Worked!" code below.

     

    void seanWriteI2C() {
     const uint8_t myLIDAR = 0x10;
     uint8_t cmdBuffer[3];
     cmdBuffer[0] = 0x01;
     cmdBuffer[1] = 0x02;
     cmdBuffer[2] = 7;
     int32_t retVal = I2CMaster_Write(i2cFd,myLIDAR,cmdBuffer,3);//guessing here, using 2 for the stuff byte plus the address byte
     if (retVal < 0) {
      Log_Debug("ERROR: seanWriteI2C: errno=%d (%s)\n", errno, strerror(errno));
     }
     else {
      Log_Debug("Sean:  Worked!\n");
     }
    }

     

    Unfortunately, it went back to not detecting the Accelerometer on the next deployment.

     

    The reason it doesn't see the Accelerometer changes, too.  Sometimes it executes and reports in the output "ERROR: platform_read(write step): errno=16 (Resource busy)" when its trying to read its register in the initI2C.  Sometimes it says "Request Timed Out".  Sometimes it says "No device or address".

     

    Very strange, that's for sure.  I'll keep at it forever, though, because allowing to connect to all my existing I2C sensors I've collected over the years will be a very good thing.

     

    Thanks,

    Sean

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Cancel
  • peterfenn
    peterfenn over 7 years ago in reply to Sean_Miller

    Sean

     

    Doh! You are too polite - I stand corrected, the default was 100 kHz not 1 Mhz

     

    It would be good to view this with a logic analyzer...

     

    -Peter

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • peterfenn
    peterfenn over 7 years ago in reply to Sean_Miller

    Sean

     

    Doh! You are too polite - I stand corrected, the default was 100 kHz not 1 Mhz

     

    It would be good to view this with a logic analyzer...

     

    -Peter

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Children
  • peterfenn
    peterfenn over 7 years ago in reply to peterfenn

    PS: You could try sending a soft reset to that TFMini module before you do the first measurement
    It appears this is done with a single 0x06 byte write, to the slave 0x10 address 






    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Cancel
  • Sean_Miller
    Sean_Miller over 7 years ago in reply to peterfenn

    Okay, I've now at least got order to the chaos.  I can do the following:

    1. Deploy and get an error during execution stating "Operation Timed Out" when its looking for the accelerometer id upon init.
    2. Deploy immediately again and get an error during execution stating "Resource Busy" when it attempts to look for the accelerometer id upon init.
    3. Cylce the power on the TFMini.
    4. Deploy again and the accelerometer ID is found and I can write a command to TFMini.  However, I still haven't pulled off a successful read.

     

    I can do this sequence again and again and it works every time.  So, I suspect it has to do with the TFMini somehow buggering up the I2C bus.

     

    So, I'm trying your soft reset suggestion.  I have placed the following code in the initi2c:

     

    // Initialize TFMini
     uint8_t my_reset_value[1] = { 0x06 };
     I2C_DeviceAddress my_TFMini = 0x10;
     result = I2CMaster_Write(i2cFd, my_TFMini, my_reset_value, 1);//send soft reset
     if (result != 0) {
      Log_Debug("ERROR: TFMini Soft Reset Fail: errno=%d (%s)\n", errno, strerror(errno));
      //return -1;
     }

     

    With this code, I get the error response that states "errno=0 (No error information)".

     

    I wonder if I should put an asterisk in front of *my_reset_value.  When I do, I get the error response "(Bad Address)".

     

    I feel I'm inches away.  Any thoughts?

     

    See ya',

    Sean

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • peterfenn
    peterfenn over 7 years ago in reply to Sean_Miller

    Sean

     

    Two observations:

     

    1) According to the definition of that I2CMaster_Write() function, this returns number of bytes successfully written, or -1 for failure

    image

     

    2) I'd suggest that your my_reset_value be defined as follows:
    uint8_t my_reset_value[0] = { 0x06 }; 

     

    -Peter

    • Cancel
    • Vote Up +4 Vote Down
    • Sign in to reply
    • Cancel
  • Sean_Miller
    Sean_Miller over 7 years ago in reply to peterfenn

    That's funny!    It was successfully writing the single byte all along.

     

    I copied the if statement from the line above and paid no attention.  Happens after this many hours of beating my head against the wall.

     

    Now to get it to read.  The chapter continues.

     

    Thanks for the second set of eyes on it!

     

    See ya',

    Sean

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • peterfenn
    peterfenn over 7 years ago in reply to Sean_Miller

    Sean

     

    For that read data command you were originally trying to send, I'd recommend using the I2CMaster_WriteThenRead() command


    The format of this command is:

    ssize_t I2CMaster_WriteThenRead(int fd, I2C_DeviceAddress address, const uint8_t *writeData, size_t lenWriteData, uint8_t *readData, size_t lenReadData);

     

    and the values that you need to send are as shown in the datasheet:

    image

    • Cancel
    • Vote Up +4 Vote Down
    • Sign in to reply
    • Cancel
  • Sean_Miller
    Sean_Miller over 7 years ago in reply to peterfenn

    Thanks.  I've been working this function this afternoon.  I have some Arduino code that works with the TFMini which confirms the 0x01, 0x02, 0x07 values as well.

     

    I'm successfully get a return value with the following:

    int32_t retVal = I2CMaster_WriteThenRead(i2cFd,myLIDAR,&cmdBuffer[0],3,incoming,7);

     

    But the return value (retVal) is 10 versus the expected 7.  Also, the first 7 array elements of "incoming" are zero'd out after the call.

     

    Weird...but I'm close!  I'll post the working code if I get it.

     

    I think the erratic behavior before was due to sending bad commands and the TFMini pulling the I2C bus low.  Things are much more stable now that the I2CMaster_ commands are coming back successful.

     

    See ya',

    Sean

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • peterfenn
    peterfenn over 7 years ago in reply to Sean_Miller

    Sean

     

    The MSFT documentation of that I2CMaster_WriteThenRead() library function is located here:

    https://docs.microsoft.com/en-us/azure-sphere/reference/applibs-reference/applibs-i2c/function-i2cmaster-writethenread

     

    Take a look at it's use also in the Weather Station Hackster.io project posted last week:
    https://www.hackster.io/gatoninja236/azure-sphere-weather-station-d5a2bc

    image

    Good Luck - you are very close now! :-)

     

    -Peter

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Cancel
  • Sean_Miller
    Sean_Miller over 7 years ago in reply to peterfenn

    Success!!

     

    Thanks for all your help, Peter!

     

    Here is the working code example that allows one to add on their own I2C sensor to the Azure Sphere.  It is to be placed and called within the i2c.c example code from the AvnetStarterKitReferenceDesign.  This is for use with the TFMini.  The cmdBuffer should be changed to match another devices command bytes per its datasheet.

     

    float readDistance() {
     //Routine to output the distance to the console
     uint16_t distance = 0; //distance
     uint16_t strength = 0; // signal strength
     uint8_t rangeType = 0; //range scale
     I2C_DeviceAddress myLIDAR = 0x10; //your I2C devices address
     uint8_t incoming[7]; //an array of bytes to hold the returned data from the TFMini.
     uint8_t cmdBuffer[] = { 0x01, 0x02, 7 }; //the bytes to send the request to retrieve distance
     
     int32_t retVal = I2CMaster_WriteThenRead(i2cFd,myLIDAR,&cmdBuffer[0],3,&incoming[0],7);
     
     if (retVal < 0) {
      Log_Debug("ERROR: seanWriteI2C: errno=%d (%s)\n", errno, strerror(errno));
      return -1;
     }
     else {
      Log_Debug("Success:  Read Distance!\n");
      for (int x = 0; x < 7; x++)
      {
       if (x == 0)
       {
        //Trigger done
        if (incoming[x] == 0x00)
        {
         Log_Debug("Problem:  Distance data not valid-");//for debugging
        }
        else if (incoming[x] == 0x01)
        {
         Log_Debug("Data valid:     ");
        }
       }
       else if (x == 2)
        distance = incoming[x]; //LSB of the distance value "Dist_L"
       else if (x == 3)
        distance |= incoming[x] << 8; //MSB of the distance value "Dist_H"
       else if (x == 4)
        strength = incoming[x]; //LSB of signal strength value
       else if (x == 5)
        strength |= incoming[x] << 8; //MSB of signal strength value
       else if (x == 6)
        rangeType = incoming[x]; //range scale
      }
      float the_return = distance / (12 * 2.54);
      Log_Debug("Distance=%f Feet\n",the_return);
      return the_return;
     }
     return -1;  //if we get this far, it failed.
    }

     

    I feel like I just whittled a life size bear from the Angel Oak.

     

    After 30 years of programming, pointer syntax still confuses the crap out of me.  My issues all along were primarily pointing to the wrong areas in memory which would send the device or Azure into a chaos.

     

    The data is rolling up to here:  https://raisingawesomedriversafetymonitoring.azureiotcentral.com/details/device/a7y9e6/measurements

     

    I'm curious?  Can anyone access this link?

     

    See ya',

    Sean

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • peterfenn
    peterfenn over 7 years ago in reply to Sean_Miller

    Sean

     

    That's great to hear! Thanks for the feedback and sharing the working code

     

    Right now I see the following message at the azure iot central link you provided

    https://raisingawesomedriversafetymonitoring.azureiotcentral.com/details/device/a7y9e6/measurements

    image

     

    -Peter