Azure Sphere Starter Kit
  • Products & Partners
  • Dev Tools
  • Avnet & Tria Boards Community
  • Azure Sphere Starter Kit
  • More
  • Cancel
Azure Sphere Starter Kit
Forum Ethernet Module Issue
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Azure Sphere Starter Kit to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 7 replies
  • Subscribers 54 subscribers
  • Views 1926 views
  • Users 0 members are here
  • azure sphere kit
  • azurespherech
  • azure sphere
  • azuresphkt
  • azure sphere starter kit
Related

Ethernet Module Issue

sagacr2018
sagacr2018 over 7 years ago

Hi All,

 

I connected Ethernet Module (ENC28J60) and loaded Ethernet Sample from Official GIT. When I am running the program, I am getting following error,

 

ERROR: Networking_SetInterfaceState for interface 'eth0' failed: errno=2 (No such file or directory)

 

Any clue how this can be resolved?

 

Does anyone have working ethernet code for Avnet Azure Starter Kit? 

  • Sign in to reply
  • Cancel

Top Replies

  • peterfenn
    peterfenn over 7 years ago in reply to sagacr2018 +2
    Rohit Note that while the MikroE ethernet Click board (based on ENC28J60) has pinout compatibility with the Avnet Starter Kit, the board configuration image Microsoft provides at this time (lan-enc28j60…
  • clem57
    clem57 over 7 years ago +1
    sagacr2018 I would read all the Microsoft doc . I am willing to bet the setup for the device is missing from the manifest file to permit usage of the Ethernet device. Every thing you touch on the hardware…
  • sagacr2018
    sagacr2018 over 7 years ago in reply to clem57 +1
    Thanks BB-Sphere. I researched more and its not something related to Manifest or permission. I completely missed the following step, Use of Ethernet requires a board configuration image in addition to…
Parents
  • e14 Contributor
    e14 Contributor over 5 years ago

    I too have the same issue in Visual Studio.

    I have deployed both the Board Configuration and the Application image. Still I have this error. Do anyone has any idea about it? Thank you.image

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • e14 Contributor
    e14 Contributor over 5 years ago

    I too have the same issue in Visual Studio.

    I have deployed both the Board Configuration and the Application image. Still I have this error. Do anyone has any idea about it? Thank you.image