Azure Sphere Starter Kit
  • Products & Partners
  • Dev Tools
  • Avnet & Tria Boards Community
  • Azure Sphere Starter Kit
  • More
  • Cancel
Azure Sphere Starter Kit
Forum Ethernet Module Issue
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Azure Sphere Starter Kit to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 7 replies
  • Subscribers 54 subscribers
  • Views 1924 views
  • Users 0 members are here
  • azure sphere kit
  • azurespherech
  • azure sphere
  • azuresphkt
  • azure sphere starter kit
Related

Ethernet Module Issue

sagacr2018
sagacr2018 over 7 years ago

Hi All,

 

I connected Ethernet Module (ENC28J60) and loaded Ethernet Sample from Official GIT. When I am running the program, I am getting following error,

 

ERROR: Networking_SetInterfaceState for interface 'eth0' failed: errno=2 (No such file or directory)

 

Any clue how this can be resolved?

 

Does anyone have working ethernet code for Avnet Azure Starter Kit? 

  • Sign in to reply
  • Cancel

Top Replies

  • peterfenn
    peterfenn over 7 years ago in reply to sagacr2018 +2
    Rohit Note that while the MikroE ethernet Click board (based on ENC28J60) has pinout compatibility with the Avnet Starter Kit, the board configuration image Microsoft provides at this time (lan-enc28j60…
  • clem57
    clem57 over 7 years ago +1
    sagacr2018 I would read all the Microsoft doc . I am willing to bet the setup for the device is missing from the manifest file to permit usage of the Ethernet device. Every thing you touch on the hardware…
  • sagacr2018
    sagacr2018 over 7 years ago in reply to clem57 +1
    Thanks BB-Sphere. I researched more and its not something related to Manifest or permission. I completely missed the following step, Use of Ethernet requires a board configuration image in addition to…
Parents
  • sagacr2018
    sagacr2018 over 7 years ago

    I completely missed sideloading additional board configuration and Program now recognizing eth0.  Now there is another problem! Microsoft only supplies Ethernet Image with support on ISU0 and Interrupt on GPIO5 but Avnet Sphere Kit doesn't have any such combination. It has SPI on ISU1 with Interrupts on GPIO 2. Help !!

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • peterfenn
    peterfenn over 7 years ago in reply to sagacr2018

    Rohit

     

    Note that while the MikroE ethernet Click board (based on ENC28J60) has pinout compatibility with the Avnet Starter Kit, the board configuration image Microsoft provides at this time (lan-enc28j60-isu0-int5) maps to ISU0 and GPIO 5 (not ISU1 and GPIO 2, as needed on the Avnet board)

    We are working with Microsoft on getting software support for this ethernet adaptor with the Avnet Starter Kit, but do not have a date yet when the ISU1 board config package will become available...

     

    MSDN tech support forum post here:
    https://social.msdn.microsoft.com/Forums/en-US/e4b57de0-63ef-4f13-9da2-74fa0cbda330/avnet-azure-sphere-starter-kit-does-…

     

    PS: At this time you can still test your ethernet based application, using the MikroE ethernet Cick board separate from the Starter Kit board.
    ie. Using fly-wires connected to ISU0 via the unpopulated Pmod connector


    -Peter

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Cancel
  • sagacr2018
    sagacr2018 over 7 years ago in reply to peterfenn

    Thanks Peter. Its weird that Microsoft is keeping configuration part as closed source. I am using ETH-Click already and I tried to connect over PMOD connector but GPIO_5 is not available on Kit. Its taken by WiFi light. Also this makes me think that other EthClicks might not work with this Kit as well. Looks like we are on mercy of Microsoft for this now image

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • billchadwick
    billchadwick over 5 years ago in reply to sagacr2018

    Is this lack of support for ETH-Click stiil true a year On?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • billchadwick
    billchadwick over 5 years ago in reply to sagacr2018

    Is this lack of support for ETH-Click stiil true a year On?