Azure Sphere Starter Kit
  • Products & Partners
  • Dev Tools
  • Avnet & Tria Boards Community
  • Azure Sphere Starter Kit
  • More
  • Cancel
Azure Sphere Starter Kit
Forum Sphere wont connect to WiFi
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Azure Sphere Starter Kit to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 5 replies
  • Subscribers 51 subscribers
  • Views 3010 views
  • Users 0 members are here
  • azure sphere kit
  • azurespherech
  • azure sphere
  • azuresphkt
  • azure sphere starter kit
Related

Sphere wont connect to WiFi

kelvic3d
kelvic3d over 7 years ago

Hello,

 

For the last week or so, my sphere wont connect to my Wifi. It appeared to start happening at the same time I had to have my router replaced because of a storm. The new router is almost identical to the old one and I set it up with the same SSID and key that I had on the previous one.

This is the response I get from the show-status comamnd

 

Configuration state : unknown
Connection state    : disconnected
Security state      : unknown
Frequency           :
Mode                :
Key management      : UNKNOWN
WPA State           : SCANNING
IP Address          :
MAC Address         : **:**:**:**:**:**   (disguised)

Command completed successfully in 00:00:01.6956155.

 

This what the list command outputs

 

Network list:

ID                  : 0
SSID                : KELVIC-Net5G
Configuration state : enabled
Connection state    : disconnected
Security state      : psk

ID                  : 1
SSID                : KELVIC-Net2.4
Configuration state : enabled
Connection state    : disconnected
Security state      : psk

Command completed successfully in 00:00:01.9069631

 

Any clue to whats going on? The Shpere was not physically connected during the storm and appears to work fine other then it wont connect to my WiFi. It has been logging into the contest server all week w/o the wifi connected.

  • Sign in to reply
  • Cancel

Top Replies

  • bwilless
    bwilless over 7 years ago +2
    I think that Mike's suggestion is a good one . . . 1. list all the networks "azsphere device wifi list" 2. Delete each one "azsphere device wifi delete -i <network ID from the list command>" 3. Add your…
  • clem57
    clem57 over 7 years ago +1
    Try to disable/enable the entry first. Then try to plug/unplug the USB. This is a known problem Microsoft needs to resolve. Clem PS. Did you check the password is the same? kelvic3d
  • clem57
    clem57 over 7 years ago +1
    Thanks kmikemoo that would be a good last trick. Some router are finicky. check that side as well.
Parents
  • clem57
    clem57 over 7 years ago

    Thanks kmikemoo that would be a good last trick. Some router are finicky. check that side as well.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • clem57
    clem57 over 7 years ago

    Thanks kmikemoo that would be a good last trick. Some router are finicky. check that side as well.